<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Can we modify suspend ram sections in power mode switch example to be smaller? [imx7ulp]</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-we-modify-suspend-ram-sections-in-power-mode-switch-example/m-p/1657750#M206567</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You can modify the RAM space with the linker file, however you can not with ROM space.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Thu, 25 May 2023 14:40:34 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2023-05-25T14:40:34Z</dc:date>
    <item>
      <title>Can we modify suspend ram sections in power mode switch example to be smaller? [imx7ulp]</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-we-modify-suspend-ram-sections-in-power-mode-switch-example/m-p/1656795#M206494</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;we wanted run in VLLS mode on A7 and M4 core. We are using RAM target for m4, but m_text region is not enough for us. I was curious if we can move some space from&amp;nbsp;&lt;SPAN&gt;m_m4_suspend_ram/&lt;/SPAN&gt;&lt;SPAN&gt;m_a7_suspend_ram regions to m_text region. I see that some part of RAM is stored there and then restored as a result of ROM may overwrite specific part of RAM (but don't see how much and where).&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;QSPI memory is used for permanent storing/logging data from m4 core.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 24 May 2023 15:57:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-we-modify-suspend-ram-sections-in-power-mode-switch-example/m-p/1656795#M206494</guid>
      <dc:creator>cervenka</dc:creator>
      <dc:date>2023-05-24T15:57:22Z</dc:date>
    </item>
    <item>
      <title>Re: Can we modify suspend ram sections in power mode switch example to be smaller? [imx7ulp]</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-we-modify-suspend-ram-sections-in-power-mode-switch-example/m-p/1657750#M206567</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You can modify the RAM space with the linker file, however you can not with ROM space.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 25 May 2023 14:40:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-we-modify-suspend-ram-sections-in-power-mode-switch-example/m-p/1657750#M206567</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2023-05-25T14:40:34Z</dc:date>
    </item>
  </channel>
</rss>