<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: PMIC_ON_REQ Behaviour</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-ON-REQ-Behaviour/m-p/243311#M20648</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Feb 2014 03:36:50 GMT</pubDate>
    <dc:creator>YixingKong</dc:creator>
    <dc:date>2014-02-27T03:36:50Z</dc:date>
    <item>
      <title>PMIC_ON_REQ Behaviour</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-ON-REQ-Behaviour/m-p/243306#M20643</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am designing a system with i.MX6 Dualite processor and external DC/DC Converters ( No PMU).&lt;/P&gt;&lt;P&gt;My system needs the Processor to turn ON automatically when the power is applied ( No Button press).&lt;/P&gt;&lt;P&gt;However I should be able to turn – off the processor via the switch connected to ON_OFF Button. &lt;/P&gt;&lt;P&gt;The system will be OFF for a specific duration and should turn ON again automatically..&lt;/P&gt;&lt;P&gt;Note that VDD_SNVS is always present.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am making use of PMIC_ON REQ Signal along with a 555 timer to meet this requirement.&lt;/P&gt;&lt;P&gt;However my question is :&lt;/P&gt;&lt;OL style="list-style-type: decimal;"&gt;&lt;LI&gt;Can the system come up automatically second time without pressing ON_OFF Button again?&lt;/LI&gt;&lt;LI&gt;What are the criteria’s to assert “PMIC_ON_REQ”?&lt;/LI&gt;&lt;LI&gt;Whether the PMIC_ON_REQ gets asserted/de-asserted only by ON_OFF Button press? &lt;/LI&gt;&lt;LI&gt;Consider I turned off the unit by pressing ON_OFF Button. PMIC_ON_REQ = Low. When the system turns ON again automatically, Can it over drive PMIC_IN_REQ to High State from low state? &lt;/LI&gt;&lt;LI&gt;Once SOC is powered up, will it change the state of&amp;nbsp; PMIC_ON_REQ from Low to High?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please clarify,&lt;/P&gt;&lt;P&gt;Sincerely&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Oct 2013 19:11:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PMIC-ON-REQ-Behaviour/m-p/243306#M20643</guid>
      <dc:creator>krishnaprasada</dc:creator>
      <dc:date>2013-10-28T19:11:00Z</dc:date>
    </item>
    <item>
      <title>Re: PMIC_ON_REQ Behaviour</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-ON-REQ-Behaviour/m-p/243307#M20644</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Table 60-3, Power Mode Transitions, in i.MX 6Dual/Quad Reference Manual gives some good info about this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And for i.MX 6DualLite, it's Table 59-1 in DualLite/Solo ref. manual.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Nov 2013 06:41:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PMIC-ON-REQ-Behaviour/m-p/243307#M20644</guid>
      <dc:creator>VladanJovanovic</dc:creator>
      <dc:date>2013-11-01T06:41:50Z</dc:date>
    </item>
    <item>
      <title>Re: PMIC_ON_REQ Behaviour</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-ON-REQ-Behaviour/m-p/243308#M20645</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Yes. As long as the processor start-up sequence is followed, the voltage levels are met and the POR_B signal is released after the power up sequence has finished, the processor will turn on.&lt;BR /&gt;2. PMIC_ON_REQ is a processor signal that turrns on the PMIC, but it actually doesn't affect the processor turn-on. The signal you should be looking at is POR_B. As I mentined, it must be asserted right after the power-up sequence finishes. You will need to control it with a voltage level equal to VDD_SNVS_IN, since this is the reference voltage of POR_B.&lt;/P&gt;&lt;P&gt;3. Yes, PMIC_ON_REQ is asserted with an ONOFF button press.&lt;/P&gt;&lt;P&gt;4. Not sure I understand this question. If the info above is not enough and you still need an answer on this, could you please elaborate?&lt;/P&gt;&lt;P&gt;5. PMIC_ON_REQ signal will stay high as long as the processor is on, and will go low when the system requires to turn off or go to sleep.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;P&gt;Jorge.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Nov 2013 21:09:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PMIC-ON-REQ-Behaviour/m-p/243308#M20645</guid>
      <dc:creator>JorgeRama_rezRi</dc:creator>
      <dc:date>2013-11-04T21:09:16Z</dc:date>
    </item>
    <item>
      <title>Re: PMIC_ON_REQ Behaviour</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-ON-REQ-Behaviour/m-p/243309#M20646</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;More useful info about PMIC_ON_REQ: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-97660?et=watches.email.document"&gt;https://community.freescale.com/docs/DOC-97660?et=watches.email.document&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;P&gt;Jorge.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Nov 2013 21:16:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PMIC-ON-REQ-Behaviour/m-p/243309#M20646</guid>
      <dc:creator>JorgeRama_rezRi</dc:creator>
      <dc:date>2013-11-04T21:16:21Z</dc:date>
    </item>
    <item>
      <title>Re: PMIC_ON_REQ Behaviour</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-ON-REQ-Behaviour/m-p/243310#M20647</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel &lt;/P&gt;&lt;P&gt;free to reply with an update to this discussion.&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Feb 2014 09:11:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PMIC-ON-REQ-Behaviour/m-p/243310#M20647</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-02-21T09:11:31Z</dc:date>
    </item>
    <item>
      <title>Re: PMIC_ON_REQ Behaviour</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-ON-REQ-Behaviour/m-p/243311#M20648</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Feb 2014 03:36:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PMIC-ON-REQ-Behaviour/m-p/243311#M20648</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-02-27T03:36:50Z</dc:date>
    </item>
  </channel>
</rss>