<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SPL to u-boot in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SPL-to-u-boot/m-p/1655379#M206324</link>
    <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Maybe you can try&amp;nbsp;HANDOFF&lt;/P&gt;&lt;P&gt;config HANDOFF&lt;BR /&gt;bool "Pass hand-off information from SPL to U-Boot proper"&lt;BR /&gt;depends on BLOBLIST&lt;BR /&gt;help&lt;BR /&gt;It is useful to be able to pass information from SPL to U-Boot&lt;BR /&gt;proper to preserve state that is known in SPL and is needed in U-Boot.&lt;BR /&gt;Enable this to locate the handoff information in U-Boot proper, early&lt;BR /&gt;in boot. It is available in gd-&amp;gt;handoff. The state state is set up&lt;BR /&gt;in SPL (or TPL if that is being used).&lt;/P&gt;</description>
    <pubDate>Tue, 23 May 2023 07:01:45 GMT</pubDate>
    <dc:creator>dtony</dc:creator>
    <dc:date>2023-05-23T07:01:45Z</dc:date>
    <item>
      <title>SPL to u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPL-to-u-boot/m-p/1650577#M205894</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a way to pass info from SPL to u-boot ?&lt;/P&gt;&lt;P&gt;In SPL I read a fuse and I have to pass it to u-boot.&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Wed, 17 May 2023 16:11:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPL-to-u-boot/m-p/1650577#M205894</guid>
      <dc:creator>Arm7</dc:creator>
      <dc:date>2023-05-17T16:11:34Z</dc:date>
    </item>
    <item>
      <title>Re: SPL to u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPL-to-u-boot/m-p/1654311#M206234</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/216780"&gt;@Arm7&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The uboot will query storage first, if there is no env, it will directly use the env at compile time.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Harvey&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 22 May 2023 03:25:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPL-to-u-boot/m-p/1654311#M206234</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2023-05-22T03:25:06Z</dc:date>
    </item>
    <item>
      <title>Re: SPL to u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPL-to-u-boot/m-p/1655379#M206324</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Maybe you can try&amp;nbsp;HANDOFF&lt;/P&gt;&lt;P&gt;config HANDOFF&lt;BR /&gt;bool "Pass hand-off information from SPL to U-Boot proper"&lt;BR /&gt;depends on BLOBLIST&lt;BR /&gt;help&lt;BR /&gt;It is useful to be able to pass information from SPL to U-Boot&lt;BR /&gt;proper to preserve state that is known in SPL and is needed in U-Boot.&lt;BR /&gt;Enable this to locate the handoff information in U-Boot proper, early&lt;BR /&gt;in boot. It is available in gd-&amp;gt;handoff. The state state is set up&lt;BR /&gt;in SPL (or TPL if that is being used).&lt;/P&gt;</description>
      <pubDate>Tue, 23 May 2023 07:01:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPL-to-u-boot/m-p/1655379#M206324</guid>
      <dc:creator>dtony</dc:creator>
      <dc:date>2023-05-23T07:01:45Z</dc:date>
    </item>
  </channel>
</rss>