<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX8MQ custom board getting kernel panic</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MQ-custom-board-getting-kernel-panic/m-p/1655233#M206306</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thank you. It was solved.&lt;/P&gt;</description>
    <pubDate>Tue, 23 May 2023 04:31:50 GMT</pubDate>
    <dc:creator>Saravanans1</dc:creator>
    <dc:date>2023-05-23T04:31:50Z</dc:date>
    <item>
      <title>iMX8MQ custom board getting kernel panic</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MQ-custom-board-getting-kernel-panic/m-p/1645380#M205317</link>
      <description>&lt;P&gt;We have using the iMx8MQ custom board while booting the board from emmc it was stuck in the kernel and showed the Kernel panic errors. Attached log for reference&lt;/P&gt;&lt;P&gt;[2023-05-02 18:29:26.814] [ 3.368409] EXT4-fs (mmcblk0p2): error loading journal&lt;BR /&gt;[2023-05-02 18:29:26.814] [ 3.378764] VFS: Cannot open root device "mmcblk0p2" or unknown-block(179,2): error -5&lt;BR /&gt;[2023-05-02 18:29:26.814] [ 3.386690] Please append a correct "root=" boot option; here are the available partitions:&lt;BR /&gt;[2023-05-02 18:29:26.814] [ 3.395070] 1f00 32768 mtdblock0&lt;BR /&gt;[2023-05-02 18:29:26.814] [ 3.395072] (driver?)&lt;BR /&gt;[2023-05-02 18:29:26.814] [ 3.401641] b300 30535680 mmcblk0&lt;BR /&gt;[2023-05-02 18:29:26.814] [ 3.401643] driver: mmcblk&lt;BR /&gt;[2023-05-02 18:29:26.814] [ 3.408467] b301 5452596 mmcblk0p1 fb8f6d72-01&lt;BR /&gt;[2023-05-02 18:29:26.814] [ 3.408468]&lt;BR /&gt;[2023-05-02 18:29:26.814] [ 3.415279] b302 5452596 mmcblk0p2 fb8f6d72-02&lt;BR /&gt;[2023-05-02 18:29:26.814] [ 3.415280]&lt;BR /&gt;[2023-05-02 18:29:26.814] [ 3.422124] b303 17825792 mmcblk0p3 fb8f6d72-03&lt;BR /&gt;[2023-05-02 18:29:26.814] [ 3.422125]&lt;BR /&gt;[2023-05-02 18:29:26.814] [ 3.428939] b304 1048576 mmcblk0p4 fb8f6d72-04&lt;BR /&gt;[2023-05-02 18:29:26.814] [ 3.428940]&lt;BR /&gt;[2023-05-02 18:29:26.814] [ 3.435761] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,2)&lt;BR /&gt;[2023-05-02 18:29:26.814] [ 3.444199] CPU: 1 PID: 1 Comm: swapper/0 Not tainted 5.4.70-2.3.2+ #1&lt;BR /&gt;[2023-05-02 18:29:26.814] [ 3.450725] Hardware name: NXP i.MX8MQ EVK (DT)&lt;BR /&gt;[2023-05-02 18:29:26.814] [ 3.455253] Call trace:&lt;BR /&gt;[2023-05-02 18:29:26.814] [ 3.457706] dump_backtrace+0x0/0x140&lt;BR /&gt;[2023-05-02 18:29:26.832] [ 3.461369] show_stack+0x14/0x20&lt;BR /&gt;[2023-05-02 18:29:26.832] [ 3.464685] dump_stack+0xb4/0x114&lt;BR /&gt;[2023-05-02 18:29:26.832] [ 3.468087] panic+0x158/0x324&lt;BR /&gt;[2023-05-02 18:29:26.832] [ 3.471143] mount_block_root+0x1d0/0x284&lt;BR /&gt;[2023-05-02 18:29:26.832] [ 3.475150] mount_root+0x124/0x158&lt;BR /&gt;[2023-05-02 18:29:26.832] [ 3.478636] prepare_namespace+0x12c/0x18c&lt;BR /&gt;[2023-05-02 18:29:26.832] [ 3.482732] kernel_init_freeable+0x210/0x23c&lt;BR /&gt;[2023-05-02 18:29:26.832] [ 3.487089] kernel_init+0x10/0x100&lt;BR /&gt;[2023-05-02 18:29:26.832] [ 3.490578] ret_from_fork+0x10/0x1c&lt;BR /&gt;[2023-05-02 18:29:26.832] [ 3.494157] SMP: stopping secondary CPUs&lt;BR /&gt;[2023-05-02 18:29:26.832] [ 3.498597] Kernel Offset: disabled&lt;BR /&gt;[2023-05-02 18:29:26.832] [ 3.502084] CPU features: 0x0002,2000200c&lt;BR /&gt;[2023-05-02 18:29:26.832] [ 3.506092] Memory Limit: none&lt;BR /&gt;[2023-05-02 18:29:26.832] [ 3.509149] ---[ end Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,2) ]---&lt;/P&gt;</description>
      <pubDate>Fri, 05 May 2023 09:35:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MQ-custom-board-getting-kernel-panic/m-p/1645380#M205317</guid>
      <dc:creator>Saravanans1</dc:creator>
      <dc:date>2023-05-05T09:35:25Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MQ custom board getting kernel panic</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MQ-custom-board-getting-kernel-panic/m-p/1647179#M205528</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/197174"&gt;@Saravanans1&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;I hope you are doing well.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;One can rebuild the journal but you will need a Linux machine to do it.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;One can check if the kernel parameter for root= is pointing to the correct partition.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;One can try to re-image the card and try again.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If you are using a driver on u-boot, you need to match the version on kernel side.&lt;/SPAN&gt;&lt;/P&gt;
&lt;DIV&gt;In other words, you might have to use the same version among u-boot, kernel, and rootfs to prevent boot failure issues.&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;Thanks &amp;amp; Regards,&lt;/DIV&gt;
&lt;DIV&gt;Dhruvit Vasavada&lt;/DIV&gt;</description>
      <pubDate>Tue, 09 May 2023 13:10:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MQ-custom-board-getting-kernel-panic/m-p/1647179#M205528</guid>
      <dc:creator>Dhruvit</dc:creator>
      <dc:date>2023-05-09T13:10:28Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MQ custom board getting kernel panic</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MQ-custom-board-getting-kernel-panic/m-p/1648880#M205717</link>
      <description>&lt;P&gt;Thanks for your quick response. We will check and update you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Saravanan S&lt;/P&gt;</description>
      <pubDate>Thu, 11 May 2023 16:30:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MQ-custom-board-getting-kernel-panic/m-p/1648880#M205717</guid>
      <dc:creator>Saravanans1</dc:creator>
      <dc:date>2023-05-11T16:30:14Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MQ custom board getting kernel panic</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MQ-custom-board-getting-kernel-panic/m-p/1649722#M205819</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We have flashed the binary again using uuu tool in serial download mode. Now the kernel panic problem is solved.&lt;/P&gt;</description>
      <pubDate>Sat, 13 May 2023 16:14:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MQ-custom-board-getting-kernel-panic/m-p/1649722#M205819</guid>
      <dc:creator>Saravanans1</dc:creator>
      <dc:date>2023-05-13T16:14:09Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MQ custom board getting kernel panic</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MQ-custom-board-getting-kernel-panic/m-p/1649916#M205847</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/197174"&gt;@Saravanans1&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;As this case is solved, can I mark this as close?&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Dhruvit Vasavada&lt;/P&gt;</description>
      <pubDate>Mon, 15 May 2023 05:18:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MQ-custom-board-getting-kernel-panic/m-p/1649916#M205847</guid>
      <dc:creator>Dhruvit</dc:creator>
      <dc:date>2023-05-15T05:18:59Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MQ custom board getting kernel panic</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MQ-custom-board-getting-kernel-panic/m-p/1655233#M206306</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thank you. It was solved.&lt;/P&gt;</description>
      <pubDate>Tue, 23 May 2023 04:31:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MQ-custom-board-getting-kernel-panic/m-p/1655233#M206306</guid>
      <dc:creator>Saravanans1</dc:creator>
      <dc:date>2023-05-23T04:31:50Z</dc:date>
    </item>
  </channel>
</rss>