<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MIMXRT1060-EVKB USB dev_composite_cdc_msc_disk_freertos example in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1060-EVKB-USB-dev-composite-cdc-msc-disk-freertos-example/m-p/1654072#M206195</link>
    <description>&lt;P&gt;I'm using MCUXpresso v11.7.0 with SDK v2.13.0 on MIMXRT1060-EVKB&lt;/P&gt;&lt;P&gt;I'm trying to test the USB interface using the evkbmimxrt1060_dev_composite_cdc_msc_disk_freertos.&lt;/P&gt;&lt;P&gt;The demo text says that the example provides a vcom and ram disk interface.&lt;/P&gt;&lt;P&gt;It compiles, however when I attempt to run, it stalls after the "Please insert Disk" message is displayed.&amp;nbsp; &amp;nbsp;It only proceeds if I insert an SD card into the onboard socket, but a disk doesn't show up on the PC attached to the USB.&amp;nbsp; &amp;nbsp; Why is this dependent on a physical sd card if it is implementing a ram disk?&lt;/P&gt;&lt;P&gt;Has anyone gotten this demo to work on this configuration?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Sat, 20 May 2023 00:21:09 GMT</pubDate>
    <dc:creator>CktDesigner</dc:creator>
    <dc:date>2023-05-20T00:21:09Z</dc:date>
    <item>
      <title>MIMXRT1060-EVKB USB dev_composite_cdc_msc_disk_freertos example</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1060-EVKB-USB-dev-composite-cdc-msc-disk-freertos-example/m-p/1654072#M206195</link>
      <description>&lt;P&gt;I'm using MCUXpresso v11.7.0 with SDK v2.13.0 on MIMXRT1060-EVKB&lt;/P&gt;&lt;P&gt;I'm trying to test the USB interface using the evkbmimxrt1060_dev_composite_cdc_msc_disk_freertos.&lt;/P&gt;&lt;P&gt;The demo text says that the example provides a vcom and ram disk interface.&lt;/P&gt;&lt;P&gt;It compiles, however when I attempt to run, it stalls after the "Please insert Disk" message is displayed.&amp;nbsp; &amp;nbsp;It only proceeds if I insert an SD card into the onboard socket, but a disk doesn't show up on the PC attached to the USB.&amp;nbsp; &amp;nbsp; Why is this dependent on a physical sd card if it is implementing a ram disk?&lt;/P&gt;&lt;P&gt;Has anyone gotten this demo to work on this configuration?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Sat, 20 May 2023 00:21:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1060-EVKB-USB-dev-composite-cdc-msc-disk-freertos-example/m-p/1654072#M206195</guid>
      <dc:creator>CktDesigner</dc:creator>
      <dc:date>2023-05-20T00:21:09Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1060-EVKB USB dev_composite_cdc_msc_disk_freertos example</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1060-EVKB-USB-dev-composite-cdc-msc-disk-freertos-example/m-p/1656017#M206384</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/212894"&gt;@CktDesigner&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope you are doing great!&lt;/P&gt;
&lt;P&gt;According to the example doc:&amp;nbsp;&lt;/P&gt;
&lt;P class="lia-indent-padding-left-30px"&gt;The USB MSC RAM SD card application is a simple demonstration program based on the MCUXpresso SDK. It is enumerated as a U-disk. Users can read and write the SD card as a standard U-disk.&lt;/P&gt;
&lt;P class="lia-indent-padding-left-30px"&gt;&amp;nbsp;&lt;/P&gt;
&lt;P class="lia-indent-padding-left-30px"&gt;the doc is located inside SDK zip. Just find the SDK and browse to &amp;lt;sdk name&amp;gt;.zip\boards\&amp;lt;board name&amp;gt;\usb_examples\usb_device_msc_disk\freertos\readme.pdf&lt;/P&gt;
&lt;P&gt;So this example is expected to enumerate as a disk once the SD card is inserted. Below an example with windows 10 OS.&amp;nbsp;&lt;/P&gt;
&lt;P class="lia-indent-padding-left-60px"&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="diego_charles_0-1684874099662.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/224556i0078F971D04D44BD/image-size/medium?v=v2&amp;amp;px=400" role="button" title="diego_charles_0-1684874099662.png" alt="diego_charles_0-1684874099662.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;diego_charles_0-1684874099662.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;You may have raised this question as this description when importing the project is a bit generic, and I agree with you.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="diego_charles_1-1684874204599.png" style="width: 594px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/224557i5B18A39E98E66512/image-dimensions/594x134?v=v2" width="594" height="134" role="button" title="diego_charles_1-1684874204599.png" alt="diego_charles_1-1684874204599.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;diego_charles_1-1684874204599.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;If you want&amp;nbsp; get the RT1060 to get enumerated without an SD card, maybe you could try &lt;EM&gt;dev_msc_ramdisk_freertos&lt;/EM&gt; instead. Or If you are getting issue with the&amp;nbsp;&lt;EM&gt;evkbmimxrt1060_dev_composite_cdc_msc_disk_freertos &lt;/EM&gt;please let me know more details so we could trouble shoot it!&lt;/P&gt;
&lt;P&gt;All the best,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Diego&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 23 May 2023 20:45:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1060-EVKB-USB-dev-composite-cdc-msc-disk-freertos-example/m-p/1656017#M206384</guid>
      <dc:creator>diego_charles</dc:creator>
      <dc:date>2023-05-23T20:45:57Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1060-EVKB USB dev_composite_cdc_msc_disk_freertos example</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1060-EVKB-USB-dev-composite-cdc-msc-disk-freertos-example/m-p/1658753#M206693</link>
      <description>&lt;P&gt;Thanks!&amp;nbsp; &amp;nbsp;Yes, I was relying on the pop-up description you captured above that indicated that it would create a RAMdisk.&amp;nbsp; &amp;nbsp;Since I was looking for a composite example with a RAMdisk,&amp;nbsp; I thought it would be the perfect example.&amp;nbsp; &amp;nbsp; I did find the example you mentioned and found it worked.&amp;nbsp; &amp;nbsp;Now to try to figure out how to access the same space from the MIMXRT1060 side (as a file?) so data can be transferred easily.&amp;nbsp; &amp;nbsp;Thanks again!&lt;/P&gt;</description>
      <pubDate>Sun, 28 May 2023 14:32:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1060-EVKB-USB-dev-composite-cdc-msc-disk-freertos-example/m-p/1658753#M206693</guid>
      <dc:creator>CktDesigner</dc:creator>
      <dc:date>2023-05-28T14:32:31Z</dc:date>
    </item>
  </channel>
</rss>