<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 i.MX RT Series Boot Loader</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-RT-Series-Boot-Loader/m-p/1653178#M206121</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using K66 and KV58 for our controller.&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) I was told that NXP is going to update i.MX RT series instead of K and KV series. I want to starting develop our controller based on i.MX RT series.&lt;/P&gt;&lt;P&gt;2) Can anybody recommend MCU in RT series to replace K66, and KV?&lt;/P&gt;&lt;P&gt;For K66, I am using 32M SDRAM, 32M NOR flash, network, CANBUS, and etc...No LCD, camera interafces.&lt;/P&gt;&lt;P&gt;For KV58, I am using it to control 2 BLDCs+1D.&lt;/P&gt;&lt;P&gt;RT1050/1060/1064 will be a good fit? How about availability?&lt;/P&gt;&lt;P&gt;3) I am building boot-loader for K66 over USB and Network to write my application to internal flash. Can I do the same on RT series. Because I see there is flash loader in ROM that can't be changed, can you tell me how to do it? Do I need to build my own boot-loader in external flash, then load my application?&lt;/P&gt;&lt;P&gt;4)&amp;nbsp;I am building boot-loader for KV58 over CANBUS to&amp;nbsp;write my application to internal flash. Can I do the same on RT series. Because I see there is flash loader in ROM that can't be changed, can you tell me how to do it? Do I need to build my own boot-loader in external flash, then load my application?&lt;/P&gt;&lt;P&gt;5) RT 1050/1060/1064 are exchangeable on hardware level? What do I need to change?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;</description>
    <pubDate>Thu, 18 May 2023 14:14:40 GMT</pubDate>
    <dc:creator>a8Chcx</dc:creator>
    <dc:date>2023-05-18T14:14:40Z</dc:date>
    <item>
      <title>i.MX RT Series Boot Loader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-RT-Series-Boot-Loader/m-p/1653178#M206121</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using K66 and KV58 for our controller.&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) I was told that NXP is going to update i.MX RT series instead of K and KV series. I want to starting develop our controller based on i.MX RT series.&lt;/P&gt;&lt;P&gt;2) Can anybody recommend MCU in RT series to replace K66, and KV?&lt;/P&gt;&lt;P&gt;For K66, I am using 32M SDRAM, 32M NOR flash, network, CANBUS, and etc...No LCD, camera interafces.&lt;/P&gt;&lt;P&gt;For KV58, I am using it to control 2 BLDCs+1D.&lt;/P&gt;&lt;P&gt;RT1050/1060/1064 will be a good fit? How about availability?&lt;/P&gt;&lt;P&gt;3) I am building boot-loader for K66 over USB and Network to write my application to internal flash. Can I do the same on RT series. Because I see there is flash loader in ROM that can't be changed, can you tell me how to do it? Do I need to build my own boot-loader in external flash, then load my application?&lt;/P&gt;&lt;P&gt;4)&amp;nbsp;I am building boot-loader for KV58 over CANBUS to&amp;nbsp;write my application to internal flash. Can I do the same on RT series. Because I see there is flash loader in ROM that can't be changed, can you tell me how to do it? Do I need to build my own boot-loader in external flash, then load my application?&lt;/P&gt;&lt;P&gt;5) RT 1050/1060/1064 are exchangeable on hardware level? What do I need to change?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;</description>
      <pubDate>Thu, 18 May 2023 14:14:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-RT-Series-Boot-Loader/m-p/1653178#M206121</guid>
      <dc:creator>a8Chcx</dc:creator>
      <dc:date>2023-05-18T14:14:40Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX RT Series Boot Loader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-RT-Series-Boot-Loader/m-p/1653338#M206132</link>
      <description>&lt;P&gt;Hello, my name is Pavel, and I will be supporting your case, let me get into your case and when I have more information, I will contact you.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Thu, 18 May 2023 21:34:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-RT-Series-Boot-Loader/m-p/1653338#M206132</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2023-05-18T21:34:41Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX RT Series Boot Loader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-RT-Series-Boot-Loader/m-p/1655095#M206297</link>
      <description>&lt;P&gt;Hello, I review the information on the RT1064, and this could be a good option.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-left" image-alt="Pavel_Hernandez_0-1684801603271.png" style="width: 200px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/224293i733B12B5B75F138E/image-size/small?v=v2&amp;amp;px=200" role="button" title="Pavel_Hernandez_0-1684801603271.png" alt="Pavel_Hernandez_0-1684801603271.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Tue, 23 May 2023 00:27:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-RT-Series-Boot-Loader/m-p/1655095#M206297</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2023-05-23T00:27:32Z</dc:date>
    </item>
  </channel>
</rss>