<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Create an image with torch 2.0 or above</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Create-an-image-with-torch-2-0-or-above/m-p/1652961#M206093</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/192970"&gt;@Harvey021&lt;/a&gt;&lt;/P&gt;&lt;P&gt;Thanks for your response.&lt;/P&gt;&lt;P&gt;Is there a release date?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Sho&lt;/P&gt;</description>
    <pubDate>Thu, 18 May 2023 08:29:47 GMT</pubDate>
    <dc:creator>Sho_1</dc:creator>
    <dc:date>2023-05-18T08:29:47Z</dc:date>
    <item>
      <title>Create an image with torch 2.0 or above</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Create-an-image-with-torch-2-0-or-above/m-p/1648526#M205673</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I need to create an image with torch 2.0 or above, using the demo in &lt;A href="https://github.com/nxp-imx/meta-imx" target="_self"&gt;nxp-github&lt;/A&gt; I can&amp;nbsp; create image with torch 1.9.1post2 using&amp;nbsp;&lt;U&gt;&lt;EM&gt;Yocto Project BSP 6.1.1_1.0.0 Release.&amp;nbsp;&lt;/EM&gt;&lt;/U&gt;&lt;/P&gt;&lt;P&gt;Can I change line:9 in &lt;A href="https://github.com/nxp-imx/meta-imx/blob/langdale-6.1.1-1.0.0/meta-ml/recipes-libraries/pytorch/pytorch_git.bb" target="_self"&gt;python_git.bb&lt;/A&gt; file such that torch 2.0 will be install? or I must do it in other way? How?&lt;/P&gt;&lt;P&gt;Appreciate any help,&amp;nbsp;&lt;/P&gt;&lt;P&gt;# IMX8M&lt;/P&gt;&lt;P&gt;&lt;LI-PRODUCT title="IMX8MPLUS" id="IMX8MPLUS"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 11 May 2023 09:14:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Create-an-image-with-torch-2-0-or-above/m-p/1648526#M205673</guid>
      <dc:creator>Sho_1</dc:creator>
      <dc:date>2023-05-11T09:14:25Z</dc:date>
    </item>
    <item>
      <title>Re: Create an image with torch 2.0 or above</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Create-an-image-with-torch-2-0-or-above/m-p/1649877#M205836</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/193000"&gt;@Sho_1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The current release commit (&lt;SPAN&gt;SRCREV = "ef997d8f79877295e69e5cf34b524eea603c1fae"&lt;/SPAN&gt;) does not support for the 2.0 or above. Next release might support it.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Mon, 15 May 2023 03:42:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Create-an-image-with-torch-2-0-or-above/m-p/1649877#M205836</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2023-05-15T03:42:27Z</dc:date>
    </item>
    <item>
      <title>Re: Create an image with torch 2.0 or above</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Create-an-image-with-torch-2-0-or-above/m-p/1652961#M206093</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/192970"&gt;@Harvey021&lt;/a&gt;&lt;/P&gt;&lt;P&gt;Thanks for your response.&lt;/P&gt;&lt;P&gt;Is there a release date?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Sho&lt;/P&gt;</description>
      <pubDate>Thu, 18 May 2023 08:29:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Create-an-image-with-torch-2-0-or-above/m-p/1652961#M206093</guid>
      <dc:creator>Sho_1</dc:creator>
      <dc:date>2023-05-18T08:29:47Z</dc:date>
    </item>
    <item>
      <title>Re: Create an image with torch 2.0 or above</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Create-an-image-with-torch-2-0-or-above/m-p/1653064#M206106</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;As I know, will be Q2.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Thu, 18 May 2023 10:41:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Create-an-image-with-torch-2-0-or-above/m-p/1653064#M206106</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2023-05-18T10:41:17Z</dc:date>
    </item>
    <item>
      <title>Re: Create an image with torch 2.0 or above</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Create-an-image-with-torch-2-0-or-above/m-p/1710447#M211329</link>
      <description>Hi,&lt;BR /&gt;&lt;BR /&gt;Is there a new release date?&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;&lt;BR /&gt;Sho&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;</description>
      <pubDate>Thu, 24 Aug 2023 07:53:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Create-an-image-with-torch-2-0-or-above/m-p/1710447#M211329</guid>
      <dc:creator>Sho_1</dc:creator>
      <dc:date>2023-08-24T07:53:15Z</dc:date>
    </item>
    <item>
      <title>Re: Create an image with torch 2.0 or above</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Create-an-image-with-torch-2-0-or-above/m-p/1710448#M211330</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/192970"&gt;@Harvey021&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Is there a new release date?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Sho&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 24 Aug 2023 07:54:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Create-an-image-with-torch-2-0-or-above/m-p/1710448#M211330</guid>
      <dc:creator>Sho_1</dc:creator>
      <dc:date>2023-08-24T07:54:32Z</dc:date>
    </item>
  </channel>
</rss>