<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: u-boot default env i-MX8 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-default-env-i-MX8/m-p/1651703#M206001</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/217222"&gt;@jkavaiya&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can try "env default [-f] -a" in U-Boot prompt.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
    <pubDate>Wed, 17 May 2023 05:30:36 GMT</pubDate>
    <dc:creator>Harvey021</dc:creator>
    <dc:date>2023-05-17T05:30:36Z</dc:date>
    <item>
      <title>u-boot default env i-MX8</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-default-env-i-MX8/m-p/1649678#M205813</link>
      <description>&lt;P&gt;Is there a way to re-store default u-boot env? Like factory reset?&lt;/P&gt;&lt;P&gt;I messed up system looks like and its not booting anymore. My eMMC is unusable and not booting from SD. Thanks for help!!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;U-Boot SPL 2020.04-00022-g332c0bf3 (Apr 07 2022 - 15:57:48 +0000)
Training for 3GByte Micron
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3000MTS
Training FAILED
Re-training for 1GByte Samsung memory
DDRINFO: start DRAM init
DDRINFO: DRAM rate 4000MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
Normal Boot
Trying to boot from BOOTROM
image offset 0x8000, pagesize 0x200, ivt offset 0x0
NOTICE:  BL31: v2.2(release):rel_imx_5.4.70_2.3.0-0-gf1d7187f2
NOTICE:  BL31: Built : 10:39:24, Apr  4 2022


U-Boot 2020.04-00022-g332c0bf3 (Apr 07 2022 - 15:57:48 +0000)

CPU:   i.MX8MP[8] rev1.1 1800 MHz (running at 1200 MHz)
CPU:   Commercial temperature grade (0C to 95C) at 42C
Reset cause: POR
Model: NXP i.MX8MPlus LPDDR4 SolidRun board
DRAM:  1 GiB
MMC:   FSL_SDHC: 1, FSL_SDHC: 2
Loading Environment from MMC... OK
[*]-Video Link 0probe video device failed, ret -2

        [0] lcd-controller@32e80000, video
        [1] mipi_dsi@32e60000, video_bridge
        [2] adv7535@39, panel
probe video device failed, ret -2
In:    serial
Out:   serial
Err:   serial

 BuildInfo:
  - ATF f1d7187
  - U-Boot 2020.04-00022-g332c0bf3

switch to partitions #0, OK
mmc2(part 0) is current device
board_late_init: could not identify board, defaulting to HummingBoard Pulse Revision 2.5!
board_late_init: fdtfile set in environment, keeping as is.
flash target is MMC:2
Net:
Warning: ethernet@30bf0000 (eth1) using random MAC address - 62:b9:ee:7c:bd:77
eth1: ethernet@30bf0000 [PRIME]
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot:  0&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;u-boot=&amp;gt; mmc list
FSL_SDHC: 1
FSL_SDHC: 2 (eMMC)
u-boot=&amp;gt; mmc dev 1
switch to partitions #0, OK
mmc1 is current device
u-boot=&amp;gt; ls mmc 2:1
** Unrecognized filesystem type **&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 12 May 2023 23:56:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-default-env-i-MX8/m-p/1649678#M205813</guid>
      <dc:creator>jkavaiya</dc:creator>
      <dc:date>2023-05-12T23:56:36Z</dc:date>
    </item>
    <item>
      <title>Re: u-boot default env i-MX8</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-default-env-i-MX8/m-p/1651703#M206001</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/217222"&gt;@jkavaiya&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can try "env default [-f] -a" in U-Boot prompt.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Wed, 17 May 2023 05:30:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-default-env-i-MX8/m-p/1651703#M206001</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2023-05-17T05:30:36Z</dc:date>
    </item>
  </channel>
</rss>