<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.mx53 SATA link down (SStatus 0 SControl 300) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-mx53-SATA-link-down-SStatus-0-SControl-300/m-p/243042#M20596</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In reply to myself I swapped out the SSD and the new drive although a 1.5GHz than the original 3GHz sata works apparently correctly, so the drive had gone bad.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 29 Oct 2013 10:44:43 GMT</pubDate>
    <dc:creator>davee</dc:creator>
    <dc:date>2013-10-29T10:44:43Z</dc:date>
    <item>
      <title>i.mx53 SATA link down (SStatus 0 SControl 300)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx53-SATA-link-down-SStatus-0-SControl-300/m-p/243041#M20595</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;linux 2.6.35.3&lt;/P&gt;&lt;P&gt;i.mx53&lt;/P&gt;&lt;P&gt;kingston SSD 128GB sata&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've got a i.mx53 board based on the imx53qsb and i'm trying to use the SATA connection during boot up I see:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;scsi0 : ahci&lt;/P&gt;&lt;P&gt;ata1: SATA max UDMA/133 mmio [mem 0x10000000-0x10000fff] port 0x100 irq 28&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;then not long later it comes up with:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ata1: SATA link down (SStatus 0 SControl 300)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tried sending "0 0 0" to &lt;SPAN style="color: #2e8b57; font-family: Monaco, 'Andale Mono', 'Courier New', Courier, mono; font-size: 12px;"&gt;/sys/class/scsi_host/host0/scan&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #2e8b57; font-family: Monaco, 'Andale Mono', 'Courier New', Courier, mono; font-size: 12px;"&gt;which resulted in&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;ata1: hard resetting link&lt;/P&gt;&lt;P&gt;ata1: SATA link down (SStatus 0 SControl 300)&lt;/P&gt;&lt;P&gt;ata1: EH complete&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone aid me in tracking the problem down, the Google search results don't seems to resolve to anything?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Oct 2013 17:26:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx53-SATA-link-down-SStatus-0-SControl-300/m-p/243041#M20595</guid>
      <dc:creator>davee</dc:creator>
      <dc:date>2013-10-28T17:26:07Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx53 SATA link down (SStatus 0 SControl 300)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx53-SATA-link-down-SStatus-0-SControl-300/m-p/243042#M20596</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In reply to myself I swapped out the SSD and the new drive although a 1.5GHz than the original 3GHz sata works apparently correctly, so the drive had gone bad.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Oct 2013 10:44:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx53-SATA-link-down-SStatus-0-SControl-300/m-p/243042#M20596</guid>
      <dc:creator>davee</dc:creator>
      <dc:date>2013-10-29T10:44:43Z</dc:date>
    </item>
  </channel>
</rss>