<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Help with using the octal flash on RT1160-EVK</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Help-with-using-the-octal-flash-on-RT1160-EVK/m-p/1650955#M205927</link>
    <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I'm trying to use the octal flash on the RT1160-EVK without much success.&lt;/P&gt;&lt;P&gt;I modified the resistors on the board as outlined in the Board User Manual. Have set SW1 to 0010, and SW2 to 0010000000.&lt;/P&gt;&lt;P&gt;I'm using a modified version of the example project evkmimxrt1160_flexspi_nor_edma_transfer_cm7 to test this. Changed the flash config in evkmimxrt1160_flexspi_nor_config.c following examples from &lt;A href="https://community.nxp.com/t5/i-MX-RT/RT1170-EVK-Octal-Flash-not-usable/m-p/1249206" target="_blank"&gt;https://community.nxp.com/t5/i-MX-RT/RT1170-EVK-Octal-Flash-not-usable/m-p/1249206&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;The code compiles but never gets to main when I run it (see screenshot below):&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielberhe_0-1684225855347.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/223331iDAF5BE23CA66E73D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="danielberhe_0-1684225855347.png" alt="danielberhe_0-1684225855347.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Any idea where I'm going wrong? I've attached the MCUXpresso project.&lt;/P&gt;</description>
    <pubDate>Tue, 16 May 2023 08:35:29 GMT</pubDate>
    <dc:creator>danielberhe</dc:creator>
    <dc:date>2023-05-16T08:35:29Z</dc:date>
    <item>
      <title>Help with using the octal flash on RT1160-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Help-with-using-the-octal-flash-on-RT1160-EVK/m-p/1650955#M205927</link>
      <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I'm trying to use the octal flash on the RT1160-EVK without much success.&lt;/P&gt;&lt;P&gt;I modified the resistors on the board as outlined in the Board User Manual. Have set SW1 to 0010, and SW2 to 0010000000.&lt;/P&gt;&lt;P&gt;I'm using a modified version of the example project evkmimxrt1160_flexspi_nor_edma_transfer_cm7 to test this. Changed the flash config in evkmimxrt1160_flexspi_nor_config.c following examples from &lt;A href="https://community.nxp.com/t5/i-MX-RT/RT1170-EVK-Octal-Flash-not-usable/m-p/1249206" target="_blank"&gt;https://community.nxp.com/t5/i-MX-RT/RT1170-EVK-Octal-Flash-not-usable/m-p/1249206&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;The code compiles but never gets to main when I run it (see screenshot below):&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielberhe_0-1684225855347.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/223331iDAF5BE23CA66E73D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="danielberhe_0-1684225855347.png" alt="danielberhe_0-1684225855347.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Any idea where I'm going wrong? I've attached the MCUXpresso project.&lt;/P&gt;</description>
      <pubDate>Tue, 16 May 2023 08:35:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Help-with-using-the-octal-flash-on-RT1160-EVK/m-p/1650955#M205927</guid>
      <dc:creator>danielberhe</dc:creator>
      <dc:date>2023-05-16T08:35:29Z</dc:date>
    </item>
    <item>
      <title>Re: Help with using the octal flash on RT1160-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Help-with-using-the-octal-flash-on-RT1160-EVK/m-p/1651856#M206016</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/158341"&gt;@danielberhe&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;Don't worry, it is not difficult, please refer to my document, although it is for the RT1170, but RT1160 is the same situation:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/RT1170-Octal-flash-enablement/ta-p/1498369" target="_blank"&gt;https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/RT1170-Octal-flash-enablement/ta-p/1498369&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp; You can try it at first.&lt;/P&gt;
&lt;P&gt;If you meet any issues, please kindly let me know.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Kerry&lt;/P&gt;</description>
      <pubDate>Wed, 17 May 2023 07:53:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Help-with-using-the-octal-flash-on-RT1160-EVK/m-p/1651856#M206016</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2023-05-17T07:53:39Z</dc:date>
    </item>
    <item>
      <title>Re: Help with using the octal flash on RT1160-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Help-with-using-the-octal-flash-on-RT1160-EVK/m-p/1652130#M206043</link>
      <description>&lt;P&gt;Hi Kerry,&lt;/P&gt;&lt;P&gt;Thank you for the link.&lt;/P&gt;&lt;P&gt;I've had partial success following the document you linked. Running fsl_romapi from RAM appears to work and I was able to get the flash information. Although the the Erase sector and page program bits fail.&lt;/P&gt;&lt;P&gt;No luck with debugging hello world app from octal flash. I've modified the flexspi_nor_config_t to resemble what is in the linked document. I regenerated the cfx file to include the flash reset pin. Below is the console output:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;BR /&gt;MCUXpresso IDE RedlinkMulti Driver v11.7 (Mar 22 2023 09:52:55 - crt_emu_cm_redlink build 13)&lt;BR /&gt;Found chip XML file in C:/Users/danbb/hello/Debug\MIMXRT1166xxxxx.xml&lt;BR /&gt;( 5) Remote configuration complete&lt;BR /&gt;Reconnected to existing LinkServer process.&lt;BR /&gt;============= SCRIPT: RT1160_connect_M7_wake_M4.scp =============&lt;BR /&gt;RT1160 Connect M7 and Wake M4 Script&lt;BR /&gt;DpID = 6BA02477&lt;BR /&gt;APID = 0x84770001&lt;BR /&gt;Setting M4 spin code&lt;BR /&gt;Setting M4 clock&lt;BR /&gt;Resetting M4 core&lt;BR /&gt;Releasing M4&lt;BR /&gt;View cores on the DAP AP&lt;BR /&gt;DpID = 6BA02477&lt;BR /&gt;TAP 0: 6BA02477 Core 0: M7 APID: 84770001 ROM Table: E00FD003*&lt;BR /&gt;TAP 0: 6BA02477 Core 1: M4 APID: 24770011 ROM Table: E00FF003&lt;BR /&gt;============= END SCRIPT ========================================&lt;BR /&gt;Probe Firmware: CMSIS-DAP (ARM)&lt;BR /&gt;Serial Number: 02440000020b708200000000000000000000000097969905&lt;BR /&gt;VID:PID: 0D28:0204&lt;BR /&gt;USB Path: \\?\hid#vid_0d28&amp;amp;pid_0204&amp;amp;mi_03#9&amp;amp;369fd963&amp;amp;0&amp;amp;0000#{4d1e55b2-f16f-11cf-88cb-001111000030}&lt;BR /&gt;Using memory from core 0 after searching for a good core&lt;BR /&gt;debug interface type = CoreSight DP (DAP DP ID 6BA02477) over SWD TAP 0&lt;BR /&gt;processor type = Cortex-M7 (CPU ID 00000C27) on DAP AP 0&lt;BR /&gt;number of h/w breakpoints = 8&lt;BR /&gt;number of flash patches = 0&lt;BR /&gt;number of h/w watchpoints = 4&lt;BR /&gt;Probe(0): Connected&amp;amp;Reset. DpID: 6BA02477. CpuID: 00000C27. Info: &amp;lt;None&amp;gt;&lt;BR /&gt;Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.&lt;BR /&gt;Content of CoreSight Debug ROM(s):&lt;BR /&gt;RBASE E00FD000: CID B105100D PID 000008E88C ROM (type 0x1)&lt;BR /&gt;ROM 1 E00FE000: CID B105100D PID 04000BB4C8 ROM (type 0x1)&lt;BR /&gt;ROM 2 E00FF000: CID B105100D PID 04000BB4C7 ROM (type 0x1)&lt;BR /&gt;ROM 3 E000E000: CID B105E00D PID 04000BB00C Gen SCS (type 0x0)&lt;BR /&gt;ROM 3 E0001000: CID B105E00D PID 04000BB002 Gen DWT (type 0x0)&lt;BR /&gt;ROM 3 E0002000: CID B105E00D PID 04000BB00E Gen (type 0x0)&lt;BR /&gt;ROM 3 E0000000: CID B105E00D PID 04000BB001 Gen ITM (type 0x0)&lt;BR /&gt;ROM 2 E0041000: CID B105900D PID 04001BB975 CSt ARM ETMv4.0 type 0x13 Trace Source - Core&lt;BR /&gt;ROM 2 E0042000: CID B105900D PID 04004BB906 CSt type 0x14 Debug Control - Trigger, e.g. ECT&lt;BR /&gt;ROM 1 E0043000: CID B105900D PID 04001BB908 CSt CSTF type 0x12 Trace Link - Trace funnel/router&lt;BR /&gt;NXP: MIMXRT1166xxxxx&lt;BR /&gt;DAP stride is 1024 bytes (256 words)&lt;BR /&gt;Inspected v.2 External Flash Device on SPI using SFDP JEDEC ID C:\Users\danbb/iMXRT117x_FlexSPI_SFDP/builds/MIMXRT1160_SFDP_MXIC_OPI.cfx&lt;BR /&gt;Image 'iMXRT1170_SFDP_FlexSPI1_MXIC_OPI May 17 2023 10:35:18'&lt;BR /&gt;Opening flash driver C:\Users\danbb/iMXRT117x_FlexSPI_SFDP/builds/MIMXRT1160_SFDP_MXIC_OPI.cfx&lt;BR /&gt;Sending VECTRESET to run flash driver&lt;BR /&gt;flash driver polled mailbox (8 bytes at 0x2000A6D8) read failed (on poll 1/301) - retrying after 1ms - rc Em(12). Target rejected debug access at location 0x00000000&lt;BR /&gt;AFTER driver startup timeout (302 5ms retries)&lt;BR /&gt;Driver Addresses&lt;BR /&gt;Start: 20000000&lt;BR /&gt;Entry: 20000035&lt;BR /&gt;End: 200006C8&lt;BR /&gt;Stack: 200026C8&lt;BR /&gt;Mailbox:2000A6C8&lt;BR /&gt;Driver Register State&lt;BR /&gt;R0: 40CAC0B0&lt;BR /&gt;R1: 0A000000&lt;BR /&gt;R2: 80000000&lt;BR /&gt;R3: 0000F000&lt;BR /&gt;R4: E000ED00&lt;BR /&gt;R5: 0022946D&lt;BR /&gt;R6: 001640CD&lt;BR /&gt;R7: 00207DC8&lt;BR /&gt;R8: 2024AE80&lt;BR /&gt;R9: 2024AE84&lt;BR /&gt;R10: 00211C0C&lt;BR /&gt;R11: 000000F0&lt;BR /&gt;R12: 00000000&lt;BR /&gt;SP: 20241D98&lt;BR /&gt;LR: 002015F3&lt;BR /&gt;PC: 00223104&lt;BR /&gt;xPSR: 81000000&lt;BR /&gt;MSP: 20241D98&lt;BR /&gt;PSP: 00000000&lt;BR /&gt;CFBP: 00000001 (CONTROL=0x0, FAULTMASK=0x0, BASEPRI=0x0, PRIMASK=0x1)&lt;BR /&gt;Flash Driver V.2 startup failed - rc Ef(34): Timed-out initializing flash.&lt;BR /&gt;chip initialization failed - Ef(34): Timed-out initializing flash.&lt;BR /&gt;failed to initialize flash driver C:\Users\danbb/iMXRT117x_FlexSPI_SFDP/builds/MIMXRT1160_SFDP_MXIC_OPI.cfx&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Wed, 17 May 2023 13:53:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Help-with-using-the-octal-flash-on-RT1160-EVK/m-p/1652130#M206043</guid>
      <dc:creator>danielberhe</dc:creator>
      <dc:date>2023-05-17T13:53:02Z</dc:date>
    </item>
    <item>
      <title>Re: Help with using the octal flash on RT1160-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Help-with-using-the-octal-flash-on-RT1160-EVK/m-p/1652761#M206083</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/158341"&gt;@danielberhe&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;Which debugger you are using now?&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp; As you also need the related flashloader file, different debugger is using the different flashloader.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp; CMSIS DAP is using the .cfx,&amp;nbsp; JLINK, I suggest you use the RT-UFL.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;If you use the .cfx, do you try my chapter&amp;nbsp;&lt;STRONG&gt;4. CMSIS DAP Flashloader&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp; Do you generate the .cfx file again?&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Kerry&lt;/P&gt;</description>
      <pubDate>Thu, 18 May 2023 04:54:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Help-with-using-the-octal-flash-on-RT1160-EVK/m-p/1652761#M206083</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2023-05-18T04:54:49Z</dc:date>
    </item>
    <item>
      <title>Re: Help with using the octal flash on RT1160-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Help-with-using-the-octal-flash-on-RT1160-EVK/m-p/1653036#M206102</link>
      <description>&lt;P&gt;Hi Kerry,&lt;/P&gt;&lt;P&gt;I'm using the DAP flashloader and yes, I did follow section 4 of the document and regenerated the .cfx. I then used that .cfx by updating my project in properties-&amp;gt;C/C++ Build-&amp;gt;MCU settings.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Thu, 18 May 2023 10:02:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Help-with-using-the-octal-flash-on-RT1160-EVK/m-p/1653036#M206102</guid>
      <dc:creator>danielberhe</dc:creator>
      <dc:date>2023-05-18T10:02:48Z</dc:date>
    </item>
    <item>
      <title>Re: Help with using the octal flash on RT1160-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Help-with-using-the-octal-flash-on-RT1160-EVK/m-p/1653468#M206141</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/158341"&gt;@danielberhe&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; Share your modified .cfx to me, when I have time, I will test it on my side.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;BTW, you can modify your on board EVK debugger to the JLINK, then try the RT-UFL, whether that method works or not?&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;You can firmware the on board debugger to JLINK with the LPCScrypt:&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;&lt;A href="https://www.nxp.com/lpcscrypt" target="_blank"&gt;https://www.nxp.com/lpcscrypt&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;Please try it on your side, the RT-UFL, you can use my doc mentioned file.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Kerry&lt;/P&gt;</description>
      <pubDate>Fri, 19 May 2023 03:19:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Help-with-using-the-octal-flash-on-RT1160-EVK/m-p/1653468#M206141</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2023-05-19T03:19:59Z</dc:date>
    </item>
    <item>
      <title>Re: Help with using the octal flash on RT1160-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Help-with-using-the-octal-flash-on-RT1160-EVK/m-p/2090485#M236864</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/60336"&gt;@kerryzhou&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;I been trying to do the same with the rt600 on a custom evk runnning on flexspi port A Octal.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;By following your note on the rt1170, I was able to get to the point where in the IDE seems to do a successful operation when I flash it with the RT UFL algo. But is not actually flashing.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Also, I get this error when I try to erase memory with j-commander :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="skanda19_0-1746050766259.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/335918i1D61555C8A74BB9C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="skanda19_0-1746050766259.png" alt="skanda19_0-1746050766259.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;To what I believe is that RT algorithm needs to support octal and I need to enable it. Can you give some detail on how to do this with the rt600 ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 30 Apr 2025 22:07:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Help-with-using-the-octal-flash-on-RT1160-EVK/m-p/2090485#M236864</guid>
      <dc:creator>skanda19</dc:creator>
      <dc:date>2025-04-30T22:07:50Z</dc:date>
    </item>
  </channel>
</rss>