<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: caam-keygen source code for iMX8</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/caam-keygen-source-code-for-iMX8/m-p/1647343#M205547</link>
    <description>&lt;P&gt;Hi Harvey,&lt;/P&gt;&lt;P&gt;Thank you for giving me the link for caam-keygen utility!&amp;nbsp; I was able to download the files and to build the utility successfully for the Toradex Apalis-iMX8 dev kit that I've been using.&amp;nbsp; After I transferred the utility to the embedded linux running on the dev kit, I was able to execute the steps successfully in the app note for encrypting and decrypting data with DM-Crypt and CAAM.&amp;nbsp; The app note I've been using is&amp;nbsp;AN12714,&lt;BR /&gt;i.MX Encrypted Storage Using CAAM Secure Keys Rev 2.&lt;/P&gt;&lt;P&gt;Thanks Again!!&lt;/P&gt;&lt;P&gt;Rick&lt;/P&gt;</description>
    <pubDate>Tue, 09 May 2023 18:37:27 GMT</pubDate>
    <dc:creator>nxpuser_rb</dc:creator>
    <dc:date>2023-05-09T18:37:27Z</dc:date>
    <item>
      <title>caam-keygen source code for iMX8</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/caam-keygen-source-code-for-iMX8/m-p/1645794#M205358</link>
      <description>&lt;P&gt;Does anyone have an active link to the source code for the caam-keygen source code?&amp;nbsp; I have a version of yocto embedded linux from Toradex that I built for the Apalis iMX8QM module.&amp;nbsp; It runs successfully on the Toradex dev kit for the IXORA carrier board with the Apalis iMX8.&amp;nbsp; I can load manually the linux modules required for dm-crypt, dm-mod, and trusted.&amp;nbsp; The command "dmsetup targets" lists crypt. I can successfully follow the instructions in the i.MX Linux User's guide to encrypt/decrypt data on non-volatile storage using a CAAM trusted plain key, but the bsp does not include the utility caam-keygen utility required for encryption using CAAM tagged keys.&lt;/P&gt;&lt;P&gt;Can someone give the source for the caam-keygen utility?&amp;nbsp; I have the arm cross compiler for the bsp, so I could build the utility separately and install it on the board.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 06 May 2023 01:14:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/caam-keygen-source-code-for-iMX8/m-p/1645794#M205358</guid>
      <dc:creator>nxpuser_rb</dc:creator>
      <dc:date>2023-05-06T01:14:56Z</dc:date>
    </item>
    <item>
      <title>Re: caam-keygen source code for iMX8</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/caam-keygen-source-code-for-iMX8/m-p/1645902#M205370</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/216672"&gt;@nxpuser_rb&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can find the source from the link:&amp;nbsp;&lt;A href="https://github.com/nxp-imx/keyctl_caam" target="_blank"&gt;GitHub - nxp-imx/keyctl_caam: Keyctl CAAM Security&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Sat, 06 May 2023 07:53:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/caam-keygen-source-code-for-iMX8/m-p/1645902#M205370</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2023-05-06T07:53:21Z</dc:date>
    </item>
    <item>
      <title>Re: caam-keygen source code for iMX8</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/caam-keygen-source-code-for-iMX8/m-p/1647343#M205547</link>
      <description>&lt;P&gt;Hi Harvey,&lt;/P&gt;&lt;P&gt;Thank you for giving me the link for caam-keygen utility!&amp;nbsp; I was able to download the files and to build the utility successfully for the Toradex Apalis-iMX8 dev kit that I've been using.&amp;nbsp; After I transferred the utility to the embedded linux running on the dev kit, I was able to execute the steps successfully in the app note for encrypting and decrypting data with DM-Crypt and CAAM.&amp;nbsp; The app note I've been using is&amp;nbsp;AN12714,&lt;BR /&gt;i.MX Encrypted Storage Using CAAM Secure Keys Rev 2.&lt;/P&gt;&lt;P&gt;Thanks Again!!&lt;/P&gt;&lt;P&gt;Rick&lt;/P&gt;</description>
      <pubDate>Tue, 09 May 2023 18:37:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/caam-keygen-source-code-for-iMX8/m-p/1647343#M205547</guid>
      <dc:creator>nxpuser_rb</dc:creator>
      <dc:date>2023-05-09T18:37:27Z</dc:date>
    </item>
  </channel>
</rss>