<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: DDR3 size in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/DDR3-size/m-p/1645049#M205284</link>
    <description>Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203368"&gt;@Manuel_Salas&lt;/a&gt;, Thanks for your answer,&lt;BR /&gt;So, I have another questions, same topic:&lt;BR /&gt;Is there a way to automatically detect different types of DDR3 in SPL/u-boot ?</description>
    <pubDate>Thu, 04 May 2023 23:09:56 GMT</pubDate>
    <dc:creator>Arm7</dc:creator>
    <dc:date>2023-05-04T23:09:56Z</dc:date>
    <item>
      <title>DDR3 size</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR3-size/m-p/1644941#M205275</link>
      <description>&lt;P&gt;In the i.MX6 SOLO is there a way to read the size of the chip DDR3 ?&lt;/P&gt;</description>
      <pubDate>Thu, 04 May 2023 18:25:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR3-size/m-p/1644941#M205275</guid>
      <dc:creator>Arm7</dc:creator>
      <dc:date>2023-05-04T18:25:19Z</dc:date>
    </item>
    <item>
      <title>Re: DDR3 size</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR3-size/m-p/1644980#M205277</link>
      <description>&lt;P&gt;Hello!&lt;/P&gt;
&lt;P&gt;You can do it in U-boot with the command bdinfo.&lt;/P&gt;
&lt;P&gt;That command will show to you information about of the board, including the DRAM size.&lt;/P&gt;
&lt;P&gt;Look for "size" under of DRAM bank section.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope this can help to you.&lt;/P&gt;</description>
      <pubDate>Thu, 04 May 2023 19:49:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR3-size/m-p/1644980#M205277</guid>
      <dc:creator>Manuel_Salas</dc:creator>
      <dc:date>2023-05-04T19:49:29Z</dc:date>
    </item>
    <item>
      <title>Re: DDR3 size</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR3-size/m-p/1645049#M205284</link>
      <description>Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203368"&gt;@Manuel_Salas&lt;/a&gt;, Thanks for your answer,&lt;BR /&gt;So, I have another questions, same topic:&lt;BR /&gt;Is there a way to automatically detect different types of DDR3 in SPL/u-boot ?</description>
      <pubDate>Thu, 04 May 2023 23:09:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR3-size/m-p/1645049#M205284</guid>
      <dc:creator>Arm7</dc:creator>
      <dc:date>2023-05-04T23:09:56Z</dc:date>
    </item>
    <item>
      <title>Re: DDR3 size</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR3-size/m-p/1645682#M205343</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/216780"&gt;@Arm7&lt;/a&gt;&amp;nbsp;,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Unfortunately, in U-boot that is not possible, but for IMX6 Solo the supported interfaces are 16/32-bit DDR3-800, and LV-DDR3-800.&lt;/P&gt;&lt;P&gt;Best regards!&lt;/P&gt;</description>
      <pubDate>Fri, 05 May 2023 17:53:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR3-size/m-p/1645682#M205343</guid>
      <dc:creator>Manuel_Salas</dc:creator>
      <dc:date>2023-05-05T17:53:43Z</dc:date>
    </item>
  </channel>
</rss>