<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic USB 3 Polarity Inversion TX and RX in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-3-Polarity-Inversion-TX-and-RX/m-p/1644318#M205215</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;according to the USB3 spec it is allowed to invert the polarity of the USB_TX or USB_RX signals without any further adjustments.&lt;/P&gt;&lt;P&gt;Since we got some issues with our USB-Interface where we inverted USB2_TX_N and USB2_TX_P as well as USB2_RX_N and USB2_RX_P, I want to make sure this is allowed with the i.MX8M Plus.&lt;/P&gt;&lt;P&gt;Can anybody confirm this inversion is possible and we do not have to adjust any settings or similar?&lt;/P&gt;&lt;P&gt;&lt;LI-PRODUCT title="IMX8MPLUS" id="IMX8MPLUS"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 04 May 2023 06:32:22 GMT</pubDate>
    <dc:creator>MNTR</dc:creator>
    <dc:date>2023-05-04T06:32:22Z</dc:date>
    <item>
      <title>USB 3 Polarity Inversion TX and RX</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-3-Polarity-Inversion-TX-and-RX/m-p/1644318#M205215</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;according to the USB3 spec it is allowed to invert the polarity of the USB_TX or USB_RX signals without any further adjustments.&lt;/P&gt;&lt;P&gt;Since we got some issues with our USB-Interface where we inverted USB2_TX_N and USB2_TX_P as well as USB2_RX_N and USB2_RX_P, I want to make sure this is allowed with the i.MX8M Plus.&lt;/P&gt;&lt;P&gt;Can anybody confirm this inversion is possible and we do not have to adjust any settings or similar?&lt;/P&gt;&lt;P&gt;&lt;LI-PRODUCT title="IMX8MPLUS" id="IMX8MPLUS"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 04 May 2023 06:32:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-3-Polarity-Inversion-TX-and-RX/m-p/1644318#M205215</guid>
      <dc:creator>MNTR</dc:creator>
      <dc:date>2023-05-04T06:32:22Z</dc:date>
    </item>
    <item>
      <title>Re: USB 3 Polarity Inversion TX and RX</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-3-Polarity-Inversion-TX-and-RX/m-p/1646312#M205430</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/216746"&gt;@MNTR&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;TX/RX polarity inversion is supported on i.MX8MP.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;USB 3.0&amp;nbsp;PHY has auto polarity detection and adjustment support.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Dhruvit Vasavada&lt;/P&gt;
&lt;DIV class="view-original-post-link"&gt;&amp;nbsp;&lt;/DIV&gt;</description>
      <pubDate>Mon, 08 May 2023 09:43:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-3-Polarity-Inversion-TX-and-RX/m-p/1646312#M205430</guid>
      <dc:creator>Dhruvit</dc:creator>
      <dc:date>2023-05-08T09:43:32Z</dc:date>
    </item>
    <item>
      <title>Re: USB 3 Polarity Inversion TX and RX</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-3-Polarity-Inversion-TX-and-RX/m-p/1646824#M205487</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201299"&gt;@Dhruvit&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;thank you very much.&amp;nbsp;&lt;BR /&gt;Are there any limitations?&amp;nbsp;&lt;BR /&gt;For example: can I invert just one of the super speed pairs (TX inverted, RX not inverted)?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Thanks in advance&lt;/P&gt;</description>
      <pubDate>Tue, 09 May 2023 06:24:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-3-Polarity-Inversion-TX-and-RX/m-p/1646824#M205487</guid>
      <dc:creator>MNTR</dc:creator>
      <dc:date>2023-05-09T06:24:14Z</dc:date>
    </item>
    <item>
      <title>Re: USB 3 Polarity Inversion TX and RX</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-3-Polarity-Inversion-TX-and-RX/m-p/1648631#M205690</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/216746"&gt;@MNTR&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;i.MX8MP has&amp;nbsp;Synopsys USB 3.0 PHY.&lt;/P&gt;
&lt;P&gt;Lane Polarity inversion only talks about Rx signals.&lt;/P&gt;
&lt;P&gt;Please refer to&amp;nbsp;Universal Serial Bus 3.0 Specification for more information.&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Dhruvit Vasavada&lt;/P&gt;</description>
      <pubDate>Thu, 11 May 2023 11:09:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-3-Polarity-Inversion-TX-and-RX/m-p/1648631#M205690</guid>
      <dc:creator>Dhruvit</dc:creator>
      <dc:date>2023-05-11T11:09:42Z</dc:date>
    </item>
  </channel>
</rss>