<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Config Tool Update causes DDR error</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Config-Tool-Update-causes-DDR-error/m-p/1644093#M205196</link>
    <description>&lt;P&gt;I've updated the Config Tools for i.MX to Version 13.1. The updated DDR tool now has a constant error "Failed to generate code" (see picture). Its says "tool problem" and offers no specific issue. Even when I create a new from scratch configuration, the same thing happens. If I change any setting, I get a 'not supported"&amp;nbsp; error. The CPU selected is MIMX8ML4xxxKZ. The Pin tools still works fine as far as I can tell. To reproduce, open the new, create a new config, select&amp;nbsp;MIMX8ML4xxxKZ. Go back and forth between pin tool and DDR tool a couple of times and/or do an "Update Code".&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ToolProblem.png" style="width: 856px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/221617i50031EFC546D2E2D/image-size/large?v=v2&amp;amp;px=999" role="button" title="ToolProblem.png" alt="ToolProblem.png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 04 May 2023 00:03:33 GMT</pubDate>
    <dc:creator>lcotten</dc:creator>
    <dc:date>2023-05-04T00:03:33Z</dc:date>
    <item>
      <title>Config Tool Update causes DDR error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Config-Tool-Update-causes-DDR-error/m-p/1644093#M205196</link>
      <description>&lt;P&gt;I've updated the Config Tools for i.MX to Version 13.1. The updated DDR tool now has a constant error "Failed to generate code" (see picture). Its says "tool problem" and offers no specific issue. Even when I create a new from scratch configuration, the same thing happens. If I change any setting, I get a 'not supported"&amp;nbsp; error. The CPU selected is MIMX8ML4xxxKZ. The Pin tools still works fine as far as I can tell. To reproduce, open the new, create a new config, select&amp;nbsp;MIMX8ML4xxxKZ. Go back and forth between pin tool and DDR tool a couple of times and/or do an "Update Code".&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ToolProblem.png" style="width: 856px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/221617i50031EFC546D2E2D/image-size/large?v=v2&amp;amp;px=999" role="button" title="ToolProblem.png" alt="ToolProblem.png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 04 May 2023 00:03:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Config-Tool-Update-causes-DDR-error/m-p/1644093#M205196</guid>
      <dc:creator>lcotten</dc:creator>
      <dc:date>2023-05-04T00:03:33Z</dc:date>
    </item>
    <item>
      <title>Re: Config Tool Update causes DDR error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Config-Tool-Update-causes-DDR-error/m-p/1644648#M205251</link>
      <description>&lt;P&gt;Please go to&amp;nbsp;C:\ProgramData\NXP\mcu_data_v13 and delete the processor folder. After that recreate the project from scratch.&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;</description>
      <pubDate>Thu, 04 May 2023 11:19:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Config-Tool-Update-causes-DDR-error/m-p/1644648#M205251</guid>
      <dc:creator>addiyi</dc:creator>
      <dc:date>2023-05-04T11:19:11Z</dc:date>
    </item>
    <item>
      <title>Re: Config Tool Update causes DDR error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Config-Tool-Update-causes-DDR-error/m-p/1644875#M205269</link>
      <description>&lt;P&gt;I tried that. It didn't work. So, I uninstalled the app, deleted the whole "mcu_data_v13" folder (kept a copy), and reinstalled. Then I created a new config, and the problem is fixed. I was then able to import all my pin settings. So, I think all is well now. One interesting note: even after a fresh reinstallation, when I create new configs, the DDR tool comes up with my swizzle already in it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there yet another badge for this? (kidding!)&lt;/P&gt;</description>
      <pubDate>Thu, 04 May 2023 16:34:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Config-Tool-Update-causes-DDR-error/m-p/1644875#M205269</guid>
      <dc:creator>lcotten</dc:creator>
      <dc:date>2023-05-04T16:34:08Z</dc:date>
    </item>
    <item>
      <title>Re: Config Tool Update causes DDR error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Config-Tool-Update-causes-DDR-error/m-p/1645510#M205327</link>
      <description>&lt;P&gt;You can check the Preset. If it is Custom then changes are applied to default configuration, otherwise it should show Default LPDDR4 Configuration.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="addiyi_0-1683286698723.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/221980i1BCE4A7841CC8C85/image-size/medium?v=v2&amp;amp;px=400" role="button" title="addiyi_0-1683286698723.png" alt="addiyi_0-1683286698723.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 05 May 2023 11:38:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Config-Tool-Update-causes-DDR-error/m-p/1645510#M205327</guid>
      <dc:creator>addiyi</dc:creator>
      <dc:date>2023-05-05T11:38:27Z</dc:date>
    </item>
  </channel>
</rss>