<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックExample LPUART DMA use?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Example-LPUART-DMA-use/m-p/1641845#M204989</link>
    <description>&lt;P&gt;I'm using RT1024 which has nice full-function LPUARTs. I need to receive characters via DMA with a completion interrupt on &lt;U&gt;either&lt;/U&gt; (inactivity and data received) &lt;U&gt;or&lt;/U&gt; (received data hits high-water mark or count). In the completion ISR/callback I'll transfer the received characters (into a FreeRTOS stream buffer) and do whatever is necessary to continue DMA input processing (toggling receive buffers if this is needed).&lt;/P&gt;&lt;P&gt;Is there an example that shows how to do this? Can it be done using one of the FSL drivers? Please note I do not want to use a ring buffer - just give me the data please.&lt;/P&gt;&lt;P&gt;Thanks in advance for any help,&lt;BR /&gt;Best Regards, Dave&lt;/P&gt;&lt;P&gt;PS: Next question will be DMA output, blocking til completion (sending output lines from a queue).&lt;/P&gt;</description>
    <pubDate>Thu, 27 Apr 2023 23:59:20 GMT</pubDate>
    <dc:creator>davenadler</dc:creator>
    <dc:date>2023-04-27T23:59:20Z</dc:date>
    <item>
      <title>Example LPUART DMA use?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Example-LPUART-DMA-use/m-p/1641845#M204989</link>
      <description>&lt;P&gt;I'm using RT1024 which has nice full-function LPUARTs. I need to receive characters via DMA with a completion interrupt on &lt;U&gt;either&lt;/U&gt; (inactivity and data received) &lt;U&gt;or&lt;/U&gt; (received data hits high-water mark or count). In the completion ISR/callback I'll transfer the received characters (into a FreeRTOS stream buffer) and do whatever is necessary to continue DMA input processing (toggling receive buffers if this is needed).&lt;/P&gt;&lt;P&gt;Is there an example that shows how to do this? Can it be done using one of the FSL drivers? Please note I do not want to use a ring buffer - just give me the data please.&lt;/P&gt;&lt;P&gt;Thanks in advance for any help,&lt;BR /&gt;Best Regards, Dave&lt;/P&gt;&lt;P&gt;PS: Next question will be DMA output, blocking til completion (sending output lines from a queue).&lt;/P&gt;</description>
      <pubDate>Thu, 27 Apr 2023 23:59:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Example-LPUART-DMA-use/m-p/1641845#M204989</guid>
      <dc:creator>davenadler</dc:creator>
      <dc:date>2023-04-27T23:59:20Z</dc:date>
    </item>
    <item>
      <title>Re: Example LPUART DMA use?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Example-LPUART-DMA-use/m-p/1642047#M205014</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/132425"&gt;@davenadler&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;To the RT UART DMA, please refer to our application note:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12679.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12679.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;The code is:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note-software/AN12679SW.zip" target="_blank"&gt;https://www.nxp.com/docs/en/application-note-software/AN12679SW.zip&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;This works perfect.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please check it at first.&lt;/P&gt;
&lt;P&gt;If you still have issues about it, just kindly let me know.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Kerry&lt;/P&gt;</description>
      <pubDate>Fri, 28 Apr 2023 07:00:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Example-LPUART-DMA-use/m-p/1642047#M205014</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2023-04-28T07:00:14Z</dc:date>
    </item>
  </channel>
</rss>