<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX8M Mini: VPU H1 Encoder image down-scaling not supported? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-VPU-H1-Encoder-image-down-scaling-not-supported/m-p/1641609#M204970</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;No sorry, it won;t work.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Thu, 27 Apr 2023 13:02:19 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2023-04-27T13:02:19Z</dc:date>
    <item>
      <title>i.MX8M Mini: VPU H1 Encoder image down-scaling not supported?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-VPU-H1-Encoder-image-down-scaling-not-supported/m-p/1641559#M204959</link>
      <description>&lt;P&gt;I am trying to use the image down-scaler on the i.MX8M Mini prior to encoding video to H.264 with the H1.&lt;/P&gt;&lt;P&gt;However function &lt;SPAN&gt;EWLReadAsicConfig&lt;/SPAN&gt;() returns &lt;SPAN&gt;cfg_info&lt;/SPAN&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;SPAN&gt;scalingEnabled set to EWL_HW_CONFIG_NOT_SUPPORTED, implying it is not supported!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Page 4759 of the Ref Manual Rev. 3, 11/2020 states that the preprocessing block is able to do Image down-scaling using a "Proprietary averaging filter".&lt;/P&gt;&lt;P&gt;The manual state above that the pre-processing is pipelined with the encoder and can oly be used with the H1. This is exactly my use case.&lt;/P&gt;&lt;P&gt;The datasheet (IMX8MMCEC) does not make any mention of the down-scaling being disabled on some i.XM8M Mini and not others.&lt;/P&gt;&lt;P&gt;I have tried to ignore the &lt;SPAN&gt;scalingEnabled&lt;/SPAN&gt; flag in the imx-vpu-hantro library and set the scaledWidth and scaledHeight variables anyway, but the image is not down-scaled.&lt;/P&gt;&lt;P&gt;Can you please confirm whether the down-scaling works with the H1 on the i.MX8M Mini?&lt;/P&gt;</description>
      <pubDate>Thu, 27 Apr 2023 12:00:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-VPU-H1-Encoder-image-down-scaling-not-supported/m-p/1641559#M204959</guid>
      <dc:creator>vincentz63</dc:creator>
      <dc:date>2023-04-27T12:00:21Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M Mini: VPU H1 Encoder image down-scaling not supported?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-VPU-H1-Encoder-image-down-scaling-not-supported/m-p/1641609#M204970</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;No sorry, it won;t work.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 27 Apr 2023 13:02:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-VPU-H1-Encoder-image-down-scaling-not-supported/m-p/1641609#M204970</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2023-04-27T13:02:19Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M Mini: VPU H1 Encoder image down-scaling not supported?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-VPU-H1-Encoder-image-down-scaling-not-supported/m-p/1641614#M204972</link>
      <description>&lt;P&gt;Can you elaborate? Is the documentation wrong? Is there a bug in the ASIC? Any workaround?&lt;/P&gt;</description>
      <pubDate>Thu, 27 Apr 2023 13:16:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-VPU-H1-Encoder-image-down-scaling-not-supported/m-p/1641614#M204972</guid>
      <dc:creator>vincentz63</dc:creator>
      <dc:date>2023-04-27T13:16:23Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M Mini: VPU H1 Encoder image down-scaling not supported?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-VPU-H1-Encoder-image-down-scaling-not-supported/m-p/1642933#M205125</link>
      <description>&lt;P&gt;Could you please provide more details? Is there a workaround or another solution?&lt;/P&gt;&lt;P&gt;I guess the next best thing is to use the 3D GPU? Any comment? If so, can you provide guidance to make use of it in the context of a GStreamer app that needs lowest possible latency?&lt;/P&gt;</description>
      <pubDate>Fri, 05 May 2023 07:58:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-VPU-H1-Encoder-image-down-scaling-not-supported/m-p/1642933#M205125</guid>
      <dc:creator>vincentz63</dc:creator>
      <dc:date>2023-05-05T07:58:49Z</dc:date>
    </item>
  </channel>
</rss>