<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX6 OTP Register programming with TRACE32 script via Lauterbach</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-OTP-Register-programming-with-TRACE32-script-via-Lauterbach/m-p/1641591#M204965</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm a beginner in the IMX6 debugging with Trace32 software.&lt;/P&gt;&lt;P&gt;The connection works with IMX6 processor.&lt;/P&gt;&lt;P&gt;I tried to read out the OTP registers with the TRACE32 sample script&lt;/P&gt;&lt;P&gt;but the following error message generated:&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF0000"&gt;bus error at address ANSD:0x21BC010&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;at the Data.Set command. See below.&lt;/P&gt;&lt;P&gt;&lt;FONT color="#3366FF"&gt;; first configure the timing parameters&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#3366FF"&gt;; the following values are valid after Reset&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#3366FF"&gt;Data.Set AD:&amp;amp;ocotpBase+0x10 %Long (0x5&amp;lt;&amp;lt;22.)|(6&amp;lt;&amp;lt;16.)|(0x1&amp;lt;&amp;lt;12.)|(0x299&amp;lt;&amp;lt;0.)&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;Could you please help me?&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 27 Apr 2023 12:43:16 GMT</pubDate>
    <dc:creator>blsoft</dc:creator>
    <dc:date>2023-04-27T12:43:16Z</dc:date>
    <item>
      <title>IMX6 OTP Register programming with TRACE32 script via Lauterbach</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-OTP-Register-programming-with-TRACE32-script-via-Lauterbach/m-p/1641591#M204965</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm a beginner in the IMX6 debugging with Trace32 software.&lt;/P&gt;&lt;P&gt;The connection works with IMX6 processor.&lt;/P&gt;&lt;P&gt;I tried to read out the OTP registers with the TRACE32 sample script&lt;/P&gt;&lt;P&gt;but the following error message generated:&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF0000"&gt;bus error at address ANSD:0x21BC010&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;at the Data.Set command. See below.&lt;/P&gt;&lt;P&gt;&lt;FONT color="#3366FF"&gt;; first configure the timing parameters&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#3366FF"&gt;; the following values are valid after Reset&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#3366FF"&gt;Data.Set AD:&amp;amp;ocotpBase+0x10 %Long (0x5&amp;lt;&amp;lt;22.)|(6&amp;lt;&amp;lt;16.)|(0x1&amp;lt;&amp;lt;12.)|(0x299&amp;lt;&amp;lt;0.)&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;Could you please help me?&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 27 Apr 2023 12:43:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-OTP-Register-programming-with-TRACE32-script-via-Lauterbach/m-p/1641591#M204965</guid>
      <dc:creator>blsoft</dc:creator>
      <dc:date>2023-04-27T12:43:16Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 OTP Register programming with TRACE32 script via Lauterbach</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-OTP-Register-programming-with-TRACE32-script-via-Lauterbach/m-p/1641855#M204990</link>
      <description>&lt;P&gt;pls refer to the enclosed application note&lt;/P&gt;</description>
      <pubDate>Fri, 28 Apr 2023 00:48:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-OTP-Register-programming-with-TRACE32-script-via-Lauterbach/m-p/1641855#M204990</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-04-28T00:48:34Z</dc:date>
    </item>
  </channel>
</rss>