<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Issue with RTC on imx8mm in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Issue-with-RTC-on-imx8mm/m-p/1638855#M204697</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201299"&gt;@Dhruvit&lt;/a&gt;&amp;nbsp;,&lt;BR /&gt;Thanks for the suggestion.&lt;BR /&gt;&lt;BR /&gt;Linked&amp;nbsp; RTC with system clock using hwclock command.&lt;BR /&gt;&lt;BR /&gt;When i try the below command to set alarm&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;echo +15 &amp;gt; /sys/class/rtc/rtc0/wakealarm&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;I can see the alarm being set,&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;nitrogen8mm:/ # cat /proc/driver/rtc                                                                                                                                                                         
rtc_time	: 11:10:25
rtc_date	: 2023-04-20
alrm_time	: 11:10:36
alrm_date	: 2023-04-20
alarm_IRQ	: yes
alrm_pending	: no
update IRQ enabled	: no
periodic IRQ enabled	: no
periodic IRQ frequency	: 1
max user IRQ frequency	: 64
24hr		: yes&lt;/LI-CODE&gt;&lt;P&gt;but when i set from the alarm application, alarm IRQ is always 'no' and the alarm time doesnt change&lt;/P&gt;</description>
    <pubDate>Mon, 24 Apr 2023 10:21:56 GMT</pubDate>
    <dc:creator>ashikp6</dc:creator>
    <dc:date>2023-04-24T10:21:56Z</dc:date>
    <item>
      <title>Issue with RTC on imx8mm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-with-RTC-on-imx8mm/m-p/1636264#M204452</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;I am using custom board based on imx8mm with android 11.&lt;BR /&gt;&lt;BR /&gt;When i use the Google desk clock application i dont see the RTC apis from drivers being called. Also the board doesnt come back from deep sleep(suspend) when the alarm triggered, even though the alarm is expected to bring the board to wakeup.&lt;BR /&gt;(Same application i have tried on my mobile phone and i am able to see the board coming out from suspend and showing the alarm notification)&lt;BR /&gt;&lt;BR /&gt;We are using only the internal RTC.&lt;BR /&gt;DTS used is,&lt;BR /&gt;snvs_rtc&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;snvs_rtc: snvs-rtc-lp {
                    compatible = "fsl,sec-v4.0-mon-rtc-lp";
                    regmap = &amp;lt;&amp;amp;snvs&amp;gt;;
                    offset = &amp;lt;0x34&amp;gt;;
                    interrupts = &amp;lt;GIC_SPI 19 IRQ_TYPE_LEVEL_HIGH&amp;gt;,
                             &amp;lt;GIC_SPI 20 IRQ_TYPE_LEVEL_HIGH&amp;gt;;
                    clocks = &amp;lt;&amp;amp;clk IMX8MM_CLK_SNVS_ROOT&amp;gt;;
                    clock-names = "snvs-rtc";
                };&lt;/LI-CODE&gt;&lt;P&gt;&lt;BR /&gt;Also tried using the following commands,&lt;BR /&gt;&amp;nbsp;&lt;I&gt;&lt;SPAN&gt;echo +15 &amp;gt; /sys/class/rtc/rtc0/wakealarm&lt;/SPAN&gt;&lt;/I&gt;&lt;BR /&gt;&lt;I&gt;&lt;SPAN&gt;echo mem &amp;gt; /sys/power/state&lt;/SPAN&gt;&lt;/I&gt;&lt;BR /&gt;In this scenario board goes to suspend and wakes up after 15s and i am seeing the RTC driver prints.&lt;BR /&gt;&lt;BR /&gt;Why is the application not able to use rtc driver and trigger the interrupt to wake up the board ?&lt;BR /&gt;Thanks,&lt;BR /&gt;Ashik&lt;/P&gt;</description>
      <pubDate>Wed, 19 Apr 2023 12:20:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-with-RTC-on-imx8mm/m-p/1636264#M204452</guid>
      <dc:creator>ashikp6</dc:creator>
      <dc:date>2023-04-19T12:20:34Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with RTC on imx8mm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-with-RTC-on-imx8mm/m-p/1637226#M204519</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/207638"&gt;@ashikp6&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;This issue could be due to the&amp;nbsp;&lt;SPAN&gt;Google desk clock application not using the correct RTC.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;One can refer to the below-mentioned document to debug further.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://developer.android.com/training/scheduling/alarms" target="_self"&gt;&lt;STRONG&gt;Schedule alarms&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Please sync RTC with the system clock using below command.&lt;/P&gt;
&lt;P&gt;#&lt;STRONG&gt;hwclock -w&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;One can monitor alarm interrupts using the below command.&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt; # cat /proc/driver/rtc&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;Please share the output of the above command after setting alarm.&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Dhruvit Vasavada&lt;/P&gt;</description>
      <pubDate>Thu, 20 Apr 2023 11:15:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-with-RTC-on-imx8mm/m-p/1637226#M204519</guid>
      <dc:creator>Dhruvit</dc:creator>
      <dc:date>2023-04-20T11:15:13Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with RTC on imx8mm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-with-RTC-on-imx8mm/m-p/1638855#M204697</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201299"&gt;@Dhruvit&lt;/a&gt;&amp;nbsp;,&lt;BR /&gt;Thanks for the suggestion.&lt;BR /&gt;&lt;BR /&gt;Linked&amp;nbsp; RTC with system clock using hwclock command.&lt;BR /&gt;&lt;BR /&gt;When i try the below command to set alarm&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;echo +15 &amp;gt; /sys/class/rtc/rtc0/wakealarm&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;I can see the alarm being set,&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;nitrogen8mm:/ # cat /proc/driver/rtc                                                                                                                                                                         
rtc_time	: 11:10:25
rtc_date	: 2023-04-20
alrm_time	: 11:10:36
alrm_date	: 2023-04-20
alarm_IRQ	: yes
alrm_pending	: no
update IRQ enabled	: no
periodic IRQ enabled	: no
periodic IRQ frequency	: 1
max user IRQ frequency	: 64
24hr		: yes&lt;/LI-CODE&gt;&lt;P&gt;but when i set from the alarm application, alarm IRQ is always 'no' and the alarm time doesnt change&lt;/P&gt;</description>
      <pubDate>Mon, 24 Apr 2023 10:21:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-with-RTC-on-imx8mm/m-p/1638855#M204697</guid>
      <dc:creator>ashikp6</dc:creator>
      <dc:date>2023-04-24T10:21:56Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with RTC on imx8mm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-with-RTC-on-imx8mm/m-p/1639830#M204801</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/207638"&gt;@ashikp6&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;It seems the Application is not using the correct RTC or does not have access to it.&lt;/P&gt;
&lt;P&gt;Is there any other RTC available on the system?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;# ls -la /dev/rtc*&lt;/LI-CODE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;One can refer to the below-mentioned links for more information.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://stackoverflow.com/questions/14398127/rtc-wakeup-is-not-working" target="_blank" rel="noopener"&gt;https://stackoverflow.com/questions/14398127/rtc-wakeup-is-not-working&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://stackoverflow.com/questions/23821356/android-sys-rtc-wakealarm-does-not-boot-device-when-off" target="_blank" rel="noopener"&gt;https://stackoverflow.com/questions/23821356/android-sys-rtc-wakealarm-does-not-boot-device-when-off&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Please try adding the below the line in&amp;nbsp;ueventd.nxp.rc&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;/dev/rtc0 0666 system system&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Dhruvit Vasavada&lt;/P&gt;</description>
      <pubDate>Tue, 25 Apr 2023 13:55:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-with-RTC-on-imx8mm/m-p/1639830#M204801</guid>
      <dc:creator>Dhruvit</dc:creator>
      <dc:date>2023-04-25T13:55:21Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with RTC on imx8mm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-with-RTC-on-imx8mm/m-p/1644633#M205248</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201299"&gt;@Dhruvit&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I tried the same application in my phone with android 11. There the application seems to be working as expected and brings the board from suspend mode when the alarm rings.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i am using only one rtc.Output of the above command is&lt;BR /&gt;/dev/rtc0&lt;/P&gt;</description>
      <pubDate>Thu, 04 May 2023 10:54:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-with-RTC-on-imx8mm/m-p/1644633#M205248</guid>
      <dc:creator>ashikp6</dc:creator>
      <dc:date>2023-05-04T10:54:53Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with RTC on imx8mm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-with-RTC-on-imx8mm/m-p/1644693#M205257</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/207638"&gt;@ashikp6&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;This issue could be due to the app not having permission to use RTC.&lt;/P&gt;
&lt;P&gt;Have you tried adding the below line in&amp;nbsp;&lt;SPAN&gt;ueventd.rc&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;/dev/rtc0 0666 system system&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Dhruvit Vasavada.&lt;/P&gt;</description>
      <pubDate>Thu, 04 May 2023 12:28:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-with-RTC-on-imx8mm/m-p/1644693#M205257</guid>
      <dc:creator>Dhruvit</dc:creator>
      <dc:date>2023-05-04T12:28:15Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with RTC on imx8mm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-with-RTC-on-imx8mm/m-p/1647165#M205524</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201299"&gt;@Dhruvit&lt;/a&gt;&amp;nbsp;,&lt;BR /&gt;&lt;BR /&gt;Tried adding&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;/dev/rtc0 0666 system system&amp;nbsp;&lt;/STRONG&gt;to /system/etc/ueventd.rc file. (Attached the updated file)&lt;BR /&gt;&lt;BR /&gt;Set alarm from application( google desk clock).Still not seeing the alarm interrupt being set as shown below&lt;BR /&gt;&lt;SPAN&gt;rtc_time &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;: 11:40:56&lt;BR /&gt;rtc_date &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;: 2023-05-09&lt;BR /&gt;alrm_time &amp;nbsp; &amp;nbsp; &amp;nbsp; : 00:00:00&lt;BR /&gt;alrm_date &amp;nbsp; &amp;nbsp; &amp;nbsp; : 1970-01-01&lt;BR /&gt;alarm_IRQ &amp;nbsp; &amp;nbsp; &amp;nbsp; : no&lt;BR /&gt;alrm_pending &amp;nbsp; &amp;nbsp;: no&lt;BR /&gt;updateIRQ enabled &amp;nbsp; &amp;nbsp; &amp;nbsp;: no&lt;BR /&gt;periodic IRQ enabled &amp;nbsp; &amp;nbsp;: no&lt;BR /&gt;periodic IRQ frequency &amp;nbsp;: 1&lt;BR /&gt;max user IRQ frequency &amp;nbsp;: 64 2&lt;BR /&gt;4hr &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;: yes&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;Thanks,&lt;BR /&gt;Ashik&lt;/P&gt;</description>
      <pubDate>Tue, 09 May 2023 12:48:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-with-RTC-on-imx8mm/m-p/1647165#M205524</guid>
      <dc:creator>ashikp6</dc:creator>
      <dc:date>2023-05-09T12:48:15Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with RTC on imx8mm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-with-RTC-on-imx8mm/m-p/1649117#M205738</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/207638"&gt;@ashikp6&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;This issue seems to be with how user application interface with RTC devices.&lt;/P&gt;
&lt;P&gt;As RTC seems to work fine with the wakealarm interface in user space.&lt;/P&gt;
&lt;P&gt;One can try debugging on google desk clock with the highest debug logs.&lt;/P&gt;
&lt;P&gt;Please refer to the below documentation for more information regarding this.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://developer.android.com/training/scheduling/alarms#exact-permission-declare" target="_self"&gt;&lt;STRONG&gt;Declare the appropriate exact alarm permission&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;&lt;A href="https://developer.android.com/training/scheduling/alarms" target="_self" rel="nofollow noopener noreferrer"&gt;Schedule alarms&lt;/A&gt;&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Dhruvit Vasavada&lt;/P&gt;</description>
      <pubDate>Fri, 12 May 2023 05:28:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-with-RTC-on-imx8mm/m-p/1649117#M205738</guid>
      <dc:creator>Dhruvit</dc:creator>
      <dc:date>2023-05-12T05:28:10Z</dc:date>
    </item>
  </channel>
</rss>