<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: [8QXP][Android Automotive] Can't see pcie</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/8QXP-Android-Automotive-Can-t-see-pcie/m-p/1638547#M204658</link>
    <description>I close it because it like a DTS problem.&lt;BR /&gt;Seems we re-write DTS so this issue is gone, but we still don't know which point cause this issue come.</description>
    <pubDate>Mon, 24 Apr 2023 02:50:25 GMT</pubDate>
    <dc:creator>WolsYang</dc:creator>
    <dc:date>2023-04-24T02:50:25Z</dc:date>
    <item>
      <title>[8QXP][Android Automotive] Can't see pcie</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/8QXP-Android-Automotive-Can-t-see-pcie/m-p/1637947#M204584</link>
      <description>&lt;P&gt;Can not see pcie on i.MX8QXP internal PLL with&amp;nbsp;&lt;SPAN&gt;Android Automotive 12.0.0_2.1.0 (Linux 5.15.32 BSP)&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;mek_8q:/ # zcat /proc/config.gz | grep -i imx_pci                              
CONFIG_PHY_FSL_IMX_PCIE=y
mek_8q:/ # zcat /proc/config.gz | grep -i pci_imx                              
CONFIG_PCI_IMX6=y
CONFIG_PCI_IMX6_HOST=y
mek_8q:/ # dmesg | grep -i pci                                                 
[    0.000000] Kernel command line: stack_depot_disable=on kasan.stacktrace=off kvm-arm.mode=protected cgroup_disable=pressure console=ttyLP0,115200 earlycon init=/init androidboot.hardware=nxp firmware_class.pe
[    0.314189] PCI: CLS 0 bytes, default 64
[    2.834329] tcpci: probe of 1-0050 failed with error -1
mek_8q:/ # lspci                                                               
mek_8q:/ # &lt;/LI-CODE&gt;&lt;P&gt;The HW should be ok since we can see it in uboot（Please ignore gpio error, for quick test we did'nt set it yet.）&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;=&amp;gt; pci
pca953x gpio@1a: Error reading output register
imx_pcie pcie@0x5f010000: -16 unable to get clkreq.
imx_pcie pcie@0x5f010000: -2 unable to get disable-gpio.
pca953x gpio@1a: Error reading output register
imx_pcie pcie@0x5f010000: 3 unable to get power-on-gpio.
imx_pcie pcie@0x5f010000: -16 unable to get power-on-gpio.
PCI:   pcie phy link never came up&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;Also we can see it on linux with this dts config&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;&amp;amp;pcieb{
	ext_osc = &amp;lt;0&amp;gt;;
};&lt;/LI-CODE&gt;</description>
      <pubDate>Fri, 21 Apr 2023 09:35:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/8QXP-Android-Automotive-Can-t-see-pcie/m-p/1637947#M204584</guid>
      <dc:creator>WolsYang</dc:creator>
      <dc:date>2023-04-21T09:35:33Z</dc:date>
    </item>
    <item>
      <title>Re: [8QXP][Android Automotive] Can't see pcie</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/8QXP-Android-Automotive-Can-t-see-pcie/m-p/1638547#M204658</link>
      <description>I close it because it like a DTS problem.&lt;BR /&gt;Seems we re-write DTS so this issue is gone, but we still don't know which point cause this issue come.</description>
      <pubDate>Mon, 24 Apr 2023 02:50:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/8QXP-Android-Automotive-Can-t-see-pcie/m-p/1638547#M204658</guid>
      <dc:creator>WolsYang</dc:creator>
      <dc:date>2023-04-24T02:50:25Z</dc:date>
    </item>
  </channel>
</rss>