<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 IMX8X ADC_IN0  Configuration Problem</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8X-ADC-IN0-Configuration-Problem/m-p/1638427#M204643</link>
    <description>&lt;P&gt;Dear：&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;SPAN class=""&gt;In IMX8QX scheme, ADC_IN0 needs to be multiplexed as GPIO. When configured as output, no matter the output is 0 or 1, the voltage on the pin does not change.&lt;/SPAN&gt;&lt;SPAN class=""&gt; The configuration is as follows:&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;SC_P_ADC_IN0_LSIO_GPIO1_IO10 0x0600006C /*phy1_reset*/&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;or&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;SC_P_ADC_IN0_LSIO_GPIO1_IO10 0x0600004C /*phy1_reset*/&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;Please confirm whether there is a problem when ADC_IN0 is reused as gpio.&lt;/SPAN&gt;&lt;SPAN class=""&gt; Because other pins we normally configure for gpio multiplexing have no problem, but now this ADC_IN0 after multiplexing control has no reaction?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;Best Regards!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Sun, 23 Apr 2023 07:31:39 GMT</pubDate>
    <dc:creator>jack_huang1</dc:creator>
    <dc:date>2023-04-23T07:31:39Z</dc:date>
    <item>
      <title>IMX8X ADC_IN0  Configuration Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8X-ADC-IN0-Configuration-Problem/m-p/1638427#M204643</link>
      <description>&lt;P&gt;Dear：&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;SPAN class=""&gt;In IMX8QX scheme, ADC_IN0 needs to be multiplexed as GPIO. When configured as output, no matter the output is 0 or 1, the voltage on the pin does not change.&lt;/SPAN&gt;&lt;SPAN class=""&gt; The configuration is as follows:&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;SC_P_ADC_IN0_LSIO_GPIO1_IO10 0x0600006C /*phy1_reset*/&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;or&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;SC_P_ADC_IN0_LSIO_GPIO1_IO10 0x0600004C /*phy1_reset*/&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;Please confirm whether there is a problem when ADC_IN0 is reused as gpio.&lt;/SPAN&gt;&lt;SPAN class=""&gt; Because other pins we normally configure for gpio multiplexing have no problem, but now this ADC_IN0 after multiplexing control has no reaction?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;Best Regards!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 23 Apr 2023 07:31:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8X-ADC-IN0-Configuration-Problem/m-p/1638427#M204643</guid>
      <dc:creator>jack_huang1</dc:creator>
      <dc:date>2023-04-23T07:31:39Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8X ADC_IN0  Configuration Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8X-ADC-IN0-Configuration-Problem/m-p/1638518#M204654</link>
      <description>&lt;P&gt;pls refer to the link as below:&lt;/P&gt;
&lt;P&gt;"&lt;A href="https://community.nxp.com/t5/i-MX-Processors/i-MX8-ADC-IN0-pin-can-t-set-as-GPIO-function/m-p/959866" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/i-MX8-ADC-IN0-pin-can-t-set-as-GPIO-function/m-p/959866&lt;/A&gt;"&lt;/P&gt;</description>
      <pubDate>Mon, 24 Apr 2023 01:53:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8X-ADC-IN0-Configuration-Problem/m-p/1638518#M204654</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-04-24T01:53:22Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8X ADC_IN0  Configuration Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8X-ADC-IN0-Configuration-Problem/m-p/1642572#M205075</link>
      <description>&lt;P&gt;Dears：&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;SPAN class=""&gt;The problem has been solved.&lt;/SPAN&gt;&lt;SPAN class=""&gt; Thanks!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Best&amp;nbsp; Regards！&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 30 Apr 2023 13:50:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8X-ADC-IN0-Configuration-Problem/m-p/1642572#M205075</guid>
      <dc:creator>jack_huang1</dc:creator>
      <dc:date>2023-04-30T13:50:50Z</dc:date>
    </item>
  </channel>
</rss>