<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic DMA SMFC Channel Flexibility in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/DMA-SMFC-Channel-Flexibility/m-p/1637470#M204538</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;This is a question regarding the DMA SMFC Channels. I'm using a SabreSD Quad Platform with Android Pie.&lt;BR /&gt;&lt;BR /&gt;Typically (as shown in the picture below) the sensor connected to CSI0 sends the data through the dma_smfc_ch0.&lt;BR /&gt;&lt;BR /&gt;I would like to know if it's possible to configure the data path for CSI1 to make the flow go through dma_smfc_ch0 as well, instead of any other channel, since my understanding is that dma_smfc_ch0 is the only channel that is able to use the whole FIFO, while the other channels will use a reduced FIFO.&lt;BR /&gt;&lt;BR /&gt;To provide more context, currently, our application is running intensive operations in memory, so we need to have a FIFO as big as possible to queue data so that the camera pixels are not lost while the memory is busy, so I appreciate it if anyone can provide more input on this and/or there are other ideas.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="AlejandroS_0-1682013947263.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/220174iB717FC9E46B0E1F4/image-size/medium?v=v2&amp;amp;px=400" role="button" title="AlejandroS_0-1682013947263.png" alt="AlejandroS_0-1682013947263.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 20 Apr 2023 18:10:56 GMT</pubDate>
    <dc:creator>AlejandroS</dc:creator>
    <dc:date>2023-04-20T18:10:56Z</dc:date>
    <item>
      <title>DMA SMFC Channel Flexibility</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DMA-SMFC-Channel-Flexibility/m-p/1637470#M204538</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;This is a question regarding the DMA SMFC Channels. I'm using a SabreSD Quad Platform with Android Pie.&lt;BR /&gt;&lt;BR /&gt;Typically (as shown in the picture below) the sensor connected to CSI0 sends the data through the dma_smfc_ch0.&lt;BR /&gt;&lt;BR /&gt;I would like to know if it's possible to configure the data path for CSI1 to make the flow go through dma_smfc_ch0 as well, instead of any other channel, since my understanding is that dma_smfc_ch0 is the only channel that is able to use the whole FIFO, while the other channels will use a reduced FIFO.&lt;BR /&gt;&lt;BR /&gt;To provide more context, currently, our application is running intensive operations in memory, so we need to have a FIFO as big as possible to queue data so that the camera pixels are not lost while the memory is busy, so I appreciate it if anyone can provide more input on this and/or there are other ideas.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="AlejandroS_0-1682013947263.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/220174iB717FC9E46B0E1F4/image-size/medium?v=v2&amp;amp;px=400" role="button" title="AlejandroS_0-1682013947263.png" alt="AlejandroS_0-1682013947263.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 20 Apr 2023 18:10:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DMA-SMFC-Channel-Flexibility/m-p/1637470#M204538</guid>
      <dc:creator>AlejandroS</dc:creator>
      <dc:date>2023-04-20T18:10:56Z</dc:date>
    </item>
    <item>
      <title>Re: DMA SMFC Channel Flexibility</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DMA-SMFC-Channel-Flexibility/m-p/1637513#M204544</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;From camera SMFC can use only one DMA channel. "DI (data identifier)" concept is used&lt;/P&gt;
&lt;P&gt;only for MIPI interface, this is described in sect.37.4. i.MX 6Dual/6Quad Applications Processor Reference Manual&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 20 Apr 2023 20:32:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DMA-SMFC-Channel-Flexibility/m-p/1637513#M204544</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2023-04-20T20:32:17Z</dc:date>
    </item>
    <item>
      <title>Re: DMA SMFC Channel Flexibility</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DMA-SMFC-Channel-Flexibility/m-p/1638268#M204622</link>
      <description>&lt;P&gt;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/34846" target="_blank"&gt;@Bio_TICFSL&lt;/A&gt;&amp;nbsp;Thanks for the timely reply!&lt;BR /&gt;&lt;BR /&gt;Moreover, from table&amp;nbsp;&lt;STRONG&gt;IPUx_SMFC_MAP field descriptions&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;I see (for instance):&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="AlejandroS_0-1682116187523.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/220373i7DA77C85427C0245/image-size/medium?v=v2&amp;amp;px=400" role="button" title="AlejandroS_0-1682116187523.png" alt="AlejandroS_0-1682116187523.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;My understanding is that one can map CSI1 data to DMASMFC channel 0. This way the data would be mapped to the FIFO base address 0 which is what we need.&lt;BR /&gt;&lt;BR /&gt;Is there anything else I'm missing that won't enable us to make this configuration?&lt;/P&gt;</description>
      <pubDate>Fri, 21 Apr 2023 22:29:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DMA-SMFC-Channel-Flexibility/m-p/1638268#M204622</guid>
      <dc:creator>AlejandroS</dc:creator>
      <dc:date>2023-04-21T22:29:58Z</dc:date>
    </item>
  </channel>
</rss>