<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic usb host stack support for 4G modem device in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/usb-host-stack-support-for-4G-modem-device/m-p/1637246#M204521</link>
    <description>&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;Just wanted to check if the USB &lt;STRONG&gt;host&lt;/STRONG&gt; stack available in MCUXpresso SDK supports 4G modem type devices. Also SFTP protocol as i don't see any SFTP protocol in lwip stack in the SDK.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Babu&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 20 Apr 2023 11:39:35 GMT</pubDate>
    <dc:creator>sbabu</dc:creator>
    <dc:date>2023-04-20T11:39:35Z</dc:date>
    <item>
      <title>usb host stack support for 4G modem device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/usb-host-stack-support-for-4G-modem-device/m-p/1637246#M204521</link>
      <description>&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;Just wanted to check if the USB &lt;STRONG&gt;host&lt;/STRONG&gt; stack available in MCUXpresso SDK supports 4G modem type devices. Also SFTP protocol as i don't see any SFTP protocol in lwip stack in the SDK.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Babu&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 20 Apr 2023 11:39:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/usb-host-stack-support-for-4G-modem-device/m-p/1637246#M204521</guid>
      <dc:creator>sbabu</dc:creator>
      <dc:date>2023-04-20T11:39:35Z</dc:date>
    </item>
    <item>
      <title>Re: usb host stack support for 4G modem device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/usb-host-stack-support-for-4G-modem-device/m-p/1637338#M204529</link>
      <description>&lt;P&gt;Thank you for contacting NXP support!&lt;/P&gt;
&lt;P&gt;Are you using iMX8 or iMXRT?&lt;/P&gt;</description>
      <pubDate>Thu, 20 Apr 2023 14:44:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/usb-host-stack-support-for-4G-modem-device/m-p/1637338#M204529</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2023-04-20T14:44:41Z</dc:date>
    </item>
    <item>
      <title>Re: usb host stack support for 4G modem device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/usb-host-stack-support-for-4G-modem-device/m-p/1637437#M204533</link>
      <description>&lt;P&gt;Hi Chavira,&lt;/P&gt;&lt;P&gt;We are using MX RT1024.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Subash&lt;/P&gt;</description>
      <pubDate>Thu, 20 Apr 2023 16:56:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/usb-host-stack-support-for-4G-modem-device/m-p/1637437#M204533</guid>
      <dc:creator>sbabu</dc:creator>
      <dc:date>2023-04-20T16:56:44Z</dc:date>
    </item>
    <item>
      <title>Re: usb host stack support for 4G modem device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/usb-host-stack-support-for-4G-modem-device/m-p/1639961#M204812</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/214337"&gt;@sbabu&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The SFTP protocol is not supported. As for the 4G modem type devices, I believe it depend on the USB class type required for your modem. As long as it is a supported class, it should be OK.&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Tue, 25 Apr 2023 18:11:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/usb-host-stack-support-for-4G-modem-device/m-p/1639961#M204812</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2023-04-25T18:11:51Z</dc:date>
    </item>
    <item>
      <title>Re: usb host stack support for 4G modem device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/usb-host-stack-support-for-4G-modem-device/m-p/1641783#M204985</link>
      <description>&lt;P&gt;Hi again&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/214337"&gt;@sbabu&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I believe this Application Note will be useful for your inquiry:&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN13940.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN13940.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 27 Apr 2023 19:14:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/usb-host-stack-support-for-4G-modem-device/m-p/1641783#M204985</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2023-04-27T19:14:54Z</dc:date>
    </item>
  </channel>
</rss>