<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX8M Mini LPDDR4-3000 Trace length/delay matching in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-LPDDR4-3000-Trace-length-delay-matching/m-p/1636376#M204465</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm currently designing a custom PCB with the i.MX8M Mini using the LPDDR4-3000 as memory. I have multiple questions when it comes to routing the LPDDR4-3000 to the i.MX8M Mini.&lt;/P&gt;&lt;P&gt;I'm aware of the &lt;STRONG&gt;i.MX 8M Mini&amp;nbsp;Hardware Developer's Guide&lt;/STRONG&gt; document but still have a lot of questions.&amp;nbsp;&lt;/P&gt;&lt;P&gt;NOTE: I'm currently using Autodesk Fusion 360 and therefor I'm limited when it comes SI Simulations. I know Fusion 360 has a SI Simulation tool extension, but it's not really useful...&amp;nbsp;&lt;/P&gt;&lt;P&gt;My current design is using the exact same board stack up and trace widths (for controlled impedance) as the &lt;STRONG&gt;8MMINILPD4-CPU&lt;/STRONG&gt; (see figure 1 &amp;amp; 2 below).&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. Is it sufficient enough if I only &lt;STRONG&gt;length&lt;/STRONG&gt; match all signals to the DDR (note that I'm using Layer 1, 3 and 8 like in the&amp;nbsp;&lt;STRONG&gt;8MMINILPD4-CPU&amp;nbsp;&lt;/STRONG&gt;design)? See figure 3 below, Layer 1 = red, Layer 3 = yellow, Layer 8 = blue. All signals have an equal length of 868 mil.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. If &lt;STRONG&gt;length&lt;/STRONG&gt; matching is not sufficient I will have to &lt;STRONG&gt;time delay&lt;/STRONG&gt; match. Do I have to include the pkg delays into these calculations?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;3. Is there a rule of thumb for the Signal Propagation e.g. per 1mm about 6.7ps?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;4. With the current stack up, will I need to be very exact and calculate different signal propagation for signals in the third layer, because these are striplines and the signal is therefor slower than on microstrips?&lt;/P&gt;&lt;P&gt;Thanks in advance and help is much appreciated!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;SPEEDBIRD&lt;/P&gt;</description>
    <pubDate>Wed, 19 Apr 2023 15:06:33 GMT</pubDate>
    <dc:creator>SPEEDBIRD</dc:creator>
    <dc:date>2023-04-19T15:06:33Z</dc:date>
    <item>
      <title>i.MX8M Mini LPDDR4-3000 Trace length/delay matching</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-LPDDR4-3000-Trace-length-delay-matching/m-p/1636376#M204465</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm currently designing a custom PCB with the i.MX8M Mini using the LPDDR4-3000 as memory. I have multiple questions when it comes to routing the LPDDR4-3000 to the i.MX8M Mini.&lt;/P&gt;&lt;P&gt;I'm aware of the &lt;STRONG&gt;i.MX 8M Mini&amp;nbsp;Hardware Developer's Guide&lt;/STRONG&gt; document but still have a lot of questions.&amp;nbsp;&lt;/P&gt;&lt;P&gt;NOTE: I'm currently using Autodesk Fusion 360 and therefor I'm limited when it comes SI Simulations. I know Fusion 360 has a SI Simulation tool extension, but it's not really useful...&amp;nbsp;&lt;/P&gt;&lt;P&gt;My current design is using the exact same board stack up and trace widths (for controlled impedance) as the &lt;STRONG&gt;8MMINILPD4-CPU&lt;/STRONG&gt; (see figure 1 &amp;amp; 2 below).&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. Is it sufficient enough if I only &lt;STRONG&gt;length&lt;/STRONG&gt; match all signals to the DDR (note that I'm using Layer 1, 3 and 8 like in the&amp;nbsp;&lt;STRONG&gt;8MMINILPD4-CPU&amp;nbsp;&lt;/STRONG&gt;design)? See figure 3 below, Layer 1 = red, Layer 3 = yellow, Layer 8 = blue. All signals have an equal length of 868 mil.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. If &lt;STRONG&gt;length&lt;/STRONG&gt; matching is not sufficient I will have to &lt;STRONG&gt;time delay&lt;/STRONG&gt; match. Do I have to include the pkg delays into these calculations?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;3. Is there a rule of thumb for the Signal Propagation e.g. per 1mm about 6.7ps?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;4. With the current stack up, will I need to be very exact and calculate different signal propagation for signals in the third layer, because these are striplines and the signal is therefor slower than on microstrips?&lt;/P&gt;&lt;P&gt;Thanks in advance and help is much appreciated!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;SPEEDBIRD&lt;/P&gt;</description>
      <pubDate>Wed, 19 Apr 2023 15:06:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-LPDDR4-3000-Trace-length-delay-matching/m-p/1636376#M204465</guid>
      <dc:creator>SPEEDBIRD</dc:creator>
      <dc:date>2023-04-19T15:06:33Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M Mini LPDDR4-3000 Trace length/delay matching</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-LPDDR4-3000-Trace-length-delay-matching/m-p/1637100#M204510</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/216082"&gt;@SPEEDBIRD&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;Please see the response to your queries below:&lt;/P&gt;
&lt;P&gt;1. Is it sufficient enough if I only length match all signals to the DDR (note that I'm using Layer 1, 3 and 8 like in the 8MMINILPD4-CPU design)? See figure 3 below, Layer 1 = red, Layer 3 = yellow, Layer 8 = blue. All signals have an equal length of 868 mil.&lt;BR /&gt;&lt;STRONG&gt;[NXP]: If all the DDR signals mentioned in Section 3.4.2.1 i.MX 8M Mini LPDDR4-3000 routing recommendations of HDG document and all recommended guidelines are followed, then it is good to go.&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;2. If length matching is not sufficient I will have to time delay match. Do I have to include the pkg delays into these calculations?&lt;BR /&gt;&lt;STRONG&gt;[NXP]: Package delay of memory IC shall not be taken into consideration.&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;3. Is there a rule of thumb for the Signal Propagation e.g. per 1mm about 6.7ps? &lt;BR /&gt;&lt;STRONG&gt;[NXP]: One can refer to the below-mentioned link for refer of Signal propagation.&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&lt;A href="https://www.protoexpress.com/blog/signal-propagation-delay-pcb/" target="_blank"&gt;https://www.protoexpress.com/blog/signal-propagation-delay-pcb/&lt;/A&gt;&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;4. With the current stack up, will I need to be very exact and calculate different signal propagation for signals in the third layer, because these are striplines and the signal is therefore slower than on microstrips?&lt;BR /&gt;&lt;STRONG&gt;[NXP]: Yes, that is correct.&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Ritesh M Patel&lt;/P&gt;</description>
      <pubDate>Thu, 20 Apr 2023 09:36:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-LPDDR4-3000-Trace-length-delay-matching/m-p/1637100#M204510</guid>
      <dc:creator>riteshmpatel</dc:creator>
      <dc:date>2023-04-20T09:36:59Z</dc:date>
    </item>
  </channel>
</rss>