<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: What are all the Linux-kernel versions compatible with the Android 11.0.0_2.2.0 using i.MX8MQ EV in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/What-are-all-the-Linux-kernel-versions-compatible-with-the/m-p/1636106#M204434</link>
    <description>&lt;P&gt;refer to the release note, android 11.0.0_2.2.0 uses Linux 5.10.35 kernel&lt;/P&gt;</description>
    <pubDate>Wed, 19 Apr 2023 09:32:23 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2023-04-19T09:32:23Z</dc:date>
    <item>
      <title>What are all the Linux-kernel versions compatible with the Android 11.0.0_2.2.0 using i.MX8MQ EVK?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-are-all-the-Linux-kernel-versions-compatible-with-the/m-p/1635964#M204417</link>
      <description>&lt;P&gt;What are all the Linux-kernel versions which are compatible (so that I should not get any checkvinff error) with the Android 11.0.0_2.2.0 using i.MX8MQ EVK? And replacing the separately built kernel Image alone of the supported version to the Android source code helps me to upgrade the kernel?&lt;/P&gt;</description>
      <pubDate>Wed, 19 Apr 2023 07:02:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-are-all-the-Linux-kernel-versions-compatible-with-the/m-p/1635964#M204417</guid>
      <dc:creator>Iyshwarya</dc:creator>
      <dc:date>2023-04-19T07:02:19Z</dc:date>
    </item>
    <item>
      <title>Re: What are all the Linux-kernel versions compatible with the Android 11.0.0_2.2.0 using i.MX8MQ EV</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-are-all-the-Linux-kernel-versions-compatible-with-the/m-p/1636106#M204434</link>
      <description>&lt;P&gt;refer to the release note, android 11.0.0_2.2.0 uses Linux 5.10.35 kernel&lt;/P&gt;</description>
      <pubDate>Wed, 19 Apr 2023 09:32:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-are-all-the-Linux-kernel-versions-compatible-with-the/m-p/1636106#M204434</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-04-19T09:32:23Z</dc:date>
    </item>
  </channel>
</rss>