<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックFuse the secure boot key using UUU tool</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Fuse-the-secure-boot-key-using-UUU-tool/m-p/1634200#M204250</link>
    <description>&lt;P&gt;Hi team,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Just for information, I am using the imx6q board and implementing the secure boot HAB and have tested the manual fused the public key&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;SRK_1_2_3=_4_fuse.bin&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;is this is working fine, but i want to automate this fusing using in the UUU script.&lt;/P&gt;&lt;P&gt;I have already the information about the HAB block in u-boot.imx.log file&lt;/P&gt;&lt;P&gt;$cat u-boot.imx.log&lt;BR /&gt;Image Type: Freescale IMX Boot Image&lt;BR /&gt;Image Ver: 2 (i.MX53/6/7 compatible)&lt;BR /&gt;Mode: DCD&lt;BR /&gt;Data Size: 602112 Bytes = 588.00 KiB = 0.57 MiB&lt;BR /&gt;Load Address: 877ff420&lt;BR /&gt;Entry Point: 87800000&lt;BR /&gt;HAB Blocks: 877ff400 00000000 0008ec00&lt;BR /&gt;DCD Blocks: 00910000 0000002c 000001c4&lt;/P&gt;&lt;P&gt;As per the UUU pdf " the IVT is modified when downloading to the target the binary must be signed with a cleared DCD pointer".&lt;/P&gt;&lt;P&gt;Do i have to use the mentioned script for generating the DCD pointer,&amp;nbsp;/mod_4_mfgtool.sh for all images ? or How it works ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please give suggestion on this action.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Rk&lt;/P&gt;</description>
    <pubDate>Sun, 16 Apr 2023 08:41:46 GMT</pubDate>
    <dc:creator>rakesh3</dc:creator>
    <dc:date>2023-04-16T08:41:46Z</dc:date>
    <item>
      <title>Fuse the secure boot key using UUU tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Fuse-the-secure-boot-key-using-UUU-tool/m-p/1634200#M204250</link>
      <description>&lt;P&gt;Hi team,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Just for information, I am using the imx6q board and implementing the secure boot HAB and have tested the manual fused the public key&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;SRK_1_2_3=_4_fuse.bin&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;is this is working fine, but i want to automate this fusing using in the UUU script.&lt;/P&gt;&lt;P&gt;I have already the information about the HAB block in u-boot.imx.log file&lt;/P&gt;&lt;P&gt;$cat u-boot.imx.log&lt;BR /&gt;Image Type: Freescale IMX Boot Image&lt;BR /&gt;Image Ver: 2 (i.MX53/6/7 compatible)&lt;BR /&gt;Mode: DCD&lt;BR /&gt;Data Size: 602112 Bytes = 588.00 KiB = 0.57 MiB&lt;BR /&gt;Load Address: 877ff420&lt;BR /&gt;Entry Point: 87800000&lt;BR /&gt;HAB Blocks: 877ff400 00000000 0008ec00&lt;BR /&gt;DCD Blocks: 00910000 0000002c 000001c4&lt;/P&gt;&lt;P&gt;As per the UUU pdf " the IVT is modified when downloading to the target the binary must be signed with a cleared DCD pointer".&lt;/P&gt;&lt;P&gt;Do i have to use the mentioned script for generating the DCD pointer,&amp;nbsp;/mod_4_mfgtool.sh for all images ? or How it works ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please give suggestion on this action.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Rk&lt;/P&gt;</description>
      <pubDate>Sun, 16 Apr 2023 08:41:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Fuse-the-secure-boot-key-using-UUU-tool/m-p/1634200#M204250</guid>
      <dc:creator>rakesh3</dc:creator>
      <dc:date>2023-04-16T08:41:46Z</dc:date>
    </item>
    <item>
      <title>Re: Fuse the secure boot key using UUU tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Fuse-the-secure-boot-key-using-UUU-tool/m-p/1634678#M204308</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/212816"&gt;@rakesh3&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can try to add the command line (for example: FB:ucmd fuse prog -y bank word hashval ) to uuu script.&lt;/P&gt;
&lt;P&gt;Other images are not related to DCD.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Mon, 17 Apr 2023 12:45:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Fuse-the-secure-boot-key-using-UUU-tool/m-p/1634678#M204308</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2023-04-17T12:45:26Z</dc:date>
    </item>
  </channel>
</rss>