<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: MIPI CSI Interface with differnt voltage level</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-Interface-with-differnt-voltage-level/m-p/1633759#M204215</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/189291"&gt;@YHE_Desko&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;i.MX8MP MIPI interface is compliant&amp;nbsp;with MIPI D-PHY specification V1.2 and&amp;nbsp;MIPI CSI2 Specification V1.3 except for the C-PHY feature.&lt;/P&gt;
&lt;P&gt;One can use the CSI sensors which comply with above mentioned MIPI specifications.&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Ritesh M Patel&lt;/P&gt;</description>
    <pubDate>Fri, 14 Apr 2023 08:49:13 GMT</pubDate>
    <dc:creator>riteshmpatel</dc:creator>
    <dc:date>2023-04-14T08:49:13Z</dc:date>
    <item>
      <title>MIPI CSI Interface with differnt voltage level</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-Interface-with-differnt-voltage-level/m-p/1633074#M204149</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;we have a problem by PCB design. Our processor imx8mp is currently using 1.2V for MIPI-CSI interface, but the sensor we using (AR2020) can only support 1.05V MIPI-CSI interface. To avoid any changes on processor bord side, we are trying to find a solution for this problem just on the sensor side.&lt;/P&gt;&lt;P&gt;Is a level shifter (level translation) necessary for this situation? Or we can just directly connect them?&lt;/P&gt;&lt;P&gt;I am looking forward for your answer. Thanks a lot.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Yujia&lt;/P&gt;</description>
      <pubDate>Thu, 13 Apr 2023 10:20:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-Interface-with-differnt-voltage-level/m-p/1633074#M204149</guid>
      <dc:creator>YHE_Desko</dc:creator>
      <dc:date>2023-04-13T10:20:51Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI CSI Interface with differnt voltage level</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-Interface-with-differnt-voltage-level/m-p/1633759#M204215</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/189291"&gt;@YHE_Desko&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;i.MX8MP MIPI interface is compliant&amp;nbsp;with MIPI D-PHY specification V1.2 and&amp;nbsp;MIPI CSI2 Specification V1.3 except for the C-PHY feature.&lt;/P&gt;
&lt;P&gt;One can use the CSI sensors which comply with above mentioned MIPI specifications.&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Ritesh M Patel&lt;/P&gt;</description>
      <pubDate>Fri, 14 Apr 2023 08:49:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-Interface-with-differnt-voltage-level/m-p/1633759#M204215</guid>
      <dc:creator>riteshmpatel</dc:creator>
      <dc:date>2023-04-14T08:49:13Z</dc:date>
    </item>
  </channel>
</rss>