<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: scfw API</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/scfw-API/m-p/1632555#M204094</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Yes, interrupts in the chip are managed through two IPs. One of the IP is the GIC-500 from ARM and Interrupt Steer controller and in this case it is linked to GIC-500 implementation from ARM.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
    <pubDate>Wed, 12 Apr 2023 20:21:13 GMT</pubDate>
    <dc:creator>JorgeCas</dc:creator>
    <dc:date>2023-04-12T20:21:13Z</dc:date>
    <item>
      <title>scfw API</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/scfw-API/m-p/1632144#M204083</link>
      <description>&lt;P&gt;we are using imxqm and trying to suspend the cores and ddr, ew are using&amp;nbsp;sc_pm_set_cpu_resume API to to resume cpu from lp mode, address parameter in the API .. is this the address scfw jumps when GIC interrupt is hit.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Apr 2023 12:41:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/scfw-API/m-p/1632144#M204083</guid>
      <dc:creator>Lakshmi_AG</dc:creator>
      <dc:date>2023-04-12T12:41:24Z</dc:date>
    </item>
    <item>
      <title>Re: scfw API</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/scfw-API/m-p/1632555#M204094</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Yes, interrupts in the chip are managed through two IPs. One of the IP is the GIC-500 from ARM and Interrupt Steer controller and in this case it is linked to GIC-500 implementation from ARM.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Wed, 12 Apr 2023 20:21:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/scfw-API/m-p/1632555#M204094</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2023-04-12T20:21:13Z</dc:date>
    </item>
  </channel>
</rss>