<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX8MPLUSLPD4-PEVK USB Boot not detected in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MPLUSLPD4-PEVK-USB-Boot-not-detected/m-p/1632321#M204088</link>
    <description>&lt;P&gt;Issue is caused due to having UUU installed on WSL which is not able to read USB ports natively.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 12 Apr 2023 16:25:14 GMT</pubDate>
    <dc:creator>MartinKozevnikov</dc:creator>
    <dc:date>2023-04-12T16:25:14Z</dc:date>
    <item>
      <title>IMX8MPLUSLPD4-PEVK USB Boot not detected</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MPLUSLPD4-PEVK-USB-Boot-not-detected/m-p/1632176#M204087</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;I've been trying to bring up the board using the "Serial Download Mode" and the UUU tool found here &lt;A href="https://github.com/nxp-imx/mfgtools" target="_blank" rel="noopener"&gt;https://github.com/nxp-imx/mfgtools&lt;/A&gt;. UUU got built fine in WSL. The board gets brought up fine in eMMC boot and SD boot mode with "Linux 6.1.1_1.0.0" image. However, for USB boot to work we need a USB connection to PC. This connection is not being recognised by PC.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;When running ./uuu -lsusb I get the following:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="MartinKozevnikov_0-1681305077158.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/218951iD914696320D04C27/image-size/medium?v=v2&amp;amp;px=400" role="button" title="MartinKozevnikov_0-1681305077158.png" alt="MartinKozevnikov_0-1681305077158.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;There are 4 USB connectors on the EVK.&amp;nbsp;&lt;BR /&gt;1) J23, Micro USB Serial UART connection&lt;BR /&gt;2) J5, USB-C Power connection&lt;BR /&gt;3) J6, USB-C Port 1 DRP connection&lt;BR /&gt;4) J7, USB-A Port 2 Host connection&lt;BR /&gt;&lt;BR /&gt;I've connected Port 1 to my PC which doesn't seem to get recognised.&lt;BR /&gt;&lt;BR /&gt;The board:&amp;nbsp;&lt;A href="https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/evaluation-kit-for-the-i-mx-8m-plus-applications-processor:8MPLUSLPD4-EVK" target="_blank" rel="noopener"&gt;https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/evaluation-kit-for-the-i-mx-8m-plus-applications-processor:8MPLUSLPD4-EVK&lt;/A&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Apr 2023 13:16:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MPLUSLPD4-PEVK-USB-Boot-not-detected/m-p/1632176#M204087</guid>
      <dc:creator>MartinKozevnikov</dc:creator>
      <dc:date>2023-04-12T13:16:18Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MPLUSLPD4-PEVK USB Boot not detected</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MPLUSLPD4-PEVK-USB-Boot-not-detected/m-p/1632321#M204088</link>
      <description>&lt;P&gt;Issue is caused due to having UUU installed on WSL which is not able to read USB ports natively.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Apr 2023 16:25:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MPLUSLPD4-PEVK-USB-Boot-not-detected/m-p/1632321#M204088</guid>
      <dc:creator>MartinKozevnikov</dc:creator>
      <dc:date>2023-04-12T16:25:14Z</dc:date>
    </item>
  </channel>
</rss>