<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX8QM Android Automotive OS 10 Phone Call Sound Issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-Android-Automotive-OS-10-Phone-Call-Sound-Issue/m-p/1629314#M203847</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;In the Android Automotive release, the route is configured as follows: Alarm, notification, and system sounds are played from the audio jack on the CPU board. Other sounds such as music are played from the extended audio board.&lt;/P&gt;
&lt;P&gt;Additionally, Android Automotive is supported under Professional Services scheme. You could refer to the following link for additional details:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/support/support/nxp-professional-services:PROFESSIONAL-SERVICE?_gl=1*uavym6*_ga*MTYwNjM1NzY2My4xNjc3Njk0NTAy*_ga_WM5LE0KMSH*MTY3NzY5NDUwMi4xLjAuMTY3NzY5NDUwMi4wLjAuMA" target="_self"&gt;NXP Professional Services | NXP&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
    <pubDate>Thu, 06 Apr 2023 18:45:57 GMT</pubDate>
    <dc:creator>JorgeCas</dc:creator>
    <dc:date>2023-04-06T18:45:57Z</dc:date>
    <item>
      <title>iMX8QM Android Automotive OS 10 Phone Call Sound Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-Android-Automotive-OS-10-Phone-Call-Sound-Issue/m-p/1628277#M203769</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am developing on the iMX8QM EVK board with Android Automotive OS version 10_2.4.0.&lt;/P&gt;&lt;P&gt;I updated the "wm896_config.json" file located in the "android_build/device/fsl/common/audio-json" directory as follows.&lt;BR /&gt;Thus, I heard the sounds of MUSIC_CONTEXT, NAVIGATION_CONTEXT, VOICE_COMMAND_CONTEXT, CALL_RING_CONTEXT, CALL_CONTEXT over the 3.5mm jack on the board.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;{
  "driver_name": "wm8960-audio",
  "bus_name": "bus0_media_out",
  "supported_out_devices": ["speaker", "wired_headphone", "wired_headset", "bus"],
  "supported_in_devices": ["builtin_mic","wired_headset"],
  "support_lpa": 1,

  "init_ctl": [
    {"name": "Left Output Mixer PCM Playback Switch", "type": "int", "val": 1},
    {"name": "Right Output Mixer PCM Playback Switch", "type": "int", "val": 1},
    {"name": "Playback Volume", "type": "int", "val": 230},
    {"name": "Speaker Playback Volume", "type": "int", "val": 120},
    {"name": "Headphone Playback Volume", "type": "int", "val": 120}
  ],

  "builtin_mic_ctl": [
    {"name": "ALC Function", "type": "int", "val": 3},
    {"name": "Left Input Mixer Boost Switch", "type": "int", "val": 1},
    {"name": "ADC PCM Capture Volume", "type": "int", "val": 230},
    {"name": "Capture Volume", "type": "int", "val": 60}
  ],

  "out_volume_ctl": [
    "Playback Volume"
  ]
}&lt;/LI-CODE&gt;&lt;P&gt;I connected my phone to the board with bluetooth. I made a call and when the call was made, I could hear the ringtone with my headphones through the jack on the board.&lt;/P&gt;&lt;P&gt;I answered the call but could not hear the conversations through the earpiece and my voice did not go to the caller.&lt;/P&gt;&lt;P&gt;How can I solve this problem?&lt;/P&gt;&lt;P&gt;Can you help me with this?&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Efecan&lt;/P&gt;</description>
      <pubDate>Wed, 05 Apr 2023 13:26:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-Android-Automotive-OS-10-Phone-Call-Sound-Issue/m-p/1628277#M203769</guid>
      <dc:creator>cbl</dc:creator>
      <dc:date>2023-04-05T13:26:42Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM Android Automotive OS 10 Phone Call Sound Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-Android-Automotive-OS-10-Phone-Call-Sound-Issue/m-p/1629314#M203847</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;In the Android Automotive release, the route is configured as follows: Alarm, notification, and system sounds are played from the audio jack on the CPU board. Other sounds such as music are played from the extended audio board.&lt;/P&gt;
&lt;P&gt;Additionally, Android Automotive is supported under Professional Services scheme. You could refer to the following link for additional details:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/support/support/nxp-professional-services:PROFESSIONAL-SERVICE?_gl=1*uavym6*_ga*MTYwNjM1NzY2My4xNjc3Njk0NTAy*_ga_WM5LE0KMSH*MTY3NzY5NDUwMi4xLjAuMTY3NzY5NDUwMi4wLjAuMA" target="_self"&gt;NXP Professional Services | NXP&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Thu, 06 Apr 2023 18:45:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-Android-Automotive-OS-10-Phone-Call-Sound-Issue/m-p/1629314#M203847</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2023-04-06T18:45:57Z</dc:date>
    </item>
  </channel>
</rss>