<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Linux driver for Timer PWM Module (TPM) on i.MX8QXP? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Linux-driver-for-Timer-PWM-Module-TPM-on-i-MX8QXP/m-p/1627763#M203724</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I would like to use the TPM unit on the i.MX8QXP processor from Linux. Checking the 5.15.72-2.2.0 kernel, I can find a TPM driver for the i.MX7ULP and i.MX8ULP. The documentation is here:&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/nxp-imx/linux-imx/blob/lf-5.15.71-2.2.0/Documentation/devicetree/bindings/timer/nxp%2Ctpm-timer.yaml" target="_blank"&gt;https://github.com/nxp-imx/linux-imx/blob/lf-5.15.71-2.2.0/Documentation/devicetree/bindings/timer/nxp%2Ctpm-timer.yaml&lt;/A&gt;&lt;/P&gt;&lt;P&gt;So as far as I can see, there is currently no official support for TPM on this platform. Is the i.MX8ULP module compatible with the one in i.MX8QXP or will this require a completely new driver?&lt;/P&gt;&lt;P&gt;Any hint will be greatly appreciated!&lt;/P&gt;</description>
    <pubDate>Tue, 04 Apr 2023 15:16:02 GMT</pubDate>
    <dc:creator>laodzu</dc:creator>
    <dc:date>2023-04-04T15:16:02Z</dc:date>
    <item>
      <title>Linux driver for Timer PWM Module (TPM) on i.MX8QXP?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-driver-for-Timer-PWM-Module-TPM-on-i-MX8QXP/m-p/1627763#M203724</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I would like to use the TPM unit on the i.MX8QXP processor from Linux. Checking the 5.15.72-2.2.0 kernel, I can find a TPM driver for the i.MX7ULP and i.MX8ULP. The documentation is here:&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/nxp-imx/linux-imx/blob/lf-5.15.71-2.2.0/Documentation/devicetree/bindings/timer/nxp%2Ctpm-timer.yaml" target="_blank"&gt;https://github.com/nxp-imx/linux-imx/blob/lf-5.15.71-2.2.0/Documentation/devicetree/bindings/timer/nxp%2Ctpm-timer.yaml&lt;/A&gt;&lt;/P&gt;&lt;P&gt;So as far as I can see, there is currently no official support for TPM on this platform. Is the i.MX8ULP module compatible with the one in i.MX8QXP or will this require a completely new driver?&lt;/P&gt;&lt;P&gt;Any hint will be greatly appreciated!&lt;/P&gt;</description>
      <pubDate>Tue, 04 Apr 2023 15:16:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-driver-for-Timer-PWM-Module-TPM-on-i-MX8QXP/m-p/1627763#M203724</guid>
      <dc:creator>laodzu</dc:creator>
      <dc:date>2023-04-04T15:16:02Z</dc:date>
    </item>
    <item>
      <title>Re: Linux driver for Timer PWM Module (TPM) on i.MX8QXP?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-driver-for-Timer-PWM-Module-TPM-on-i-MX8QXP/m-p/1627830#M203729</link>
      <description>&lt;P&gt;Hello!&lt;/P&gt;
&lt;P&gt;Theoretically the IMX7ULP and the IMX8QXP have the same TPM module, the only difference is the counter, in the IMX7ULP the counter is of 16-bit. And in IMX8QXP the counter is of 32-bit.&lt;/P&gt;
&lt;P&gt;Also, I checked and the combability with the IMX8ULP is until &lt;A href="https://github.com/nxp-imx/linux-imx/blob/git.kernel.org/linux-stable/linux-5.17.y/Documentation/devicetree/bindings/timer/nxp,tpm-timer.yaml" target="_self"&gt;5.17.y Kernel&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;So, the driver should works well in the IMX8QXP.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards!&lt;/P&gt;</description>
      <pubDate>Tue, 04 Apr 2023 17:31:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-driver-for-Timer-PWM-Module-TPM-on-i-MX8QXP/m-p/1627830#M203729</guid>
      <dc:creator>Manuel_Salas</dc:creator>
      <dc:date>2023-04-04T17:31:51Z</dc:date>
    </item>
  </channel>
</rss>