<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Install cactus player on custom hardware</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Install-cactus-player-on-custom-hardware/m-p/1627429#M203673</link>
    <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;I have enabled vpu encoder and decoder on my device(imx8qxp) running android_11.0.0_2.2.0. I wanted to test the hardware decoder. I have tried running a video on imx8qxp MEK hardware and observe less CPU usage. MEK seems to have built-in media player (cactus player). But when I use some other apk on the same hardware CPU usage seems to be more.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, I want to confirm the same behaviour on my custom hardware. However, I am unable to install this media player. Is it NXP customizied player? If so, Can I get the apk installer so that I can tryout the same.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;</description>
    <pubDate>Tue, 04 Apr 2023 07:24:54 GMT</pubDate>
    <dc:creator>Nishal</dc:creator>
    <dc:date>2023-04-04T07:24:54Z</dc:date>
    <item>
      <title>Install cactus player on custom hardware</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Install-cactus-player-on-custom-hardware/m-p/1627429#M203673</link>
      <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;I have enabled vpu encoder and decoder on my device(imx8qxp) running android_11.0.0_2.2.0. I wanted to test the hardware decoder. I have tried running a video on imx8qxp MEK hardware and observe less CPU usage. MEK seems to have built-in media player (cactus player). But when I use some other apk on the same hardware CPU usage seems to be more.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, I want to confirm the same behaviour on my custom hardware. However, I am unable to install this media player. Is it NXP customizied player? If so, Can I get the apk installer so that I can tryout the same.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;</description>
      <pubDate>Tue, 04 Apr 2023 07:24:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Install-cactus-player-on-custom-hardware/m-p/1627429#M203673</guid>
      <dc:creator>Nishal</dc:creator>
      <dc:date>2023-04-04T07:24:54Z</dc:date>
    </item>
    <item>
      <title>Re: Install cactus player on custom hardware</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Install-cactus-player-on-custom-hardware/m-p/1627527#M203688</link>
      <description>&lt;P&gt;In our platform contains a pre-installed Cactus player in the android 11 version BSP.&lt;/P&gt;
&lt;P&gt;You can see if it exist in the &lt;/P&gt;
&lt;P&gt;the list in&amp;nbsp;device/nxp/imx8m/ProductConfigCommon.mk&lt;/P&gt;
&lt;PRE&gt;&lt;SPAN class=""&gt; PRODUCT_PACKAGES += \&lt;/SPAN&gt;
&lt;SPAN class=""&gt;    vsidaemon \&lt;/SPAN&gt;
&lt;SPAN class=""&gt;    CactusPlayer&lt;/SPAN&gt;&amp;nbsp;&lt;/PRE&gt;
&lt;P&gt;&amp;nbsp; &lt;/P&gt;</description>
      <pubDate>Tue, 04 Apr 2023 08:56:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Install-cactus-player-on-custom-hardware/m-p/1627527#M203688</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2023-04-04T08:56:52Z</dc:date>
    </item>
  </channel>
</rss>