<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic About using CSI and PWM functions at the same time in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/About-using-CSI-and-PWM-functions-at-the-same-time/m-p/1626218#M203560</link>
    <description>&lt;P&gt;Hello everyone, I wanted to enable PWM8_OUT on imx6ull's ENET1_RX_ER port, but I noticed that pwm8 also manages the pwm output on the CSI_HSYNC port. Does this mean that there is some kind of potential conflict (e.g. CCM configuration) if I want to enable CMOS Sensor Interface (CSI) at the same time? What do I need to pay attention to? Thanks a lot.&lt;/P&gt;</description>
    <pubDate>Fri, 31 Mar 2023 17:12:38 GMT</pubDate>
    <dc:creator>JanTang</dc:creator>
    <dc:date>2023-03-31T17:12:38Z</dc:date>
    <item>
      <title>About using CSI and PWM functions at the same time</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-using-CSI-and-PWM-functions-at-the-same-time/m-p/1626218#M203560</link>
      <description>&lt;P&gt;Hello everyone, I wanted to enable PWM8_OUT on imx6ull's ENET1_RX_ER port, but I noticed that pwm8 also manages the pwm output on the CSI_HSYNC port. Does this mean that there is some kind of potential conflict (e.g. CCM configuration) if I want to enable CMOS Sensor Interface (CSI) at the same time? What do I need to pay attention to? Thanks a lot.&lt;/P&gt;</description>
      <pubDate>Fri, 31 Mar 2023 17:12:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-using-CSI-and-PWM-functions-at-the-same-time/m-p/1626218#M203560</guid>
      <dc:creator>JanTang</dc:creator>
      <dc:date>2023-03-31T17:12:38Z</dc:date>
    </item>
    <item>
      <title>Re: About using CSI and PWM functions at the same time</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-using-CSI-and-PWM-functions-at-the-same-time/m-p/1627353#M203667</link>
      <description>&lt;P&gt;refer to the dts file&lt;/P&gt;
&lt;P&gt;"&lt;A href="https://github.com/nxp-imx/linux-imx/blob/git.kernel.org/linux-stable/linux-4.14.y/arch/arm/boot/dts/imx6ul-14x14-evk.dts" target="_blank"&gt;https://github.com/nxp-imx/linux-imx/blob/git.kernel.org/linux-stable/linux-4.14.y/arch/arm/boot/dts/imx6ul-14x14-evk.dts&lt;/A&gt;"&lt;/P&gt;
&lt;P&gt;MX6UL_PAD_CSI_HSYNC__CSI_HSYNC 0x1b088&lt;/P&gt;
&lt;P&gt;so PWM8 doesn't be used for csi hsync in current bsp, you can use it&lt;/P&gt;</description>
      <pubDate>Tue, 04 Apr 2023 06:21:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-using-CSI-and-PWM-functions-at-the-same-time/m-p/1627353#M203667</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-04-04T06:21:33Z</dc:date>
    </item>
  </channel>
</rss>