<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX8MP HDMI + LVDS Dual Display</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-HDMI-LVDS-Dual-Display/m-p/1626139#M203554</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Maybe you have to change the dtb, the bsp includes a btb for dual display the &lt;STRONG&gt;&lt;EM&gt;imx8mp-evk-basler-rm67191.dts&lt;/EM&gt;&lt;/STRONG&gt; add to linux-imx/arch/arch/arm64/boot/dts/freescale and can works fo your display or change the pixel clock if it different&lt;/P&gt;
&lt;P&gt;regards&lt;/P&gt;</description>
    <pubDate>Fri, 31 Mar 2023 14:46:05 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2023-03-31T14:46:05Z</dc:date>
    <item>
      <title>IMX8MP HDMI + LVDS Dual Display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-HDMI-LVDS-Dual-Display/m-p/1626096#M203550</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are trying to use the following dual display,&lt;/P&gt;&lt;P&gt;1. HDMI&lt;/P&gt;&lt;P&gt;2. LVDS =&amp;gt; 5 Inch Single Channel LVDS - 800 x 600&lt;/P&gt;&lt;P&gt;Above setup is working fine with the configuration of more than 22.5 MHz of pixel clock.&lt;/P&gt;&lt;P&gt;We currently trying to use the following dual display,&lt;/P&gt;&lt;P&gt;1. HDMI =&amp;gt; 320 x 240 =&amp;gt; Display spec specifies the pixel clock should be around 6.5 MHz only.&lt;/P&gt;&lt;P&gt;2. LVDS =&amp;gt; 5 Inch Single Channel LVDS - 800 x 600&lt;/P&gt;&lt;P&gt;When we try to set the 6.5 MHz pixel clock, display does not get working.&lt;/P&gt;&lt;P&gt;Please share the information about the above the setup,&lt;BR /&gt;1. NXP IMX8MP supported minimum pixel clock frequency&lt;BR /&gt;2. With this configuration, what is optimal pixel frequency to configure for Dual Display working.&lt;/P&gt;&lt;P&gt;Please share your inputs.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Veera.H.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 31 Mar 2023 13:11:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-HDMI-LVDS-Dual-Display/m-p/1626096#M203550</guid>
      <dc:creator>VeeraH</dc:creator>
      <dc:date>2023-03-31T13:11:09Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP HDMI + LVDS Dual Display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-HDMI-LVDS-Dual-Display/m-p/1626139#M203554</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Maybe you have to change the dtb, the bsp includes a btb for dual display the &lt;STRONG&gt;&lt;EM&gt;imx8mp-evk-basler-rm67191.dts&lt;/EM&gt;&lt;/STRONG&gt; add to linux-imx/arch/arch/arm64/boot/dts/freescale and can works fo your display or change the pixel clock if it different&lt;/P&gt;
&lt;P&gt;regards&lt;/P&gt;</description>
      <pubDate>Fri, 31 Mar 2023 14:46:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-HDMI-LVDS-Dual-Display/m-p/1626139#M203554</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2023-03-31T14:46:05Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP HDMI + LVDS Dual Display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-HDMI-LVDS-Dual-Display/m-p/1632113#M204079</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Please find here with more details,&lt;/P&gt;&lt;P&gt;We have following two displays,&lt;/P&gt;&lt;P&gt;1. HDMI LCD Display: iMX8MP HDMI OUT =&amp;gt; TFT401A =&amp;gt; 320 x 240 LCD Display&lt;/P&gt;&lt;P&gt;2.&amp;nbsp;&lt;SPAN&gt;LVDS =&amp;gt; 5 Inch Single Channel LVDS - 800 x 600&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Display 1 is in need of video pixel clock of 6.5 MHz to work. Whenever we configure the video pixel clock as 6.5 MHz, both displays are not working.&lt;BR /&gt;&lt;BR /&gt;if suppose, we have normal hdmi display with 720p and without 6.5 MHz video pixel clock. both HDMI &amp;amp; LVDS displays are working fine.&lt;/P&gt;&lt;P&gt;We are getting into issue when we try to use the small HDMI LCD Display with 320 x 240 and restricting 6.5 MHz video pixel clock.&lt;/P&gt;&lt;P&gt;Please share your inputs on video pixel clock configuration.&lt;/P&gt;</description>
      <pubDate>Wed, 12 Apr 2023 11:52:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-HDMI-LVDS-Dual-Display/m-p/1632113#M204079</guid>
      <dc:creator>VeeraH</dc:creator>
      <dc:date>2023-04-12T11:52:19Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP HDMI + LVDS Dual Display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-HDMI-LVDS-Dual-Display/m-p/1646111#M205403</link>
      <description>&lt;P&gt;Please share your inputs whether HDMI LCD Display with 240 x 320 can be interfaced with i.MX8MP.&lt;/P&gt;</description>
      <pubDate>Mon, 08 May 2023 05:01:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-HDMI-LVDS-Dual-Display/m-p/1646111#M205403</guid>
      <dc:creator>VeeraH</dc:creator>
      <dc:date>2023-05-08T05:01:34Z</dc:date>
    </item>
  </channel>
</rss>