<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックtflite + XNNPACK delegate for inference on quantized network not working</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/tflite-XNNPACK-delegate-for-inference-on-quantized-network-not/m-p/1624303#M203418</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Running on i.mx8QM MEK board, with Yocto Linux&amp;nbsp;LF5.15.71_2.2.0&lt;/P&gt;&lt;P&gt;Following the I.MX Machine Learning User Guide §3.7 to benchmark inference of TFLite using XNNPACK delegate with the example model&amp;nbsp;mobilenet_v1_1.0_224_quant.tflite, I see that XNNPACK delegate is not being used for the inference (most likely because this is a quantized network - as it works fine with fp32 models).&lt;/P&gt;&lt;P&gt;Browsing the web a little bit, it sounds like XNNPACK supports quantized networks since Sept 2021 (cf&amp;nbsp;&lt;A href="https://blog.tensorflow.org/2021/09/faster-quantized-inference-with-xnnpack.html" target="_blank"&gt;https://blog.tensorflow.org/2021/09/faster-quantized-inference-with-xnnpack.html&lt;/A&gt;).&lt;/P&gt;&lt;P&gt;Is it possible and if so how can I get the XNNPACK delegate to work with quantized networks ? I guess I need to change something somewhere in the yocto linux build scripts... but what and where ?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Wed, 29 Mar 2023 14:35:32 GMT</pubDate>
    <dc:creator>edouard_charvet</dc:creator>
    <dc:date>2023-03-29T14:35:32Z</dc:date>
    <item>
      <title>tflite + XNNPACK delegate for inference on quantized network not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/tflite-XNNPACK-delegate-for-inference-on-quantized-network-not/m-p/1624303#M203418</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Running on i.mx8QM MEK board, with Yocto Linux&amp;nbsp;LF5.15.71_2.2.0&lt;/P&gt;&lt;P&gt;Following the I.MX Machine Learning User Guide §3.7 to benchmark inference of TFLite using XNNPACK delegate with the example model&amp;nbsp;mobilenet_v1_1.0_224_quant.tflite, I see that XNNPACK delegate is not being used for the inference (most likely because this is a quantized network - as it works fine with fp32 models).&lt;/P&gt;&lt;P&gt;Browsing the web a little bit, it sounds like XNNPACK supports quantized networks since Sept 2021 (cf&amp;nbsp;&lt;A href="https://blog.tensorflow.org/2021/09/faster-quantized-inference-with-xnnpack.html" target="_blank"&gt;https://blog.tensorflow.org/2021/09/faster-quantized-inference-with-xnnpack.html&lt;/A&gt;).&lt;/P&gt;&lt;P&gt;Is it possible and if so how can I get the XNNPACK delegate to work with quantized networks ? I guess I need to change something somewhere in the yocto linux build scripts... but what and where ?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 29 Mar 2023 14:35:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/tflite-XNNPACK-delegate-for-inference-on-quantized-network-not/m-p/1624303#M203418</guid>
      <dc:creator>edouard_charvet</dc:creator>
      <dc:date>2023-03-29T14:35:32Z</dc:date>
    </item>
    <item>
      <title>Re: tflite + XNNPACK delegate for inference on quantized network not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/tflite-XNNPACK-delegate-for-inference-on-quantized-network-not/m-p/1625380#M203491</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You have to check the deepview &lt;A href="https://www.nxp.com/design/software/development-software/eiq-ml-development-environment/eiq-inference-with-deepviewrt:EIQ-INFERENCE-DEEPVIEWRT" target="_blank"&gt;https://www.nxp.com/design/software/development-software/eiq-ml-development-environment/eiq-inference-with-deepviewrt:EIQ-INFERENCE-DEEPVIEWRT&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Since not all images quantized works it have to be int8 delegate but the fp32 do not.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 30 Mar 2023 14:23:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/tflite-XNNPACK-delegate-for-inference-on-quantized-network-not/m-p/1625380#M203491</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2023-03-30T14:23:01Z</dc:date>
    </item>
  </channel>
</rss>