<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic I.MX RT1166 Flashdriver Issue in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX-RT1166-Flashdriver-Issue/m-p/1622374#M203276</link>
    <description>&lt;P&gt;I am trying to write a custom flashdriver application for the I.MX RT1166. I have been using the iMXRT117x_FlexSPI_SFDP project that can be found in the ide/Examples/Flashdrivers/NXP/iMXRT subfolder of the Mcuxpresso installation as it is my understanding that the 1170 and the M7 of the 1166 have the same peripheral addresses.&lt;/P&gt;&lt;P&gt;My issue arises once I am running the flashdriver on the 1166 eval kit. Without modifying anything in the example I am getting a hardfault in the flexspi_nor_get_config call. I have tried to change the CONFIG_OPTION0 value to the various different speeds supported and it still doesn't work.&lt;/P&gt;&lt;P&gt;Is there anything obvious I am missing or?&lt;/P&gt;</description>
    <pubDate>Mon, 27 Mar 2023 07:57:15 GMT</pubDate>
    <dc:creator>ojh</dc:creator>
    <dc:date>2023-03-27T07:57:15Z</dc:date>
    <item>
      <title>I.MX RT1166 Flashdriver Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX-RT1166-Flashdriver-Issue/m-p/1622374#M203276</link>
      <description>&lt;P&gt;I am trying to write a custom flashdriver application for the I.MX RT1166. I have been using the iMXRT117x_FlexSPI_SFDP project that can be found in the ide/Examples/Flashdrivers/NXP/iMXRT subfolder of the Mcuxpresso installation as it is my understanding that the 1170 and the M7 of the 1166 have the same peripheral addresses.&lt;/P&gt;&lt;P&gt;My issue arises once I am running the flashdriver on the 1166 eval kit. Without modifying anything in the example I am getting a hardfault in the flexspi_nor_get_config call. I have tried to change the CONFIG_OPTION0 value to the various different speeds supported and it still doesn't work.&lt;/P&gt;&lt;P&gt;Is there anything obvious I am missing or?&lt;/P&gt;</description>
      <pubDate>Mon, 27 Mar 2023 07:57:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX-RT1166-Flashdriver-Issue/m-p/1622374#M203276</guid>
      <dc:creator>ojh</dc:creator>
      <dc:date>2023-03-27T07:57:15Z</dc:date>
    </item>
  </channel>
</rss>