<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX8MPlus RMII_REF_CLK</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MPlus-RMII-REF-CLK/m-p/1621476#M203202</link>
    <description>&lt;P&gt;OK, that produces exactly the same values that I had configured manually, but DOES NOT PRODUCE ANY SIGNAL on the pad!&lt;/P&gt;&lt;P&gt;Can you measure a 50MHz clock on the SAI1_MCLK pad when configured as ENET1_TX_CLK?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 24 Mar 2023 07:32:48 GMT</pubDate>
    <dc:creator>lw1</dc:creator>
    <dc:date>2023-03-24T07:32:48Z</dc:date>
    <item>
      <title>i.MX8MPlus RMII_REF_CLK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MPlus-RMII-REF-CLK/m-p/1616913#M202857</link>
      <description>&lt;P&gt;The i.MX 8M Plus Applications Processor Data Sheet states, that the SAI1_MCLK pad can be used as RMII reference clock, but the Processor Reference Manual does not provide any information on how to accomplish this.&lt;/P&gt;&lt;P&gt;According to the latter, the SAI1_MCLK pad can be configured as ENET1_TX_CLK and GPR1 Bit 13 should control the direction of the pin, but I could not get any signal out of this pad.&lt;/P&gt;&lt;P&gt;Furthermore the GPR1 description for this bit has a note:&lt;/P&gt;&lt;P&gt;SOI bit for the pad(iomuxc_sw_input_on_pad_enet_td2) should be set also;&lt;/P&gt;&lt;P&gt;which is probably a copy/paste error from the description of Bit 20.&lt;/P&gt;&lt;P&gt;I can only output the RMII_REF_CLK via pad GPIO1_IO00 as ALT1_CCM_ENET_PHY_REF_CLK_ROOT.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any way to get SAI1_MCLK to output a 50MHz RMII clock, or is there an error in the Processor Datasheet?&lt;/P&gt;</description>
      <pubDate>Thu, 16 Mar 2023 14:22:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MPlus-RMII-REF-CLK/m-p/1616913#M202857</guid>
      <dc:creator>lw1</dc:creator>
      <dc:date>2023-03-16T14:22:03Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8MPlus RMII_REF_CLK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MPlus-RMII-REF-CLK/m-p/1618027#M202925</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;As seen on the 8.1 Table it is possible, it is possible and it may be an ALT MODE, in ENET1 section on page 1334 is mentioned SAI1_MCLK as the pad for the REF_CLK.&lt;/P&gt;
&lt;P&gt;See that ALT4 in ENET1 section uses SAI pads, so it is possible.&lt;/P&gt;
&lt;P&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Mon, 20 Mar 2023 01:25:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MPlus-RMII-REF-CLK/m-p/1618027#M202925</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2023-03-20T01:25:37Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8MPlus RMII_REF_CLK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MPlus-RMII-REF-CLK/m-p/1618978#M203012</link>
      <description>&lt;P&gt;I read what's written in the docs, BUT THAT APPARENTLY DOESN'T MATCH THE REALITY!&lt;/P&gt;&lt;P&gt;The documentation lists the ALT4 function of the SAI1_MCLK pad as ENET1_TX_CLK which usually refers to the RGMII TXC signal and not the RMII REF_CLK.&lt;/P&gt;&lt;P&gt;As stated before THERE IS NO SIGNAL on the SAI1_MCLK pad when configured as ALT4.&lt;/P&gt;</description>
      <pubDate>Tue, 21 Mar 2023 07:51:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MPlus-RMII-REF-CLK/m-p/1618978#M203012</guid>
      <dc:creator>lw1</dc:creator>
      <dc:date>2023-03-21T07:51:59Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8MPlus RMII_REF_CLK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MPlus-RMII-REF-CLK/m-p/1621120#M203170</link>
      <description>&lt;P&gt;Please create a new config tools project to see that the SAI1_MCLK pin has the TX_CLK function while the TXC used by the RGMII function is taken by another pin.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="josephlinares_0-1679595350033.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/216064iA3E3A401376CE9C1/image-size/medium?v=v2&amp;amp;px=400" role="button" title="josephlinares_0-1679595350033.png" alt="josephlinares_0-1679595350033.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;josephlinares_0-1679595350033.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 23 Mar 2023 18:16:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MPlus-RMII-REF-CLK/m-p/1621120#M203170</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2023-03-23T18:16:02Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8MPlus RMII_REF_CLK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MPlus-RMII-REF-CLK/m-p/1621476#M203202</link>
      <description>&lt;P&gt;OK, that produces exactly the same values that I had configured manually, but DOES NOT PRODUCE ANY SIGNAL on the pad!&lt;/P&gt;&lt;P&gt;Can you measure a 50MHz clock on the SAI1_MCLK pad when configured as ENET1_TX_CLK?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 24 Mar 2023 07:32:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MPlus-RMII-REF-CLK/m-p/1621476#M203202</guid>
      <dc:creator>lw1</dc:creator>
      <dc:date>2023-03-24T07:32:48Z</dc:date>
    </item>
  </channel>
</rss>