<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: IMX8MP uart2 to uart4</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-uart2-to-uart4/m-p/1618444#M202975</link>
    <description>&lt;P&gt;Hi Aldo,&lt;BR /&gt;&lt;BR /&gt;Thanks for your reply,&lt;BR /&gt;&lt;BR /&gt;I'm not using the audio, I basically changed most uart inside imx8mpxxx.dtb as nothing works...&amp;nbsp;&lt;BR /&gt;Trying to just have a simple Yocto Linux booting with UART4.&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;/P&gt;&lt;P&gt;J.&lt;/P&gt;</description>
    <pubDate>Mon, 20 Mar 2023 12:56:44 GMT</pubDate>
    <dc:creator>jmass</dc:creator>
    <dc:date>2023-03-20T12:56:44Z</dc:date>
    <item>
      <title>IMX8MP uart2 to uart4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-uart2-to-uart4/m-p/1616936#M202859</link>
      <description>&lt;P&gt;Hi NXP,&lt;BR /&gt;&lt;BR /&gt;I'm struggling with the change of uart console port. I want to change from uart2 to uart4.&lt;BR /&gt;I saw that there are some questions about it and tried the answers proposed but none of them works.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Blogs/How-to-Change-i-MX8MM-evk-Linux-Debug-UART/ba-p/1243938#M40" target="_blank"&gt;https://community.nxp.com/t5/Blogs/How-to-Change-i-MX8MM-evk-Linux-Debug-UART/ba-p/1243938#M40&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/IMX8MP-EVK-Change-u-boot-debug-console-UART2-gt-UART1/m-p/1285780/highlight/true" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/IMX8MP-EVK-Change-u-boot-debug-console-UART2-gt-UART1/m-p/1285780/highlight/true&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Plus-IMX8MP-EVK-switch-uart4-to-A53-and-change-debug/m-p/1447724#M189580" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Plus-IMX8MP-EVK-switch-uart4-to-A53-and-change-debug/m-p/1447724#M189580&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I'm using the IMX8MP-LPDDR4-EVK board only with Yocto Linux. I have done the modifications with patch files (in attachments) following others answers. I'm using the 5.15.72-2.2.0 imx manifest.&lt;BR /&gt;&lt;BR /&gt;I build only the imx-image-core. It works like a charm without modifications but as I said I want to switch uart (needed in our custom board) and that kind of work but the board does not boot.&lt;BR /&gt;&lt;BR /&gt;Here is what I did:&lt;BR /&gt;- build a clean image using imx-docker with manifest 5.15.71-2.2.0&lt;BR /&gt;- then create my own /sources/meta-folder with my /recipes-bsp/imx-atf &amp;amp; /recipes-bsp/u-boot, recipes-kernel/linux-imx&lt;BR /&gt;- added all config files + bbappend + files/modifs.patch&lt;BR /&gt;- then force compilation with bitbake imx-atf, bitbake u-boot, bitbake linux-imx&lt;/P&gt;&lt;P&gt;- then recreate a new *.wic.zst file with bitbake imx-image-core&lt;BR /&gt;&lt;BR /&gt;everything goes well and the SDcard is flashed correctly. When I power on the board, the UART port as changed and I can see the image in attachment but the boot process stops here...&lt;BR /&gt;&lt;BR /&gt;What am I missing ?&lt;BR /&gt;&lt;BR /&gt;Thanks for your reply.&lt;/P&gt;</description>
      <pubDate>Thu, 16 Mar 2023 15:09:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-uart2-to-uart4/m-p/1616936#M202859</guid>
      <dc:creator>jmass</dc:creator>
      <dc:date>2023-03-16T15:09:16Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP uart2 to uart4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-uart2-to-uart4/m-p/1617901#M202919</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Most of your changes looks correct, in you Linux patch I see that you made changes to 3 device tree files so I would like to know exactly which dts are you using for your test?&lt;BR /&gt;is it audio board dts or jailhouse dual linux dts?&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Fri, 17 Mar 2023 20:52:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-uart2-to-uart4/m-p/1617901#M202919</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2023-03-17T20:52:33Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP uart2 to uart4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-uart2-to-uart4/m-p/1618444#M202975</link>
      <description>&lt;P&gt;Hi Aldo,&lt;BR /&gt;&lt;BR /&gt;Thanks for your reply,&lt;BR /&gt;&lt;BR /&gt;I'm not using the audio, I basically changed most uart inside imx8mpxxx.dtb as nothing works...&amp;nbsp;&lt;BR /&gt;Trying to just have a simple Yocto Linux booting with UART4.&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;/P&gt;&lt;P&gt;J.&lt;/P&gt;</description>
      <pubDate>Mon, 20 Mar 2023 12:56:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-uart2-to-uart4/m-p/1618444#M202975</guid>
      <dc:creator>jmass</dc:creator>
      <dc:date>2023-03-20T12:56:44Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP uart2 to uart4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-uart2-to-uart4/m-p/1619536#M203056</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;So you’re using the default one, correct?&lt;BR /&gt;Also, are you trying this on our EVK right?&lt;BR /&gt;I do not think that it is not booting rather is just not configured correctly.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Tue, 21 Mar 2023 23:46:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-uart2-to-uart4/m-p/1619536#M203056</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2023-03-21T23:46:02Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP uart2 to uart4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-uart2-to-uart4/m-p/1619537#M203057</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Yes I am usine the default one and yes on the NXP EVK (lpddr4).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;so Am I misaine a file or something? Could it be because of the bl_31 (imx-atf) ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;P&gt;J.&lt;/P&gt;</description>
      <pubDate>Tue, 21 Mar 2023 23:49:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-uart2-to-uart4/m-p/1619537#M203057</guid>
      <dc:creator>jmass</dc:creator>
      <dc:date>2023-03-21T23:49:35Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP uart2 to uart4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-uart2-to-uart4/m-p/1621026#M203162</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;Found the issue. Need to modify meta-freescale/conf/machine/include/imx-base.inc :&lt;/P&gt;&lt;LI-CODE lang="c"&gt;SOC_ATF_BOOT_UART_BASE:mx8m-generic-bsp = "0x30a60000"&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;and imx8mp-evk.inc :&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;SERIAL_CONSOLES = "115200;ttymxc3"&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;BR /&gt;Thanks,&lt;/P&gt;&lt;P&gt;J.&lt;/P&gt;</description>
      <pubDate>Thu, 23 Mar 2023 15:27:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-uart2-to-uart4/m-p/1621026#M203162</guid>
      <dc:creator>jmass</dc:creator>
      <dc:date>2023-03-23T15:27:51Z</dc:date>
    </item>
  </channel>
</rss>