<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックCamera Support/Use in iMXRT1064</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Camera-Support-Use-in-iMXRT1064/m-p/1614723#M202705</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;&amp;nbsp;&amp;nbsp; We are currently using the&lt;STRONG&gt; iMX RT1064&lt;/STRONG&gt; in one of our projects and we are planning to use this same RT1064 for a camera related Project. But looks that RT1064 has only Parallel CSI not the serial, and we have planned to add a Bridge IC for that.&lt;BR /&gt;&lt;STRONG&gt;Requirement for this project&amp;nbsp; is 2MP camera(1080p) with real-time Video Streaming and Monitor.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Is it advisable to use the Same iMX RT1064 for our project or can we move to another Processor?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;BR /&gt;Jagan K&lt;/P&gt;</description>
    <pubDate>Tue, 14 Mar 2023 08:24:45 GMT</pubDate>
    <dc:creator>jagan_k</dc:creator>
    <dc:date>2023-03-14T08:24:45Z</dc:date>
    <item>
      <title>Camera Support/Use in iMXRT1064</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Camera-Support-Use-in-iMXRT1064/m-p/1614723#M202705</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&amp;nbsp;&amp;nbsp; We are currently using the&lt;STRONG&gt; iMX RT1064&lt;/STRONG&gt; in one of our projects and we are planning to use this same RT1064 for a camera related Project. But looks that RT1064 has only Parallel CSI not the serial, and we have planned to add a Bridge IC for that.&lt;BR /&gt;&lt;STRONG&gt;Requirement for this project&amp;nbsp; is 2MP camera(1080p) with real-time Video Streaming and Monitor.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Is it advisable to use the Same iMX RT1064 for our project or can we move to another Processor?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;BR /&gt;Jagan K&lt;/P&gt;</description>
      <pubDate>Tue, 14 Mar 2023 08:24:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Camera-Support-Use-in-iMXRT1064/m-p/1614723#M202705</guid>
      <dc:creator>jagan_k</dc:creator>
      <dc:date>2023-03-14T08:24:45Z</dc:date>
    </item>
    <item>
      <title>Re: Camera Support/Use in iMXRT1064</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Camera-Support-Use-in-iMXRT1064/m-p/1615176#M202731</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/188928"&gt;@jagan_k&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The IMRT1064 could be suitable for your application, however I cannot assure you that it will have an amazing performance, I recommend you iMXRT1170 or a i.MX processors since these are better options for streaming applications.&lt;/P&gt;
&lt;P&gt;Best Regards, Miguel.&lt;/P&gt;</description>
      <pubDate>Tue, 14 Mar 2023 18:32:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Camera-Support-Use-in-iMXRT1064/m-p/1615176#M202731</guid>
      <dc:creator>Miguel04</dc:creator>
      <dc:date>2023-03-14T18:32:18Z</dc:date>
    </item>
  </channel>
</rss>