<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックUART RX</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/UART-RX/m-p/1609648#M202336</link>
    <description>&lt;DIV&gt;&lt;SPAN class=""&gt;I setup the&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN class=""&gt;Baud Rate&lt;/SPAN&gt;&lt;SPAN class=""&gt; to 4800，and connected a&amp;nbsp;peripheral with our UART.the peripheral send&amp;nbsp; handshake packages to UART,frequency was 10HZ，the length of the data were 10 bytes.But I found a confused phenomenon is that the data were not print on time，the data were print after 40 s. is that i need to change some configures for uart?why?&lt;/SPAN&gt;&lt;/DIV&gt;</description>
    <pubDate>Mon, 06 Mar 2023 02:49:51 GMT</pubDate>
    <dc:creator>tudouboss</dc:creator>
    <dc:date>2023-03-06T02:49:51Z</dc:date>
    <item>
      <title>UART RX</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UART-RX/m-p/1609648#M202336</link>
      <description>&lt;DIV&gt;&lt;SPAN class=""&gt;I setup the&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN class=""&gt;Baud Rate&lt;/SPAN&gt;&lt;SPAN class=""&gt; to 4800，and connected a&amp;nbsp;peripheral with our UART.the peripheral send&amp;nbsp; handshake packages to UART,frequency was 10HZ，the length of the data were 10 bytes.But I found a confused phenomenon is that the data were not print on time，the data were print after 40 s. is that i need to change some configures for uart?why?&lt;/SPAN&gt;&lt;/DIV&gt;</description>
      <pubDate>Mon, 06 Mar 2023 02:49:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UART-RX/m-p/1609648#M202336</guid>
      <dc:creator>tudouboss</dc:creator>
      <dc:date>2023-03-06T02:49:51Z</dc:date>
    </item>
    <item>
      <title>Re: UART RX</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UART-RX/m-p/1610522#M202396</link>
      <description>&lt;P&gt;Which products are you using?&lt;/P&gt;</description>
      <pubDate>Tue, 07 Mar 2023 04:11:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UART-RX/m-p/1610522#M202396</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2023-03-07T04:11:25Z</dc:date>
    </item>
    <item>
      <title>Re: UART RX</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UART-RX/m-p/1613598#M202602</link>
      <description>&lt;P&gt;&lt;SPAN&gt;IMX6U6AVM08AC(IMX6DL DDR_2G EMMC_4G)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;kernel version：&lt;SPAN&gt;3.14.52&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Uboot version&lt;/SPAN&gt;：&lt;SPAN&gt;u-boot-2016.03&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;when I used the cmd "cat /dev/ttymxc3" at upper status,I found that the terminal printf "rx fifo overrun".However, the data transmission interval is 100ms, and each frame of data transmission is less than 20ms.In this case, what state is it that the register cannot be set?&lt;/P&gt;&lt;P&gt;tks&lt;/P&gt;</description>
      <pubDate>Mon, 13 Mar 2023 02:41:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UART-RX/m-p/1613598#M202602</guid>
      <dc:creator>tudouboss</dc:creator>
      <dc:date>2023-03-13T02:41:53Z</dc:date>
    </item>
  </channel>
</rss>