<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Chromium browser does not start in user context in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Chromium-browser-does-not-start-in-user-context/m-p/1609027#M202286</link>
    <description>&lt;P&gt;Hi AldoG,&lt;/P&gt;&lt;P&gt;thanks for the hints. I checked the remaining space at my home directory. It is over 5GB free space available. But it is a FAT32 partition. The rootfs is an ext4 partition. Maybe it has something to do with the mixture of both filesystems.&lt;/P&gt;</description>
    <pubDate>Fri, 03 Mar 2023 07:52:02 GMT</pubDate>
    <dc:creator>MicMoba</dc:creator>
    <dc:date>2023-03-03T07:52:02Z</dc:date>
    <item>
      <title>Chromium browser does not start in user context</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Chromium-browser-does-not-start-in-user-context/m-p/1603732#M201872</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I want to use Chromium-ozone-wayland browser on my device. I had build the yocto image sucessfully. Chrome Version: &lt;/SPAN&gt;&lt;SPAN&gt;Chromium 96.0.4664.110 stable&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;When I start chromium as user I got the following error message:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;user@ ~$ chromium 
[1223:1223:0222/143357.967200:ERROR:process_singleton_posix.cc(340)] Failed to create /home/moba/.config/chromium/SingletonLock: Operation not permitted (1)
[1223:1223:0222/143357.967678:ERROR:chrome_browser_main.cc(1313)] Failed to create a ProcessSingleton for your profile directory. This means that running multiple instances would start multiple browser processes rather than opening a new window in the existing process. Aborting now to avoid profile corruption.&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;I can start chromium as root user with 'chromium --no-sandbox'&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;What does it mean 'Failed to create a ProcessSingleton'? My home is located on a fat32 partition. But I can not image that this has something to do with it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Edit:&lt;/P&gt;&lt;P&gt;When I use 'chromium --user-data-dir=/tmp/' chromium started. So error maybe depends on the fat32 partition?&lt;/P&gt;</description>
      <pubDate>Wed, 22 Feb 2023 14:01:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Chromium-browser-does-not-start-in-user-context/m-p/1603732#M201872</guid>
      <dc:creator>MicMoba</dc:creator>
      <dc:date>2023-02-22T14:01:00Z</dc:date>
    </item>
    <item>
      <title>Re: Chromium browser does not start in user context</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Chromium-browser-does-not-start-in-user-context/m-p/1608719#M202265</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;looking through the web this seems to be a problem related to the space left in your partition:&lt;BR /&gt;&lt;A href="https://bugs.chromium.org/p/chromium/issues/detail?id=73035" target="_blank"&gt;https://bugs.chromium.org/p/chromium/issues/detail?id=73035&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://stackoverflow.com/questions/38894321/chromium-browser-singleton-bug-caused-by-power-failure" target="_blank"&gt;https://stackoverflow.com/questions/38894321/chromium-browser-singleton-bug-caused-by-power-failure&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Thu, 02 Mar 2023 20:41:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Chromium-browser-does-not-start-in-user-context/m-p/1608719#M202265</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2023-03-02T20:41:11Z</dc:date>
    </item>
    <item>
      <title>Re: Chromium browser does not start in user context</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Chromium-browser-does-not-start-in-user-context/m-p/1609027#M202286</link>
      <description>&lt;P&gt;Hi AldoG,&lt;/P&gt;&lt;P&gt;thanks for the hints. I checked the remaining space at my home directory. It is over 5GB free space available. But it is a FAT32 partition. The rootfs is an ext4 partition. Maybe it has something to do with the mixture of both filesystems.&lt;/P&gt;</description>
      <pubDate>Fri, 03 Mar 2023 07:52:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Chromium-browser-does-not-start-in-user-context/m-p/1609027#M202286</guid>
      <dc:creator>MicMoba</dc:creator>
      <dc:date>2023-03-03T07:52:02Z</dc:date>
    </item>
  </channel>
</rss>