<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: I.mx8 HDMI without I2C in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-mx8-HDMI-without-I2C/m-p/1607535#M202183</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/138651"&gt;@hhami_2040&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;I hope you are doing well.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;-&amp;gt;That HDMI I2C can only be used from HDMI IP. This is used by HDMI IP for communicating with the display devices like TV and monitors.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;-&amp;gt;The HDMI has a Master I2C interface for a display data channel (DDC) connection. The HDMI bus has Display Data Channel (I2C bus for configuration and status exchange between two devices). The DDC connects just like a standard I2C bus. The HDMI module can drive the display data channel (DDC) bus, which supports a variety of I2C commands, on the hdmi_ddc_scl and hdmi_ddc_sda pins. This allows the TV set/monitor to provide information to the host device, such as supported resolutions.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;-&amp;gt;Please share the FPGA board schematic, the block diagram you are using &amp;amp; how are you setting up the system, please share more on it.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Dhruvit Vasavada&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 01 Mar 2023 09:26:44 GMT</pubDate>
    <dc:creator>Dhruvit</dc:creator>
    <dc:date>2023-03-01T09:26:44Z</dc:date>
    <item>
      <title>I.mx8 HDMI without I2C</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-mx8-HDMI-without-I2C/m-p/1605545#M202011</link>
      <description>&lt;P&gt;Hello All,&lt;BR /&gt;We have an iMX8 QM(Apalis Module) and Ixora carrier board.&lt;BR /&gt;We have hdmi 1920*1080@60 right now!! I am currently trying to use the HDMI Interface on the i.mx8qm without I2C.&lt;BR /&gt;We want to connect HDMI to the an fpga board and dont want to have I2C!!&lt;BR /&gt;May i know whether the Bypass I2c EDID for the HDMI I2c? I see that in the driver drivers/video/mxc_hdmi.c, there are a lot of configurations that is related to i2c communication.&lt;BR /&gt;By the way, I do not need to configure any setting on the HDMI display.&lt;BR /&gt;Thanks.&lt;BR /&gt;Regards,&lt;/P&gt;</description>
      <pubDate>Sat, 25 Feb 2023 13:34:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-mx8-HDMI-without-I2C/m-p/1605545#M202011</guid>
      <dc:creator>hhami_2040</dc:creator>
      <dc:date>2023-02-25T13:34:05Z</dc:date>
    </item>
    <item>
      <title>Re: I.mx8 HDMI without I2C</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-mx8-HDMI-without-I2C/m-p/1607535#M202183</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/138651"&gt;@hhami_2040&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;I hope you are doing well.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;-&amp;gt;That HDMI I2C can only be used from HDMI IP. This is used by HDMI IP for communicating with the display devices like TV and monitors.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;-&amp;gt;The HDMI has a Master I2C interface for a display data channel (DDC) connection. The HDMI bus has Display Data Channel (I2C bus for configuration and status exchange between two devices). The DDC connects just like a standard I2C bus. The HDMI module can drive the display data channel (DDC) bus, which supports a variety of I2C commands, on the hdmi_ddc_scl and hdmi_ddc_sda pins. This allows the TV set/monitor to provide information to the host device, such as supported resolutions.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;-&amp;gt;Please share the FPGA board schematic, the block diagram you are using &amp;amp; how are you setting up the system, please share more on it.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Dhruvit Vasavada&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 01 Mar 2023 09:26:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-mx8-HDMI-without-I2C/m-p/1607535#M202183</guid>
      <dc:creator>Dhruvit</dc:creator>
      <dc:date>2023-03-01T09:26:44Z</dc:date>
    </item>
  </channel>
</rss>