<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic usb problem in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/usb-problem/m-p/1607367#M202167</link>
    <description>&lt;P&gt;Hello, I would like to ask a question, in the official example of usb, "dev_cdc_vcom_bm_cm7" is used as a slave device and the computer is used as the master device to send data to the development board, I found that multiple interrupts are generated and each interrupt has 512 bytes, is there an example of this? Is there any example where only one interrupt can be generated and all data will be received? Thanks!&lt;/P&gt;</description>
    <pubDate>Wed, 01 Mar 2023 06:00:44 GMT</pubDate>
    <dc:creator>eao</dc:creator>
    <dc:date>2023-03-01T06:00:44Z</dc:date>
    <item>
      <title>usb problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/usb-problem/m-p/1607367#M202167</link>
      <description>&lt;P&gt;Hello, I would like to ask a question, in the official example of usb, "dev_cdc_vcom_bm_cm7" is used as a slave device and the computer is used as the master device to send data to the development board, I found that multiple interrupts are generated and each interrupt has 512 bytes, is there an example of this? Is there any example where only one interrupt can be generated and all data will be received? Thanks!&lt;/P&gt;</description>
      <pubDate>Wed, 01 Mar 2023 06:00:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/usb-problem/m-p/1607367#M202167</guid>
      <dc:creator>eao</dc:creator>
      <dc:date>2023-03-01T06:00:44Z</dc:date>
    </item>
  </channel>
</rss>