<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Display Driver on imxrt1176 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Display-Driver-on-imxrt1176/m-p/1606397#M202086</link>
    <description>&lt;P&gt;These values are obtained from the specific datasheet. In specific the datasheet contains some values: &lt;A href="https://www.nxp.com/docs/en/data-sheet/RK055MHD091A0-CTG.pdf" target="_blank"&gt;Microsoft Word - RK055MHD091A0-CTG.doc (nxp.com)&lt;/A&gt;&lt;BR /&gt;You should refer to the timing table and modify the macros value according to it.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
    <pubDate>Mon, 27 Feb 2023 22:40:04 GMT</pubDate>
    <dc:creator>Omar_Anguiano</dc:creator>
    <dc:date>2023-02-27T22:40:04Z</dc:date>
    <item>
      <title>Display Driver on imxrt1176</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-Driver-on-imxrt1176/m-p/1595470#M201230</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I was not able to find all the command listed that were used in the code. Can you help me correct where I am going wrong?&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;I am using IMXRT 1176 and am using sd_jpeg example.&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;I want to understand the panel driver and I am referring the HX8394 document attached here. Whether the document is correct or can you share any other document?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Correct me if I am wrong,&lt;/P&gt;
&lt;P&gt;The display RK055MHD091 that is supported by iMXRT1176 uses&amp;nbsp;HX8394 as the TFT driver.&lt;/P&gt;
&lt;P&gt;1) The IMXRT1176 D-PHY layer supports 1 or 2 Data Lanes and&amp;nbsp;HX8394 D-PHY layer supports upto 4 Data Lanes. So, my understanding is that only 1 Data Lane can also be used whereas the code uses 2 Data Lanes. If&amp;nbsp;&lt;STRONG&gt;DEMO_MIPI_DSI_LANE_NUM &lt;/STRONG&gt;is configured to &lt;STRONG&gt;1, &lt;/STRONG&gt;will the sd_jpeg example works as usual?&lt;/P&gt;
&lt;P&gt;2) Is it possible to write the panel driver code directly in IMXRT1176 that can drive a display panel without the use of the panel driver like HX8394? Can you also share the code of HX8394?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 08 Feb 2023 22:43:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-Driver-on-imxrt1176/m-p/1595470#M201230</guid>
      <dc:creator>Devaharsha</dc:creator>
      <dc:date>2023-02-08T22:43:08Z</dc:date>
    </item>
    <item>
      <title>Re: Display Driver on imxrt1176</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-Driver-on-imxrt1176/m-p/1596010#M201279</link>
      <description>&lt;P&gt;I deleted your file due it is confidential&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 08 Feb 2023 22:47:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-Driver-on-imxrt1176/m-p/1596010#M201279</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2023-02-08T22:47:29Z</dc:date>
    </item>
    <item>
      <title>Re: Display Driver on imxrt1176</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-Driver-on-imxrt1176/m-p/1596257#M201296</link>
      <description>&lt;P&gt;Oh sorry. I thought it wont be any problem sharing here.&lt;/P&gt;&lt;P&gt;I have another query, How VSYC, HSYNC values are calculated and panel specific values like VFB,HSW,VSW,etc are calculated because in the panel driver datasheet, there's only minimum values supported?&lt;/P&gt;</description>
      <pubDate>Thu, 09 Feb 2023 06:35:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-Driver-on-imxrt1176/m-p/1596257#M201296</guid>
      <dc:creator>Devaharsha</dc:creator>
      <dc:date>2023-02-09T06:35:28Z</dc:date>
    </item>
    <item>
      <title>Re: Display Driver on imxrt1176</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-Driver-on-imxrt1176/m-p/1606397#M202086</link>
      <description>&lt;P&gt;These values are obtained from the specific datasheet. In specific the datasheet contains some values: &lt;A href="https://www.nxp.com/docs/en/data-sheet/RK055MHD091A0-CTG.pdf" target="_blank"&gt;Microsoft Word - RK055MHD091A0-CTG.doc (nxp.com)&lt;/A&gt;&lt;BR /&gt;You should refer to the timing table and modify the macros value according to it.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Mon, 27 Feb 2023 22:40:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-Driver-on-imxrt1176/m-p/1606397#M202086</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2023-02-27T22:40:04Z</dc:date>
    </item>
  </channel>
</rss>