<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックiMX8M Plus: How to enter USB Download Mode?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-How-to-enter-USB-Download-Mode/m-p/1605560#M202015</link>
    <description>&lt;P&gt;After configuring the boot pins to USB Download Mode, what other requirements are there to enter the mode? What should the state of the VBUS pin be, if relevant?&lt;BR /&gt;&lt;BR /&gt;I have tried entering USB download mode using my PHYTEC devboard but couldn't and I need to make sure it works on a board I'm designing.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Sat, 25 Feb 2023 16:40:57 GMT</pubDate>
    <dc:creator>cdvd</dc:creator>
    <dc:date>2023-02-25T16:40:57Z</dc:date>
    <item>
      <title>iMX8M Plus: How to enter USB Download Mode?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-How-to-enter-USB-Download-Mode/m-p/1605560#M202015</link>
      <description>&lt;P&gt;After configuring the boot pins to USB Download Mode, what other requirements are there to enter the mode? What should the state of the VBUS pin be, if relevant?&lt;BR /&gt;&lt;BR /&gt;I have tried entering USB download mode using my PHYTEC devboard but couldn't and I need to make sure it works on a board I'm designing.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Sat, 25 Feb 2023 16:40:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-How-to-enter-USB-Download-Mode/m-p/1605560#M202015</guid>
      <dc:creator>cdvd</dc:creator>
      <dc:date>2023-02-25T16:40:57Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M Plus: How to enter USB Download Mode?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-How-to-enter-USB-Download-Mode/m-p/1606023#M202053</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/212272"&gt;@cdvd&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;USBx_VBUS shall be powered by 5V. One can check the input voltage range of the USBx_VBUS pin in the i.MX8MP datasheet.&lt;/P&gt;
&lt;P&gt;One can also refer to &lt;STRONG&gt;Section 6.1.2.3 Boot From Fuses mode &lt;/STRONG&gt;in the i.MX8MP Reference Manual.&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Ritesh M Patel&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 27 Feb 2023 10:49:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-How-to-enter-USB-Download-Mode/m-p/1606023#M202053</guid>
      <dc:creator>riteshmpatel</dc:creator>
      <dc:date>2023-02-27T10:49:29Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M Plus: How to enter USB Download Mode?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-How-to-enter-USB-Download-Mode/m-p/1606041#M202056</link>
      <description>&lt;P&gt;Hey&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201596"&gt;@riteshmpatel&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;I've looked at the reference manual, and the section about booting from fuses doesn't talk about VBUS at all.&amp;nbsp;&lt;/P&gt;&lt;P&gt;You are saying to "power" the VBUS pin (USB1/2_VBUS_3V3) in the PHY interface, but really it should be pulled to a voltage. Previous releases of the iMX series had a power requirement at this pin, but the 8MP does not.&lt;/P&gt;&lt;P&gt;My question is, what should the connection here be to make sure USB works on OTG mode?&lt;/P&gt;&lt;P&gt;Please find screenshot from your reference design, saying that "VBUS can ignored if not using OTG mode". But what if OTG _is_ required?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot 2023-02-27 121920.png" style="width: 401px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/212485i53764DC09F174910/image-dimensions/401x366?v=v2" width="401" height="366" role="button" title="Screenshot 2023-02-27 121920.png" alt="Screenshot 2023-02-27 121920.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Moreover, when looking at "production programming pins", you are exposing both USB_DM and USB_VBUS. So VBUS must be required for OTG, right? Why else would you do this?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot 2023-02-27 122826.png" style="width: 817px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/212488i70E460B5F42F5AA0/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot 2023-02-27 122826.png" alt="Screenshot 2023-02-27 122826.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;What are the USB VBUS pin requirements for OTG, if any? Do I need to connect it to the USB connector's VBUS? How, if the connector can be powered by the board itself via a power switch?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Mon, 27 Feb 2023 11:29:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-How-to-enter-USB-Download-Mode/m-p/1606041#M202056</guid>
      <dc:creator>cdvd</dc:creator>
      <dc:date>2023-02-27T11:29:47Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M Plus: How to enter USB Download Mode?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-How-to-enter-USB-Download-Mode/m-p/1606796#M202121</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/212272"&gt;@cdvd&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;If one wants the USB to work in OTG mode, the USBx_VBUS pin needs to be supplied with a voltage range listed in the datasheet. Please note that for i.MX8MP, USBx_VBUS is not the power pin, rather it is a sense pin.&lt;/P&gt;
&lt;P&gt;One can refer to the EVK schematic for connection reference of the USBx_VBUS pin.&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Ritesh M Patel&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 28 Feb 2023 11:03:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-How-to-enter-USB-Download-Mode/m-p/1606796#M202121</guid>
      <dc:creator>riteshmpatel</dc:creator>
      <dc:date>2023-02-28T11:03:34Z</dc:date>
    </item>
  </channel>
</rss>