<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: IMXRT1176 M4 Core Slow</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1176-M4-Core-Slow/m-p/1603248#M201820</link>
    <description>&lt;P&gt;Hello, I apologize for the time long being taken, I'm following your case, I'm working on your case, and when I have more information, I will contact you.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
    <pubDate>Tue, 21 Feb 2023 23:56:17 GMT</pubDate>
    <dc:creator>Pavel_Hernandez</dc:creator>
    <dc:date>2023-02-21T23:56:17Z</dc:date>
    <item>
      <title>IMXRT1176 M4 Core Slow</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1176-M4-Core-Slow/m-p/1597660#M201401</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are working on a custom board based on IMXRT 1176 and facing a problem with the performance of the M4 core in the dual core system.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;M7 is configured for 800Mhz&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Compiler options -O2&lt;/P&gt;&lt;P&gt;Memory address DTCM - 0x20000000&lt;/P&gt;&lt;P&gt;Memset for 1000 bytes takes 3.8us&lt;/P&gt;&lt;P&gt;Memcpy for 1000 bytes takes 3.8us&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;M4 is configured for 400Mhz&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Compiler options -O2&lt;/P&gt;&lt;P&gt;Memory address DTCM - 0x20000000&lt;/P&gt;&lt;P&gt;Memset for 1000 bytes takes 29us&lt;/P&gt;&lt;P&gt;Memcpy for 1000 bytes takes 27us&lt;/P&gt;&lt;P&gt;We have also attached the detailed analysis report.&amp;nbsp;&lt;/P&gt;&lt;P&gt;We would like to know the reason for this slow perfomance on the M4 core ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ashok&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 11 Feb 2023 07:49:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMXRT1176-M4-Core-Slow/m-p/1597660#M201401</guid>
      <dc:creator>ashok2</dc:creator>
      <dc:date>2023-02-11T07:49:26Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1176 M4 Core Slow</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1176-M4-Core-Slow/m-p/1599788#M201571</link>
      <description>&lt;P&gt;Hello, I will do a report on that performance, I will not have a response about that because this will involve other departments, thanks for being interested in product NXP.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Feb 2023 18:51:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMXRT1176-M4-Core-Slow/m-p/1599788#M201571</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2023-02-15T18:51:13Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1176 M4 Core Slow</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1176-M4-Core-Slow/m-p/1603248#M201820</link>
      <description>&lt;P&gt;Hello, I apologize for the time long being taken, I'm following your case, I'm working on your case, and when I have more information, I will contact you.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Tue, 21 Feb 2023 23:56:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMXRT1176-M4-Core-Slow/m-p/1603248#M201820</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2023-02-21T23:56:17Z</dc:date>
    </item>
  </channel>
</rss>