<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic I.mx 8m plus real coding and recognition performance in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-mx-8m-plus-real-coding-and-recognition-performance/m-p/1602591#M201776</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;At present, there is a project that needs several performance requirements, I wonder whether imx8mp can meet them&lt;/P&gt;&lt;P&gt;Ⅰ.Video decoding H264 at 1080p 30fps and 720p 30fps&lt;/P&gt;&lt;P&gt;Ⅱ.Can be 1080p video recognition, recognition types are respectively target recognition, license plate recognition, face recognition&lt;/P&gt;&lt;P&gt;Whether the above types of identification are supported, whether the development tools are complete, and whether the performance of 4G memory is sufficient&lt;/P&gt;&lt;P&gt;Thank&lt;/P&gt;</description>
    <pubDate>Tue, 21 Feb 2023 07:16:45 GMT</pubDate>
    <dc:creator>kemingqian</dc:creator>
    <dc:date>2023-02-21T07:16:45Z</dc:date>
    <item>
      <title>I.mx 8m plus real coding and recognition performance</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-mx-8m-plus-real-coding-and-recognition-performance/m-p/1602591#M201776</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;At present, there is a project that needs several performance requirements, I wonder whether imx8mp can meet them&lt;/P&gt;&lt;P&gt;Ⅰ.Video decoding H264 at 1080p 30fps and 720p 30fps&lt;/P&gt;&lt;P&gt;Ⅱ.Can be 1080p video recognition, recognition types are respectively target recognition, license plate recognition, face recognition&lt;/P&gt;&lt;P&gt;Whether the above types of identification are supported, whether the development tools are complete, and whether the performance of 4G memory is sufficient&lt;/P&gt;&lt;P&gt;Thank&lt;/P&gt;</description>
      <pubDate>Tue, 21 Feb 2023 07:16:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-mx-8m-plus-real-coding-and-recognition-performance/m-p/1602591#M201776</guid>
      <dc:creator>kemingqian</dc:creator>
      <dc:date>2023-02-21T07:16:45Z</dc:date>
    </item>
  </channel>
</rss>