<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックHow to select the defconfig file for Secure Boot</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-select-the-defconfig-file-for-Secure-Boot/m-p/1601930#M201727</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to enable secure boot feature for custom &lt;FONT size="4"&gt;&lt;LI-PRODUCT title="IMX8MPLUS" id="IMX8MPLUS"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/FONT&gt; board running #Android&amp;nbsp;11. I have followed the Android Security guide provided by NXP&lt;/P&gt;&lt;P&gt;In the device/nxp/imx8m/evk_8mp/UbootKernelBoardConfig.mk I see as follows:&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;# u-boot target&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;TARGET_BOOTLOADER_CONFIG := imx8mp:imx8mp_evk_android_defconfig&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;TARGET_BOOTLOADER_CONFIG += imx8mp-trusty:imx8mp_evk_android_trusty_defconfig&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;TARGET_BOOTLOADER_CONFIG += imx8mp-trusty-secure-unlock:imx8mp_evk_android_trusty_secure_unlock_defconfig&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;TARGET_BOOTLOADER_CONFIG += imx8mp-dual:imx8mp_evk_android_dual_defconfig&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;TARGET_BOOTLOADER_CONFIG += imx8mp-trusty-dual:imx8mp_evk_android_trusty_dual_defconfig&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;TARGET_BOOTLOADER_CONFIG += imx8mp-evk-uuu:imx8mp_evk_android_uuu_defconfig&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;TARGET_BOOTLOADER_CONFIG += imx8mp-powersave:imx8mp_evk_android_powersave_defconfig&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;TARGET_BOOTLOADER_CONFIG += imx8mp-trusty-powersave:imx8mp_evk_android_trusty_powersave_defconfig&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="4"&gt;After compilation in the build log I can see all the defconfigs are build.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="4"&gt;Do I have to update all the defconfigs for Secure boot? Shall I take the values from build-log for csf from all of them seperately? How do I make sure which defconfig is getting used while bootup?&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT size="4"&gt;Thanks,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="4"&gt;Abhiroop&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 20 Feb 2023 11:35:12 GMT</pubDate>
    <dc:creator>abhiroopnray</dc:creator>
    <dc:date>2023-02-20T11:35:12Z</dc:date>
    <item>
      <title>How to select the defconfig file for Secure Boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-select-the-defconfig-file-for-Secure-Boot/m-p/1601930#M201727</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to enable secure boot feature for custom &lt;FONT size="4"&gt;&lt;LI-PRODUCT title="IMX8MPLUS" id="IMX8MPLUS"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/FONT&gt; board running #Android&amp;nbsp;11. I have followed the Android Security guide provided by NXP&lt;/P&gt;&lt;P&gt;In the device/nxp/imx8m/evk_8mp/UbootKernelBoardConfig.mk I see as follows:&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;# u-boot target&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;TARGET_BOOTLOADER_CONFIG := imx8mp:imx8mp_evk_android_defconfig&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;TARGET_BOOTLOADER_CONFIG += imx8mp-trusty:imx8mp_evk_android_trusty_defconfig&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;TARGET_BOOTLOADER_CONFIG += imx8mp-trusty-secure-unlock:imx8mp_evk_android_trusty_secure_unlock_defconfig&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;TARGET_BOOTLOADER_CONFIG += imx8mp-dual:imx8mp_evk_android_dual_defconfig&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;TARGET_BOOTLOADER_CONFIG += imx8mp-trusty-dual:imx8mp_evk_android_trusty_dual_defconfig&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;TARGET_BOOTLOADER_CONFIG += imx8mp-evk-uuu:imx8mp_evk_android_uuu_defconfig&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;TARGET_BOOTLOADER_CONFIG += imx8mp-powersave:imx8mp_evk_android_powersave_defconfig&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;TARGET_BOOTLOADER_CONFIG += imx8mp-trusty-powersave:imx8mp_evk_android_trusty_powersave_defconfig&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="4"&gt;After compilation in the build log I can see all the defconfigs are build.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="4"&gt;Do I have to update all the defconfigs for Secure boot? Shall I take the values from build-log for csf from all of them seperately? How do I make sure which defconfig is getting used while bootup?&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT size="4"&gt;Thanks,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="4"&gt;Abhiroop&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 20 Feb 2023 11:35:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-select-the-defconfig-file-for-Secure-Boot/m-p/1601930#M201727</guid>
      <dc:creator>abhiroopnray</dc:creator>
      <dc:date>2023-02-20T11:35:12Z</dc:date>
    </item>
    <item>
      <title>Re: How to select the defconfig file for Secure Boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-select-the-defconfig-file-for-Secure-Boot/m-p/1602800#M201792</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201315"&gt;@abhiroopnray&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;This way that you build android images means all modes of bootloader built with HAB enabled.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You don't necessarily need all defconfigs for secure boot, you can modify the + symbols to remove what you don't want.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Tue, 21 Feb 2023 10:09:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-select-the-defconfig-file-for-Secure-Boot/m-p/1602800#M201792</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2023-02-21T10:09:26Z</dc:date>
    </item>
  </channel>
</rss>