<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX8M Plus + UFS flash</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Plus-UFS-flash/m-p/1601406#M201676</link>
    <description>&lt;P&gt;any chance to get UFS on i.MX9 series&lt;/P&gt;&lt;P&gt;emmc speeds start to feel a bit vintage&lt;/P&gt;</description>
    <pubDate>Sat, 18 Feb 2023 10:04:50 GMT</pubDate>
    <dc:creator>dav1</dc:creator>
    <dc:date>2023-02-18T10:04:50Z</dc:date>
    <item>
      <title>i.MX8M Plus + UFS flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Plus-UFS-flash/m-p/1257236#M172131</link>
      <description>&lt;P&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;In need of large flash with high performance (256GByte+)&lt;/P&gt;&lt;P&gt;Curious why the i.MX8M Plus doesn't come with a UFS peripheral, seems Kioxia is pushing for this technology over traditional eMMC's&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I know some phones use PCIe NAND flash as an alternative. Not sure what is supported in HW there on the Plus, please advice.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks David&lt;/P&gt;</description>
      <pubDate>Tue, 06 Apr 2021 09:51:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Plus-UFS-flash/m-p/1257236#M172131</guid>
      <dc:creator>dav1</dc:creator>
      <dc:date>2021-04-06T09:51:34Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M Plus + UFS flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Plus-UFS-flash/m-p/1257842#M172192</link>
      <description>&lt;P&gt;The i.MX8MPlus processor doesn't have support for UFS interface. It has the SD&amp;nbsp;Host Controller module that can support regular SD and eMMC devices, and GPMI&amp;nbsp;module that supports generic parallel NAND Flash. Also, it has the PCIe&amp;nbsp;interface, so, PCIe mass storage devices can also be supported.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Artur&lt;/P&gt;</description>
      <pubDate>Wed, 07 Apr 2021 09:14:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Plus-UFS-flash/m-p/1257842#M172192</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2021-04-07T09:14:12Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M Plus + UFS flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Plus-UFS-flash/m-p/1601406#M201676</link>
      <description>&lt;P&gt;any chance to get UFS on i.MX9 series&lt;/P&gt;&lt;P&gt;emmc speeds start to feel a bit vintage&lt;/P&gt;</description>
      <pubDate>Sat, 18 Feb 2023 10:04:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Plus-UFS-flash/m-p/1601406#M201676</guid>
      <dc:creator>dav1</dc:creator>
      <dc:date>2023-02-18T10:04:50Z</dc:date>
    </item>
  </channel>
</rss>