<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 IMXRT1175 Impossible to launch a program running in RAM with &amp;quot;blhost&amp;quot; command &amp;quot;load-image&amp;quot;</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1175-Impossible-to-launch-a-program-running-in-RAM-with/m-p/1600504#M201621</link>
    <description>&lt;P&gt;IMXRT1175 Impossible to launch a program running in RAM with "blhost" command "load-image" without loading the flashloader first.&lt;/P&gt;&lt;P&gt;The sequence is:&lt;BR /&gt;- power on&lt;BR /&gt;- command&lt;BR /&gt;blhost -t 5000 -u 0x1FC9,0x013D -j -- load-image c:\wrk\SecureProvisioning1\bootable_images\myprogram.bin&amp;nbsp; (myprogram.bin is linked in RAM)&lt;BR /&gt;But the program doesn't start.&lt;/P&gt;&lt;P&gt;I have used the SecureProvisioningTool to generate a bootable "myprogram.bin" but without success.&lt;/P&gt;&lt;P&gt;Is there a guide or an application note that can help me?&lt;BR /&gt;Thank you&lt;/P&gt;</description>
    <pubDate>Thu, 16 Feb 2023 18:13:14 GMT</pubDate>
    <dc:creator>stefanotatini</dc:creator>
    <dc:date>2023-02-16T18:13:14Z</dc:date>
    <item>
      <title>IMXRT1175 Impossible to launch a program running in RAM with "blhost" command "load-image"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1175-Impossible-to-launch-a-program-running-in-RAM-with/m-p/1600504#M201621</link>
      <description>&lt;P&gt;IMXRT1175 Impossible to launch a program running in RAM with "blhost" command "load-image" without loading the flashloader first.&lt;/P&gt;&lt;P&gt;The sequence is:&lt;BR /&gt;- power on&lt;BR /&gt;- command&lt;BR /&gt;blhost -t 5000 -u 0x1FC9,0x013D -j -- load-image c:\wrk\SecureProvisioning1\bootable_images\myprogram.bin&amp;nbsp; (myprogram.bin is linked in RAM)&lt;BR /&gt;But the program doesn't start.&lt;/P&gt;&lt;P&gt;I have used the SecureProvisioningTool to generate a bootable "myprogram.bin" but without success.&lt;/P&gt;&lt;P&gt;Is there a guide or an application note that can help me?&lt;BR /&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Thu, 16 Feb 2023 18:13:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMXRT1175-Impossible-to-launch-a-program-running-in-RAM-with/m-p/1600504#M201621</guid>
      <dc:creator>stefanotatini</dc:creator>
      <dc:date>2023-02-16T18:13:14Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1175 Impossible to launch a program running in RAM with "blhost" command "lo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1175-Impossible-to-launch-a-program-running-in-RAM-with/m-p/1602213#M201755</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200272"&gt;@stefanotatini&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The i.MX RT bootROM does not support BLHOST, only SDPHost commands. So if you want to load an image to SRAM using BLHOST, you will need to run a program , like our flashloader,&amp;nbsp; which does support BLHOST first.&lt;/P&gt;
&lt;P&gt;See the below snapshot from&amp;nbsp;AN12238 i.MX RT Flashloader Use Case.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="diego_charles_0-1676919657777.png" style="width: 598px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/211617iDE7B70840CFB8711/image-dimensions/598x269?v=v2" width="598" height="269" role="button" title="diego_charles_0-1676919657777.png" alt="diego_charles_0-1676919657777.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Please note that&amp;nbsp;&lt;SPAN&gt;AN12238&amp;nbsp;&lt;/SPAN&gt; it is for i.MX RT10xx and not specific for RT11xx. I only used this AN to give you more information on why the flashloader is used.&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;Once the MCU booted into serial downloader mode&lt;/STRONG&gt; this is what the SPT does, load the flashloader first, before loading an image.For more detials about the commands used by the tool can see SPT log output.&lt;/P&gt;
&lt;P&gt;Also, for more information, please consult our&amp;nbsp; SPT user guide&amp;nbsp;&lt;CITE class="iUh30 qLRx3b tjvcx" role="text"&gt;&lt;SPAN class="dyjrff qzEoUe"&gt;MCUXSPTUG&lt;/SPAN&gt;&lt;/CITE&gt;&lt;/P&gt;
&lt;P&gt;&lt;LI-WRAPPER&gt;&lt;/LI-WRAPPER&gt;&lt;/P&gt;
&lt;DIV class="B6fmyf"&gt;
&lt;DIV class="TbwUpd"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;/DIV&gt;
&lt;P&gt;If this does not help, please let me know more about your requirements.&lt;/P&gt;
&lt;P&gt;All the best,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Diego&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 20 Feb 2023 19:15:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMXRT1175-Impossible-to-launch-a-program-running-in-RAM-with/m-p/1602213#M201755</guid>
      <dc:creator>diego_charles</dc:creator>
      <dc:date>2023-02-20T19:15:22Z</dc:date>
    </item>
  </channel>
</rss>