<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: IMX6 SWUpdate Requires a Login</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-SWUpdate-Requires-a-Login/m-p/1599967#M201577</link>
    <description>&lt;P&gt;Within my bitbake environment I build&amp;nbsp;core-image-full-cmdline, when I load this onto my SD card. I get the same error. I cannot log into the image.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 15 Feb 2023 22:22:15 GMT</pubDate>
    <dc:creator>MichaelBMiner</dc:creator>
    <dc:date>2023-02-15T22:22:15Z</dc:date>
    <item>
      <title>IMX6 SWUpdate Requires a Login</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-SWUpdate-Requires-a-Login/m-p/1599700#M201561</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have gone back and forth with&amp;nbsp;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202155" target="_blank"&gt;@Sanket_Parekh&lt;/A&gt;&amp;nbsp;to get my u-boot environment properly setup. Now that I have that working I started to build my image and run the SWUpdate kernel.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I build my images with the commands&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;bitbake swupdate-image
bitbake mainapplication-dev
bitbake smg-image-swu&lt;/LI-CODE&gt;&lt;P&gt;Some background, when I build my image I get a file&amp;nbsp;mainapplication-dev-imx6ull14x14evk.wic.bz2. When I build SWUpdate I get the image&amp;nbsp;swupdate-image-imx6ull14x14evk.ext4.gz.u-boot.&lt;/P&gt;&lt;P&gt;I also get a properly created .SWU file but I am not ready to use this.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I program my sd card with&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;bzcat mainapplication-dev-imx6ull14x14evk.wic.bz2 | sudo dd of=/dev/sdd bs=1M conv=fsync&lt;/LI-CODE&gt;&lt;P&gt;Then I mount my SD card to my Linux machine and run&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;sudo cp swupdate-image-imx6ull14x14evk.ext4.gz.u-boot /mnt/rootfs/&lt;/LI-CODE&gt;&lt;P&gt;I boot my device and interrupt the boot process to enter u-boot. I then run the commands&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;setenv bootargs console=ttymxc0,115200 root=/dev/ram0 rootfstype=ext4 rw 
setenv swupdate_bootcmd "load mmc 1 0x82000000 swupdate-image-imx6ull14x14evk.ext4.gz.u-boot;load mmc 1 0x82a00000 imx6ull-14x14-evk.dtb;load mmc 1 0x80800000 zImage;setenv root /dev/ram0;setenv rootfstype ext4;bootz 0x80800000 0x82000000 0x82a00000"
saveenv
print swupdate_bootcmd
run swupdate_bootcmd&lt;/LI-CODE&gt;&lt;P&gt;This successfully loads the SWUpdate kernel&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;Kernel image @ 0x80800000 [ 0x000000 - 0x641778 ]
## Loading init Ramdisk from Legacy Image at 82000000 ...
   Image Name:   swupdate-image-imx6ull14x14evk-2
   Image Type:   ARM Linux RAMDisk Image (uncompressed)
   Data Size:    8992112 Bytes = 8.6 MiB
   Load Address: 00000000
   Entry Point:  00000000
   Verifying Checksum ... OK
## Flattened Device Tree blob at 82a00000
   Booting using the fdt blob at 0x82a00000
   Using Device Tree in place at 82a00000, end 82a0bb93&lt;/LI-CODE&gt;&lt;P&gt;There is a lot printed after this as modules are loaded. Then I get to the end&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;Swupdate v2021.11.0

Licensed under GPLv2. See source distribution for detailed copyright notices.

[INFO ] : SWUPDATE running :  [print_registered_handlers] : Registered handlers:
[INFO ] : SWUPDATE running :  [print_registered_handlers] :     dummy
[INFO ] : SWUPDATE running :  [print_registered_handlers] :     archive
[INFO ] : SWUPDATE running :  [print_registered_handlers] :     tar
[INFO ] : SWUPDATE running :  [print_registered_handlers] :     flash
[INFO ] : SWUPDATE running :  [print_registered_handlers] :     lua
[INFO ] : SWUPDATE running :  [print_registered_handlers] :     raw
[INFO ] : SWUPDATE running :  [print_registered_handlers] :     rawfile
[INFO ] : SWUPDATE running :  [print_registered_handlers] :     rawcopy
[INFO ] : SWUPDATE running :  [print_registered_handlers] :     shellscript
[INFO ] : SWUPDATE running :  [print_registered_handlers] :     preinstall
[INFO ] : SWUPDATE running :  [print_registered_handlers] :     postinstall
[TRACE] : SWUPDATE running :  [listener_create] : creating socket at /tmp/swupdateprog
[TRACE] : SWUPDATE running :  [network_initializer] : Main loop daemon
[TRACE] : SWUPDATE running :  [listener_create] : creating socket at /tmp/sockinstctrl
[TRACE] : SWUPDATE running :  [start_swupdate_subprocess] : Started webserver with pid 258 and fd 8
[INFO ] : SWUPDATE running :  [start_mongoose] : Mongoose web server version 6.18 with pid 258 started on port(s) 8080 with web root [/www]
Connected to SWUpdate via /tmp/swupdateprog

NXP i.MX Release Distro 5.10-hardknott imx6ull14x14evk /dev/ttymxc0

imx6ull14x14evk login: &lt;/LI-CODE&gt;&lt;P&gt;Here I am asked to login. I have tried admin/admin, admin/pass and a user I created for my main application with un/pw michael/michael. For these I always get the error&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;NXP i.MX Release Distro 5.10-hardknott imx6ull14x14evk /dev/ttymxc0

imx6ull14x14evk login: admin
Password:
Login incorrect
login[255]: invalid password for 'UNKNOWN' on 'ttymxc0'
imx6ull14x14evk login:&lt;/LI-CODE&gt;&lt;P&gt;If I attempt to login as root I am not prompted for a password.&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;imx6ull14x14evk login: root
Login incorrect
login[255]: invalid password for 'root' on 'ttymxc0'
imx6ull14x14evk login:&lt;/LI-CODE&gt;&lt;P&gt;As it stands I am completely locked out of my device every time I run the SWUpdate kernel. Has anyone else experienced this? Does anyone have any ideas?&lt;/P&gt;</description>
      <pubDate>Wed, 15 Feb 2023 16:12:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-SWUpdate-Requires-a-Login/m-p/1599700#M201561</guid>
      <dc:creator>MichaelBMiner</dc:creator>
      <dc:date>2023-02-15T16:12:50Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 SWUpdate Requires a Login</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-SWUpdate-Requires-a-Login/m-p/1599965#M201576</link>
      <description>&lt;P&gt;I believe this has to do with my rootfs, however I have not been able to confirm this. I have built a new image core-image-full-cmdline and attempted to place SWUpdate in my SD card image. When I attempt to run my SWUpdate kernel I am told there is bad data and a CRC is failing.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Feb 2023 22:20:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-SWUpdate-Requires-a-Login/m-p/1599965#M201576</guid>
      <dc:creator>MichaelBMiner</dc:creator>
      <dc:date>2023-02-15T22:20:09Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 SWUpdate Requires a Login</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-SWUpdate-Requires-a-Login/m-p/1599967#M201577</link>
      <description>&lt;P&gt;Within my bitbake environment I build&amp;nbsp;core-image-full-cmdline, when I load this onto my SD card. I get the same error. I cannot log into the image.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Feb 2023 22:22:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-SWUpdate-Requires-a-Login/m-p/1599967#M201577</guid>
      <dc:creator>MichaelBMiner</dc:creator>
      <dc:date>2023-02-15T22:22:15Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 SWUpdate Requires a Login</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-SWUpdate-Requires-a-Login/m-p/1600641#M201624</link>
      <description>&lt;P&gt;I kind of figured this out. Someone can correct me if I am wrong. NXP places a limitation preventing root from logging into the system. If you enable debug configs root can login.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The SWUpdate kernel will only be run internal to the device. To resolve my issue I create a swupdate-image.bbappend and added&amp;nbsp;IMAGE_INSTALL_append += " debugconfigs".&lt;/P&gt;&lt;P&gt;Now the SWUpdate kernel can be logged into using root and no password.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 16 Feb 2023 18:22:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-SWUpdate-Requires-a-Login/m-p/1600641#M201624</guid>
      <dc:creator>MichaelBMiner</dc:creator>
      <dc:date>2023-02-16T18:22:22Z</dc:date>
    </item>
  </channel>
</rss>